GUIComposer2 Beta 1.6
Release
Notes
This release note is divided into the following sections:
Introduction,
Documentation, What's New, Upgrade & Compatibility
Information, Host
Support, Dependencies,
Device Support, , Known Issues, Technical Support.
This is an engineering release of the GUIComposer2 Designer, and a product release of the GUIComposer2 Runtime.
Designer version number: 2.0.14
Runtime version number: 3.0.0
The
following documentation is available:
For information on enhancements and defect fixes in earlier releases,
please refer to the release notes from previous releases that are
available in the relnotes_archive
directory.
GUIComposer2 Beta 1.6 is backward compatible with the previous Beta 1.0 release.
This release supports the following hosts:
Windows 7,8,8.1
GUIComposer2 Beta 1.6 ships with support for the following devices built in:
- MSP430FR2355
- MSP430F5529
- MSP430FR4133
- MSP430FR5969
- MSP430FR6989
- MSP430G2452
- MSP430G2553
- MSP430P401R
- TMS320F28377D
Here are the known issues with this release.
- In the Serial IO Demo project template, the ti-widget-serialio component always has the following attributes set in the gist:
initcomplete devicename="MSP430FR2355" boardname="MSP430FR2355".
Workaround: the index.js file for the project overrides these settings programmatically.
Please forward issues and feedback to gc2@list.ti.com
Last updated: Sept. 22, 2015