Introduction

This module is a study of the Angle of Arrival (AoA). AoA is a technique for finding the direction that an incoming packet is coming from. The estimated time to complete this lab is between 1-2 hours. It is assumed that the reader has a basic knowledge of embedded C tool chains and general C programming concepts.

This lab is based on the rtls_master, rtls_slave and rtls_passive projects that are part of the SimpleLink™ CC2640R2 SDK.

First, the lab will cover an overview on how to get started with the AoA projects. Subsequent tasks of this lab will guide the user on how to customize these projects in order to answer most of the common AoA questions.

Prerequisites

Required Training

It is required that users complete all steps of the RTLS Introduction lab before moving on to the Angle of Arrival lab. It is also assumed that the user has already installed the software, setup the hardware, and read the recommended chapters covered by the introduction lab. For brevity, only new content will be listed here.

Software for desktop development

This module requires the following kits:

Getting started with AoA booster pack

Getting started – Desktop

Install the Software

This lab requires that you have completed all the steps in the RTLS Introduction lab. This means that you must have

  • CC2640R2 SDK installed
  • Working Python environment
  • Used rtls_example.py script that sets up an RTLS network.

Introduction to AoA

Bluetooth Core Specification Version 5.1 introduces AoA/AoD which are covered under Direction Finding Using Bluetooth Low Energy section.

AoA is for receivers that have RF switches, multiple antennas, can switch antennas and capture I/Q samples when receiving direction finding packets.

AoD is for transmitters that have RF switches, multiple antennas and can switch antennas when transmitting direction finding packets. And recieivers only have one antenna but can capture I/Q samples when receiving direction finding packets.

In the table below and throughout this lab CTE is used in place of Constant Tone Extension as defined by the BLE specification.

Direction Finding Method Transmitter Receiver
AoA Single antenna, transmit CTE Multiple antennas, RF switches, can switch antennas while capturing I/Q data of the CTE
AoD Multiple antennas, RF switches, transmits CTE while switching antennas Single antenna, can capture I/Q data of the CTE

On top of that, the Bluetooth Core Specification version 5.1 specifies the following states can support sending direction finding packets:

  1. Periodic advertising; also called Connectionless CTE
  2. Connection; also called Connection CTE

The theory behind AoA/AoD and Connectionless/Connection CTE is the same, therefore in this SimpleLink Academy training, we will only focus on Connection CTE AoA.

We will explain the AoA theory first and the walk through our SimpleLink CC2640R2F SDK offering.

AoA measurement is typically a 3-step process:

  1. Collect phase information by sampling the I/Q
  2. Calculate the phase difference among the antennas
  3. Covert the phase difference into Angle of Arrival

1. Collect phase information by sampling the I/Q

When two (or more) antennas are placed at a given distance apart from each other, their received RF signals will have a phase difference that is proportional to the difference between their respective distances from the transmitter.

Typically, the signal from one antenna will be a delayed version of the signal from the other antenna. If they are sufficiently close (less than Λ(wavelength)/2 between phase centers), you can always determine which is closest to the transmitter.

These path length differences will depend on the direction of the incoming RF waves relative to the antennas in the array. In order to measure the phase difference accurately, the radio wave packet must contain a section of constant tone with whitening disabled where there are no phase shifts caused by modulation.

Constant Tone Extension (CTE)

The constant tone extension is a section of consecutive 1's without whitening, which is effectively a +250kHz wave on top of the carrier wave. In the Bluetooth Core Specification Version 5.1, both periodic advertising packets and connection packets can contain a constant tone extension(CTE) after the CRC. The CTE can only be sent using uncoded PHY.

2. Calculate the phase difference among the antennas

Phase Difference (Φ) is measured by connecting at least two antennas to the same receiver sequentially (more antennas can be added).

The picture shown below is a constellation diagram which illustrates signal vectors from 2 antennas. If all the antennas are positioned in line and with a fixed distance d, the phase difference Φ between adjacent antennas will be constant.

In order to get a good estimate of Φ (phase), all other intentional phase shifts in the signal should be removed. Connection CTE AoA solution achieves this by adding CTE at the end of packets.

Connection CTE Packet Format

Data Physical Packet format

The grey colored part of the packet shown above means it's optional. The Constant Tone Extension is only enabled when the CP bit in the Data Physical PDU header is set. The detail of the Constant Tone Extension is then specified by the CTEInfo field in the in the Data Physical PDU.

This gives the receiver time to synchronize the demodulator first, and then store the I/Q samples from the CTE into radio RAM. The I/Q data is then extracted by the application layer.

I/Q samples are used to estimate phase difference among antennas. When the receiver gets AoA packets, the RF core will trigger an event that will lead to start of the antenna switching. The RF core will start sampling the I/Q data after the guard period of the CTE and the sampled data will be stored in the radio RAM.

By comparing the I/Q data collected from different antennas, users can get the relative phase difference among antennas.

3. Convert the phase difference into Angle of Arrival

Last step is converting the phase shift (Φ) back to AoA (Θ). Keep in mind if Φ is negative, this means that antenna 2 is ahead of antenna 1 and the Θ.

The angle between the incident wave and antenna array is Θ. Base on the picture below we know that the sin(Θ) = r/d, and d is the distance between antenna 1 and antenna 2 which is known. Then all we need to find out is r.

r is the distance to antenna 2 that the incident wave needs to travel after arriving at antenna 1. We have found that the phase difference between antenna 1 and antenna 2 is Φ, so the extra distance r is equal to wavelength of the incoming signal * Φ/(2Π).

r= Λ* Φ/(2Π)

Therfore Θ can be represented as below:

Note

In rtls_passive example, you might notice that step 3 is not implemented. The reason is simply because by step 2 using our BOOSTXL-AoA we already have linear result from +/-90 degree using antenna pair[1,2] and pair[2,3]. Therefore all we need is to have a look up table to do the fine tuning.

This saves computation time/current consumption compared to doing another arcsin function.

We also tried to do arcsin, but the result is pretty much the same as adding gain and offset after step 2.

What technique does AoA use to identify the direction of incident wave?

Task 1 – Running the AoA application

The SimpleLink™ CC2640R2 SDK has three examples dedicated to performing AoA (rtls_master, rtls_slave and rtls_passive).

In the TI BLE-Stack User's Guide → RTLS Toolbox → Angle of Arrival → AoA application Overview, we have covered how the application works.

Therefore, after following the instruction on Realtime Localization System Introduction, you should be able to get it up and running.

Task 2 – Modify AoA application to use only one antenna array

The out of box SimpleLink™ CC2640R2 SDK rtls_passive example will stay on one antenna array when receiving one AoA packet and then change to another antenna array for the next AoA packet. Following code contains the logic for antenna array switching.

  // Switch ant array
  if (gAoaReport.antConfig == antA1Config)
  {
    gAoaReport.antConfig = antA2Config;
    gAoaReport.antResult = antA2Result;
  }
  else if (gAoaReport.antConfig == antA2Config)
  {
    gAoaReport.antConfig = antA1Config;
    gAoaReport.antResult = antA1Result;
  }
  else
  {
    // Should not get here
    return;
  }

AOA.c::AOA_setupNextRun()

The angle is then decided once both arrays have received AoA packets and judge by the rssi value of the received packet to decide whether the application should trust angle derived from array 1 or array 2.

    // Signal strength is higher on A1 vs A2
    if (antA1Result->rssi > antA2Result->rssi)
    {
        // Use AoA from Antenna Array A1
        AoA_ma.array[AoA_ma.idx] = AoA_A1;
        AoA_ma.currentAoA = AoA_A1;
        AoA_ma.currentAntennaArray = 1;
        AoA_ma.currentRssi = antA1Result->rssi;
        AoA_ma.currentSignalStrength = signalStrength_A1;
        AoA_ma.currentCh = antA1Result->ch;
        AoA.currentangle = AoA_A1;
    }
    // Signal strength is higher on A2 vs A1
    else
    {
        // Use AoA from Antenna Array A2
        AoA_ma.array[AoA_ma.idx] = AoA_A2;
        AoA_ma.currentAoA = AoA_A2;
        AoA_ma.currentAntennaArray = 2;
        AoA_ma.currentRssi = antA2Result->rssi;
        AoA_ma.currentSignalStrength = signalStrength_A2;
        AoA_ma.currentCh = antA2Result->ch;
        AoA.currentangle = AoA_A2;
    }

rtls_ctrl_aoa.c::RTLSCtrl_estimateAngle()

However, this might not be how you want to design or utilize your antennas. Therefore, this section we will walk you through the changes if you only want one antenna array, like Automotive Bluetooth low energy car access satellite node reference design

  • We will go from this configuration:

  • To this configuration (using antenna array #1):

The steps below will guide you through the process of removing one of the antenna array. For this example we will be removing A2, but these steps are also applicable in case that A1 needs to be removed.

  1. Start from the rtls_passive_cc2640r2lp_app project and rename it to rtls_passive_cc2640r2lp_a1_app
  2. Exclude the files ant_array2_config_boostxl_rev1v1.c and ant_array2_config_boostxl_rev1v1.h from the build.
  3. Comment out all of the antenna array 2 dependencies from AOA.c
  //Comment out all the followings lines
  //line 64
  #include "ant_array2_config_boostxl_rev1v1.h"

  // Remove config and result declarations line ~170
  AoA_AntennaConfig *antA2Config = &BOOSTXL_AoA_Config_ArrayA2;
  AoA_AntennaResult *antA2Result = &BOOSTXL_AoA_Result_ArrayA2;

  //line 399, 402 and 405 in AOA_init()
  BOOSTXL_AoA_AntennaPattern_A2_init();
  antA2Result->updated = false;
  aoaResults->antA2Result = antA2Result;

  //line 730~733 in AOA_getActiveAnt()
  else if (gAoaReport.antConfig == antA2Config)
  {
    return 2;
  }

  //line 756~760 in AOA_setupNextRun()
  else if (gAoaReport.antConfig == antA2Config)
  {
    gAoaReport.antConfig = antA1Config;
    gAoaReport.antResult = antA1Result;
  }
  1. Change the following lines in AOA.c to take antenna 1 instead.

    //line 753 and 754 in AOA_setupNextRun()
    // Switch ant array
    if (gAoaReport.antConfig == antA1Config)
    {
     gAoaReport.antConfig = antA1Config;
     gAoaReport.antResult = antA1Result;
    }
    

    c

  2. Replace the content of RTLSCtrl_postProcessAoa in rtls_ctrl_aoa.c with the provided code snippet. What we have done here is to remove all the antenna array 2 dependency.

    void RTLSCtrl_postProcessAoa(rtlsAoa_t *aoaControlBlock, int8_t rssi, uint8_t channel)
    {
    uint8_t status;
    
    if (aoaControlBlock->aoaParams.aoaRole == AOA_ROLE_PASSIVE)
    {
     status = AOA_postProcess(rssi, channel);
    
     if (status)
     {
       switch(aoaControlBlock->aoaParams.resultMode)
       {
         case AOA_MODE_ANGLE:
         {
           AoA_Sample aoaTempResult;
           rtlsAoaResultAngle_t aoaResult;
    
           AOA_getPairAngles();
    
           {
             gAoaResults.antA1Result->updated = false;
    
             const AoA_AntennaResult *antA1Result = gAoaResults.antA1Result;
    
             aoaTempResult = RTLSCtrl_estimateAngle(antA1Result);
    
             aoaResult.angle = aoaTempResult.angle;
             aoaResult.antenna = aoaTempResult.antenna;
             aoaResult.rssi = aoaTempResult.rssi;
             aoaResult.channel = aoaTempResult.channel;
    
             RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_ANGLE, HOST_ASYNC_RSP, (uint8_t *)&aoaResult, sizeof(rtlsAoaResultAngle_t));
           }
         }
         break;
    
         case AOA_MODE_PAIR_ANGLES:
         {
           rtlsAoaResultPairAngles_t aoaResult;
           int16_t *pairAngle;
           uint8_t antenna;
    
           AOA_getPairAngles();
    
           if (gAoaResults.antA1Result->updated == true)
           {
             pairAngle = gAoaResults.antA1Result->pairAngle;
             gAoaResults.antA1Result->updated = false;
             antenna = 1;
           }
           else
           {
             // Should not get here
             return;
           }
    
           aoaResult.rssi = rssi;
           aoaResult.channel = channel;
           aoaResult.antenna = antenna;
    
           for (int i = 0; i < AOA_NUM_ANTENNAS; i++)
           {
             aoaResult.pairAngle[i] = pairAngle[i];
           }
    
           RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_PAIR_ANGLES, HOST_ASYNC_RSP, (uint8_t *)&aoaResult, sizeof(rtlsAoaResultPairAngles_t));
         }
         break;
    
         case AOA_MODE_RAW:
         {
           rtlsAoaResultRaw_t *aoaResult;
           uint16_t numAoaSamples;
           uint16_t samplesToOutput;
           AoA_IQSample *pIter;
    
           aoaResult = RTLSCtrl_malloc(sizeof(rtlsAoaResultRaw_t) + (MAX_SAMPLES_SINGLE_CHUNK * sizeof(AoA_IQSample)));
           pIter = AOA_getRawSamples();
    
           // If the array is not empty
           if (pIter != NULL && aoaResult != NULL)
           {
             // Calculate how many samples we will be outputting
             numAoaSamples = AOA_calcNumOfCteSamples(aoaControlBlock->aoaParams.cteTime,
                                                     aoaControlBlock->aoaParams.cteScanOvs,
                                                     aoaControlBlock->aoaParams.cteOffset);
    
             aoaResult->channel = channel;
             aoaResult->rssi = rssi;
             aoaResult->samplesLength = numAoaSamples;
             aoaResult->antenna = AOA_getActiveAnt();
             aoaResult->offset = 0;
    
             do
             {
               // If the remainder is larger than buff size, tx maximum buff size
               if (aoaResult->samplesLength - aoaResult->offset > MAX_SAMPLES_SINGLE_CHUNK)
               {
                 samplesToOutput = MAX_SAMPLES_SINGLE_CHUNK;
               }
               else
               {
                 // If not, then output the remaining data
                 samplesToOutput = aoaResult->samplesLength - aoaResult->offset;
               }
    
               // Copy the samples to output buffer
               for (int i = 0; i < samplesToOutput; i++)
               {
                 aoaResult->samples[i] = pIter[i];
               }
    
               RTLSHost_sendMsg(RTLS_CMD_AOA_RESULT_RAW, HOST_ASYNC_RSP, (uint8_t *)aoaResult, sizeof(rtlsAoaResultRaw_t) + (sizeof(AoA_IQSample) * samplesToOutput));
    
               aoaResult->offset += samplesToOutput;
               pIter += MAX_SAMPLES_SINGLE_CHUNK;
             }
             while (aoaResult->offset < aoaResult->samplesLength);
           }
    
           if (aoaResult)
           {
             RTLSUTIL_FREE(aoaResult);
           }
         }
         break;
    
         default:
           break;
       }
       // Once all post processing is complete, set up the next run
       AOA_setupNextRun();
     }
    }
    }
    

    rtls_ctrl_aoa.c:: RTLSCtrl_postProcessAoa

  3. Replace the content of RTLSCtrl_estimateAngle in rtls_ctrl_aoa.c with the provided code snippet. What we have done here is to remove all the antenna array 2 dependency and modify the function call to take one array only when making an angle decision.

    //line 122 under local function section
    AoA_Sample RTLSCtrl_estimateAngle(const AoA_AntennaResult *antA1Result);
    
    // The function itself
    AoA_Sample RTLSCtrl_estimateAngle(const AoA_AntennaResult *antA1Result)
    {
     AoA_Sample AoA;
    
     static AoA_movingAverage AoA_ma;
     uint8_t AoA_ma_size = sizeof(AoA_ma.array) / sizeof(AoA_ma.array[0]);
    
     // Calculate AoA for each antenna array
     const int16_t AoA_A1 = ((antA1Result->pairAngle[0] + antA1Result->pairAngle[1]) / 2) + antA1Result->channelOffset[antA1Result->ch];
     // Calculate average signal strength
     const int16_t signalStrength_A1 = (antA1Result->signalStrength[0] + antA1Result->signalStrength[1]) / 2;
    
     // Use AoA from Antenna Array A1
     AoA_ma.array[AoA_ma.idx] = AoA_A1;
     AoA_ma.currentAoA = AoA_A1;
     AoA_ma.currentAntennaArray = 1;
     AoA_ma.currentRssi = antA1Result->rssi;
     AoA_ma.currentSignalStrength = signalStrength_A1;
     AoA_ma.currentCh = antA1Result->ch;
     AoA.currentangle = AoA_A1;
    
     // Add new AoA to moving average
     AoA_ma.array[AoA_ma.idx] = AoA_ma.currentAoA;
    
     // Calculate new moving average
     AoA_ma.AoAsum = 0;
     for(uint8_t i = 0; i < AoA_ma_size; i++)
     {
         AoA_ma.AoAsum += AoA_ma.array[i];
     }
     AoA_ma.AoA = AoA_ma.AoAsum / AoA_ma_size;
    
     // Update moving average index
     if(AoA_ma.idx >= (AoA_ma_size - 1))
     {
         AoA_ma.idx = 0;
     }
     else
     {
         AoA_ma.idx++;
     }
    
     // Return results
     AoA.angle = AoA_ma.AoA;
     AoA.rssi = AoA_ma.currentRssi;
     AoA.signalStrength = AoA_ma.currentSignalStrength;
     AoA.channel = AoA_ma.currentCh;
     AoA.antenna =  AoA_ma.currentAntennaArray;
    
     return AoA;
    }
    

    rtls_ctrl_aoa.c::RTLSCtrl_estimateAngle

When complete, re-run the rtls_example.py, you will observe that all results show antenna 1. See below for example. Note the device address will be different for your launchpad.

PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 34, "rssi": -60, "antenna": 1, "channel": 21}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 36, "rssi": -66, "antenna": 1, "channel": 4}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 36, "rssi": -62, "antenna": 1, "channel": 14}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 37, "rssi": -60, "antenna": 1, "channel": 24}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 37, "rssi": -64, "antenna": 1, "channel": 34}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 34, "rssi": -65, "antenna": 1, "channel": 7}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 35, "rssi": -60, "antenna": 1, "channel": 17}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 32, "rssi": -61, "antenna": 1, "channel": 27}}
PASSIVE: 54:6C:0E:A0:3B:F8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"angle": 32, "rssi": -67, "antenna": 1, "channel": 0}}

Task 3 – Modify AoA application to use only two antennas

Now we have successfully moved from using 2 antenna arrays to 1. We will use the example from Task 2 as the baseline and make the proper changes so we only use 2 antennas from the antenna array 1.

  • Task 2 is using all 3 antennas from A1:

  • And the end goal is using the following:

The following steps will guide you through this process:

  1. Comment out the following in ant_array1_config_boostxl_rev1v1.c.

     //line 57
     #define AOA_Ax_ANT3    AOA_PIN(IOID_30)
    
     //line 131~144
     {// v23
      .a = 1,
      .b = 2,
      .sign = 1,
      .offset = -5,
      .gain = 0.9,
     },
     {// v13
      .a = 0,
      .b = 2,
      .sign = 1,
      .offset = -20,
      .gain = 0.50,
     },
    
  2. Replace the antenna toggling patten antennaPattern_A1 in ant_array1_config_boostxl_rev1v1.c with the provided pattern to remove A1.3.

    AoA_Pattern antennaPattern_A1 = {
     .numPatterns = 32,
     .initialPattern = AOA_A1_SEL | AOA_Ax_ANT2,
     .toggles =
     {
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
      AOA_A1_SEL | AOA_Ax_ANT1, // A1.1
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2 stay with antenna 2 at the end
      AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     }
    };
    

    Using different antennas instead of A1.1 and A1.2

    Our example code always uses antenna A1.2 or A2.2 to receive packets before the CTE. This is set by the code below

       .initialPattern = AOA_A1_SEL | AOA_Ax_ANT2,
    

    antennaPattern_A1[] :: ant_array1_config_boostxl_rev1v1.c

    Therefore, for users using antennas other than A1.2 or A2.2, you will need to modify the initialPattern too.

  3. Change the AOA_NUM_ANTENNAS to 2 in AOA.h

    // line 58
    #define AOA_NUM_ANTENNAS 2
    
  4. The IOs that control the antenna switches are initialized in AOA.c::AOA_openPins Therefore, we need to modify this part of the code since we are using one less IO. Change the pinMask to the following

    //line 295 and line 321
    pinMask = (1 << IOID_27 | 1 << IOID_28 | 1 << IOID_29 );
    

Fundamental done

Now the application only uses antenna A1.1 and A1.2! Very well done! And the updated software still works with RTLS_Monitor GUI.

Task 4 – AoA I/Q Samples

Python solution

The python solution for rtls_aoa in exercise 4 is provided at the end of this training.

So far we have worked on the application code to modify the rtls_passive to work with custom HW. We will now spend some time looking into the I/Q data.

The reason for checking I/Q data is that different HW design will yield different result which will affect your own angle calculation algorithm. For example, if the rf switches you are using need longer settling time than the ones on BOOSTXL-AoA, then you will need to discard more I/Q samples when doing calculations.

To decide how many I/Q samples you can use, you will need to extract I/Q samples and calculate phase to determine at which samples antennas are changing.

We will first take a look at where I/Q samples are stored and in what format.

I/Q is stored in the radio core RAM(RFC_RAM_BASE + 0x0000C000) and each I/Q pair takes up 32 bits space where I is stored in the lower 16 bits and Q is stored in higher 16 bits.

void AOA_getRxIQ(uint8_t *packetId, AoA_IQSample **samples)
{
  // Should only be called when RF Core is awake
  *packetId = (*((uint8_t*)AOA_PACKET_RAM));
  *samples = packetId ? (AoA_IQSample *)&HWREG(RFC_RAM_BASE + 0x0000C000):NULL;
}

In AOA.c

I/Q samples resolution

I and Q samples only have 13 bits resolution even though they occupy 16 bits space in radio core RAM. Since they only have 13 bits resolution, the maximum and minimum value you will observe as signed integers are [4095, -4096].

To extract the I/Q data from embedded devices over UART, we need to make sure that we have enough time to flush the I/Q data before next AoA packet arrives.

To achieve this, there are two options:

  1. Increase the connection interval. In the rtls_master readme file, it's mentioned that the connection interval should be larger than 300ms to acommodate outputting all the samples.

  2. Increase the UART baurate to 2x, 4x or 8x 115200.

    To achieve this, navigate to source/ti/blestack/npi/src/unified/npi_task.c::uint8_t NPITask_Params_init(uint8_t portType, NPI_Params *params) and add the following under the #if defined(NPI_USE_UART)

      params->portParams.uartParams.baudrate = 4 * 115200;
    

    Change baudrate to 4x 115200

In this lab we will increase connection interval to 500ms and leave the baurate as is. The connection interval can be controlled by a parameter that is passed into the connect API.

Change the following parameter in the rtls_example.py to 400.

# connection interval in units of 1.25msec configured in connection request, default is 400 (500ms)
conn_interval = 400

This parameter will later be used in the connect API as shown below

master_node.rtls.connect(address_type, address, conn_interval)

Post Processing on Embedded Device

For users that will do I/Q data post process on chip, there is no limitation on the connection interval.

Then we will build on top of the python script that is used in Realtime Localization System Introduction

First we create a csv file to store I/Q data for analyzing later if needed. You can change the filename to whichever suits you better.

import csv
from collections import namedtuple

# prepare csv file to save data
filename = 'sla_rtls_raw_IQ_toggles.csv'
outfile = open(filename, 'w', newline='')

csv_fieldnames = ['pkt', 'sample_idx', 'rssi', 'ant_array', 'channel', 'i', 'q']
csv_writer = csv.DictWriter(outfile, fieldnames=csv_fieldnames)
SampleRow = namedtuple('CsvRow', csv_fieldnames)
dump_rows = []
pkt_limit = 5
pkt_cnt = 0

csv_writer.writeheader()

Create a csv file to log I/Q data

We need to start the setup of AoA parameters and start AoA once the slave has connected to the master.

To extract I/Q data, the AoA operation mode needs to be AOA_MODE_RAW. When using rtls_example.py, you need to modify the aoa_run_mode to the following:

aoa_run_mode = 'AOA_MODE_RAW'

Change the code of rtls_example.py to enable AOA and disable TOF.

tof_supported = False
aoa_supported = True

This is the mode that is used after a connection has been established.

if msg.command == 'RTLS_CMD_CONNECT' and msg.type == 'AsyncReq':
    if msg.payload.status == 'RTLS_SUCCESS':
        if aoa_supported:
            # Find the role based on capabilities of sending node
            role = 'AOA_MASTER' if sending_node.capabilities.get('RTLS_MASTER',
                                                                 False) else 'AOA_PASSIVE'
            # Send AoA params
            sending_node.rtls.aoa_set_params(role,
                                                aoa_run_mode,
                                                aoa_cte_scan_ovs,
                                                aoa_cte_offset,
                                                aoa_cte_length)
    else:
        # If the connection failed, keep scanning
        master_node.rtls.scan()

In order to process the RAW IQ samples, we need to first calculate how many samples a connection event will produce. By migrating some of the code from AOA.c to Python, we can calculate how many IQ samples will be produced during a connection event for different oversampling rates.

# This the max number of samples that can be stored in the RF Core RAM
AOA_RES_MAX_SIZE = 511
# Note this is a direct port of AOA.c::AOA_calcNumOfCteSamples
def num_iqsamples_per_evt(cte_scan_ovs, cte_offset, cte_time):
    samp_per_evt = (((cte_time * 8) - cte_offset) * cte_scan_ovs)

    if samp_per_evt > AOA_RES_MAX_SIZE:
        samp_per_evt = AOA_RES_MAX_SIZE

    return samp_per_evt

When initializing AOA variables, we can set the number of samples per event

aoa_iq_samples_per_ce = num_iqsamples_per_evt(aoa_cte_scan_ovs, aoa_cte_offset, aoa_cte_time)

For a refresher on the AOA parameters used above and how CTE sampling works, refer to the BLE-Stack User's Guide, see RTLS Toolbox > Angle of Arrival chapter.

We have now calculated the number of IQ samples that are generated per event. Because of the size of the IQ pairs, they are fragmented before being sent over UART. The code below will re-assemble each connection event's IQ samples, sort them and dump them to a CSV file. This will continue for a number of connection events specified by pkt_limit (default = 5), but you can disable the limitation by setting it to None.

# Saving I/Q samples into csv file
if msg.command == 'RTLS_CMD_AOA_RESULT_RAW':
    payload = msg.payload
    # Extract first sample index in this payload
    offset = payload.offset

    # If we have data, and offset is 0, we are done with one dump
    if offset == 0 and len(dump_rows):
        pkt_cnt += 1

    # Make sure the samples are in order
    dump_rows = sorted(dump_rows, key=lambda sample: sample.sample_idx)

    # Write to file when we collected all IQ samples
    if len(dump_rows) == aoa_iq_samples_per_ce:
        for sample_row in dump_rows:
            csv_writer.writerow(sample_row._asdict())

        # Reset payload storage
        dump_rows = []

    # Stop script now if there was a limit configured
    if pkt_limit is not None and pkt_cnt > pkt_limit:
        break

    # Save samples for writing when dump is complete
    for sub_idx, sample in enumerate(payload.samples):
        sample = SampleRow(pkt=pkt_cnt, sample_idx=offset + sub_idx, rssi=payload.rssi,
                           ant_array=payload.antenna, channel=payload.channel, i=sample.i, q=sample.q)
        dump_rows.append(sample)

Extract I/Q data and write to a csv file

After running the script, you can see the following format in the csv file.

Here we are only interested in the payload part of the AOA_MODE_RAW command. The AOA_MODE_RAW payload has the following structure. In the python script provided above, we have extracted most of the information and save them to a csv file.

  struct = Struct(
      "rssi" / Int8sl,
      "antenna" / Int8ul,
      "channel" / Int8ul,
      "offset" / Int16ul,
      "samplesLength" / Int16ul,
      "samples" / GreedyRange(Struct(
          "q" / Int16sl,
          "i" / Int16sl,
      )),
  )

New Python Packages

For the script below you will have to install the following new Python packages

  • pandas
  • matplotlib

They can be installed with pip. Consult the RTLS Intro lab for more information on how to install packages from pip.

import matplotlib.pyplot as plt
import pandas as pd
import math

# This the max number of samples that can be stored in the RF Core RAM
AOA_RES_MAX_SIZE = 511
# Note this is a direct port of AOA.c::AOA_calcNumOfCteSamples
def num_iqsamples_per_evt(cte_scan_ovs, cte_offset, cte_time):
    samp_per_evt = (((cte_time * 8) - cte_offset) * cte_scan_ovs)

    if samp_per_evt > AOA_RES_MAX_SIZE:
        samp_per_evt = AOA_RES_MAX_SIZE

    return samp_per_evt

def cal_magnitude(q_value,i_value):

    return math.sqrt(math.pow(q_value,2)+math.pow(i_value,2))

def cal_phase(q_value,i_value):

    return math.degrees(math.atan2(q_value,i_value))

if __name__ == "__main__":
    df = pd.read_csv('sla_rtls_raw_IQ_toggles.csv')
    aoa_cte_scan_ovs = 4
    aoa_cte_offset = 4
    aoa_cte_time = 20
    aoa_iq_samples_per_ce = num_iqsamples_per_evt(aoa_cte_scan_ovs, aoa_cte_offset, aoa_cte_time)

    df['phase'] = df.apply(lambda row: cal_phase(row['q'], row['i']), axis=1)
    df['magnitude'] = df.apply(lambda row: cal_magnitude(row['q'], row['i']), axis=1)

    # Plot all the I/Q collected. Each channel will have a plot which contains I/Q samples.
    # If you have collected I/Q data on 37 data channels, then there will be 37 windows popped up
    grouped = df.groupby('channel')
    axes = grouped[['i', 'q']].plot(title="I/Q samples", grid=True)

    # Create 4 plots and each plot has x number of subplots. x = number of channels
    indexed = df.set_index(['channel', 'sample_idx'])
    indexed.unstack(level=0)[['phase']].plot(subplots=True, title="Phase information", xlim=[0,aoa_iq_samples_per_ce], ylim=[-190,+190])
    indexed.unstack(level=0)[['magnitude']].plot(subplots=True, title="Signal magnitude", xlim=[0,aoa_iq_samples_per_ce])
    indexed.unstack(level=0)[['i']].plot(subplots=True, title="I samples", xlim=[0,aoa_iq_samples_per_ce])
    indexed.unstack(level=0)[['q']].plot(subplots=True, title="Q samples", xlim=[0,aoa_iq_samples_per_ce])
    plt.show()

This script can be executed as is.

After executing the small script provided above, if the angle between rtls_passive rtls_slave is not 0 degree, you can see that magnitude of the sine wave is not the same when you swap betwen antenna 1 and antenna 2 as shown below.

Another alternative to observe the magnitude of received signal is to calculate it based on I/Q data. Since each I/Q pair is a vector, the magnitude of a vector can be calculated by sqrt(I^2+Q^2).

Using the script provided above, you will see a plot called Signal magnitude. In this plot, you can clear see that received signal magnitude from antenna 2 is almost double as from antenna 1.

More information!

If there is no antenna toggling, then the I/Q samples will form a perfect sine wave. To prove it, change the antenna toggling pattern from 2 antennas to 1 antenna(A1.2), and see how the I/Q plots look like.

AoA_Pattern antennaPattern_A1 = {
    .numPatterns = 32,
    .initialPattern = AOA_A1_SEL | AOA_Ax_ANT2,
    .toggles =
    {
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2

     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2

     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2

     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2

     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2

     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
     AOA_A1_SEL | AOA_Ax_ANT2, // A1.2
    }
};

Task 5 – Antenna Switch Settling Time

Now that we are equipped with all the needed tools to manipulate I/Q data, we will try to identify when the antenna is toggling in order to help determine which I/Q samples can be used.

As mentioned in Calculate the phase difference among the antennas, I/Q samples can be presented with constellation diagram, each I/Q pair is a vector and its angle is within a range of +180 ~ -180. Therefore when we have an I/Q pair, to obtain the angle information, we can use arctan to get angle of a vector. Then based on the I and Q value, we can find out the corresponding angle.

I > 0 I < 0
Q >=0 angle = arctan(Q/I) angle = 180 + arctan(Q/I)
Q < 0 angle = arctan(Q/I) angle = -180 + arctan(Q/I)

Luckily in python, the math.atan2 function takes care of the aforementioned logic.

Let's take a look at the Phase Information plot.

A perfect sine wave, assuming it starts at 0 degree, the phase will first go towards +180 and then, once it crosses +180, it will start from -180 and then go back to 0 degrees. From the picture provided below, you can see that in the first 8us(32 samples), there is no abrupt phase change.

When the rf switches and the angle of incident wave is not 0 degree, you will see abrupt phase change. As shown below after 2 periods, we started to switch antennas. Then the phase we obtained is no long linear.

Hence by looking at the phase information plot, you will know how many I/Q samples you can keep per period.

#
#  Copyright (c) 2018-2019, Texas Instruments Incorporated
#  All rights reserved.
#
#  Redistribution and use in source and binary forms, with or without
#  modification, are permitted provided that the following conditions
#  are met:
#
#  *  Redistributions of source code must retain the above copyright
#     notice, this list of conditions and the following disclaimer.
#
#  *  Redistributions in binary form must reproduce the above copyright
#     notice, this list of conditions and the following disclaimer in the
#     documentation and/or other materials provided with the distribution.
#
#  *  Neither the name of Texas Instruments Incorporated nor the names of
#     its contributors may be used to endorse or promote products derived
#     from this software without specific prior written permission.
#
#  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
#  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
#  THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
#  PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
#  CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
#  EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
#  PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
#  OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
#  WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
#  OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
#  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
#

import queue
import time
from rtls import RTLSManager, RTLSNode
import csv
from collections import namedtuple

# Un-comment the below to get raw serial transaction logs
# import logging, sys
# logging.basicConfig(stream=sys.stdout, level=logging.DEBUG,
#                     format='[%(asctime)s] {%(filename)s:%(lineno)d} %(levelname)s - %(message)s')



# This the max number of samples that can be stored in the RF Core RAM
AOA_RES_MAX_SIZE = 511
# Note this is a direct port of AOA.c::AOA_calcNumOfCteSamples
def num_iqsamples_per_evt(cte_scan_ovs, cte_offset, cte_time):
    samp_per_evt = (((cte_time * 8) - cte_offset) * cte_scan_ovs)

    if samp_per_evt > AOA_RES_MAX_SIZE:
        samp_per_evt = AOA_RES_MAX_SIZE

    return samp_per_evt

if __name__ == '__main__':
    # Initialize, but don't start RTLS Nodes to give to the RTLSManager
    my_nodes = [RTLSNode('COM8', 115200), RTLSNode('COM81', 115200)]

    # Initialize references to the connected devices
    master_node = None
    passive_nodes = []
    # Initialize references to the connected devices
    address = None
    address_type = None

    # ToF related settings
    samples_per_burst = 256 # Should be dividable by 16. Hint: in a 100ms interval, there are about 300~ samples
    tof_freq_list = [2408, 2412, 2418, 2424] #Other options: 2414, 2420
    tof_num_freq = len(tof_freq_list)
    auto_tof_rssi = -55

    # Select tof_sample_mode TOF_MODE_DIST or TOF_MODE_RAW
    tof_sample_mode = 'TOF_MODE_DIST'
    tof_run_mode = 'TOF_MODE_CONT'
    seed = 0
    samplesPerFreq = 1000
    calibDistance = 1 # 1 meter
    constSyncwords = False

    # AoA related settings
    aoa_run_mode = 'AOA_MODE_RAW'
    aoa_cte_scan_ovs = 4
    aoa_cte_offset = 4
    aoa_cte_time = 20
    aoa_iq_samples_per_ce = num_iqsamples_per_evt(aoa_cte_scan_ovs, aoa_cte_offset, aoa_cte_time)

    print("IQ samples per Connection event: " + str(aoa_iq_samples_per_ce))

    # Auto detect AoA or ToF support related
    tof_supported = False
    aoa_supported = True

    # If slave addr is None, the script will connect to the first RTLS slave
    # that it found. If you wish to connect to a specific device
    # (in the case of multiple RTLS slaves) then you may specify the address
    # explicitly as given in the comment to the right
    slave_addr = None  # '54:6C:0E:83:3F:3D'

    # Scan list
    scanResultList = list()

    # prepare csv file to save data
    filename = 'sla_rtls_raw_IQ_toggles.csv'
    outfile = open(filename, 'w', newline='')

    csv_fieldnames = ['pkt', 'sample_idx', 'rssi', 'ant_array', 'channel', 'i', 'q']
    csv_writer = csv.DictWriter(outfile, fieldnames=csv_fieldnames)
    SampleRow = namedtuple('CsvRow', csv_fieldnames)
    dump_rows = []
    pkt_limit = 5
    pkt_cnt = 0

    csv_writer.writeheader()


    # connection interval in units of 1.25msec configured in connection request, default is 80 (100ms)
    conn_interval = 400

    # Initialize manager reference, because on Exception we need to stop the manager to stop all the threads.
    manager = None
    try:
        # Start an RTLSManager instance without WebSocket server enabled
        manager = RTLSManager(my_nodes, websocket_port=None)
        # Create a subscriber object for RTLSManager messages
        subscriber = manager.create_subscriber()
        # Tell the manager to automatically distribute connection parameters
        manager.auto_params = True
        # Start RTLS Node threads, Serial threads, and manager thread
        manager.start()

        # Wait until nodes have responded to automatic identify command and get reference
        # to single master RTLSNode and list of passive RTLSNode instances
        master_node, passive_nodes, failed = manager.wait_identified()

        if len(failed):
            print(f"ERROR: {len(failed)} nodes could not be identified. Are they programmed?")

        # Exit if no master node exists
        if not master_node:
            raise RuntimeError("No RTLS Master node connected")

        # Combined list for lookup
        all_nodes = passive_nodes + [master_node]

        # Initialize application variables on nodes
        for node in all_nodes:
            node.tof_initialized = False
            node.seed_initialized = False
            node.aoa_initialized = False
            node.tof_calibration_configured = False
            node.tof_calibrated = False
            node.tof_started = False

        #
        # At this point the connected devices are initialized and ready
        #

        # Display list of connected devices and their capabilities
        print(f"{master_node.identifier} {', '.join([cap for cap, available in master_node.capabilities.items() if available])}")

        # Iterate over Passives and detect their capabilities
        for pn in passive_nodes:
            print(f"{pn.identifier} {', '.join([cap for cap, available in pn.capabilities.items() if available])}")

        # Check over aggregated capabilities to see if they make sense
        capabilities_per_node = [[cap for cap, avail in node.capabilities.items() if avail] for node in all_nodes]
        tof_supported = all('TOF_PASSIVE' in node_caps or 'TOF_MASTER' in node_caps for node_caps in capabilities_per_node)

        # Assume AoA if all nodes are not ToF
        aoa_supported = all(not ('TOF_PASSIVE' in node_caps or 'TOF_MASTER' in node_caps) for node_caps in capabilities_per_node)

        # Check that Nodes all must be either AoA or ToF
        if not (tof_supported or aoa_supported):
            raise RuntimeError("All nodes must be either AoA or ToF")

        # Need at least 1 passive for AoA
        if aoa_supported and len(passive_nodes) == 0:
            raise RuntimeError('Need at least 1 passive for AoA')

        # Send an example command to each of them, from commands listed at the bottom of rtls/ss_rtls.py
        for n in all_nodes:
            n.rtls.identify()

        while True:
            # Get messages from manager
            try:
                identifier, msg_pri, msg = subscriber.pend(block=True, timeout=0.05).as_tuple()

                # Get reference to RTLSNode based on identifier in message
                sending_node = manager[identifier]

                if sending_node in passive_nodes:
                    print(f"PASSIVE: {identifier} --> {msg.as_json()}")
                else:
                    print(f"MASTER: {identifier} --> {msg.as_json()}")

                # If we received an error, print it.
                if msg.command == 'RTLS_EVT_ERROR':
                    print(f"Received RTLS_EVT_ERROR with status: {msg.payload.status}")

                # If we received an assert, print it.
                if msg.command == 'RTLS_EVT_ASSERT' and msg.type == 'AsyncReq':
                    raise RuntimeError(f"Received HCI H/W Assert with code: {msg.payload.cause}")


                # After identify is received, we start scanning
                if msg.command == 'RTLS_CMD_IDENTIFY':
                    master_node.rtls.scan()

                # Once we start scaning, we will save the address of the
                # last scan response
                if msg.command == 'RTLS_CMD_SCAN' and msg.type == 'AsyncReq':
                    # Slave address none means that we connect to any slave
                    if slave_addr is None:
                        address = msg.payload.addr
                        address_type = msg.payload.addrType
                    else:
                        scanResultList.append(msg.payload.addr)
                        scanResultList.append(msg.payload.addrType)

                # Once the scan has stopped and we have a valid address, then
                # connect
                if msg.command == 'RTLS_CMD_SCAN_STOP':
                    if slave_addr is None:
                        if address is not None and address_type is not None:
                            master_node.rtls.connect(address_type, address, conn_interval)
                    elif slave_addr in scanResultList:
                        i = scanResultList.index(slave_addr)
                        master_node.rtls.connect(scanResultList[i + 1], scanResultList[i], conn_interval)
                        scanResultList.clear()
                    else:
                        # If we didn't find the device, keep scanning.
                        master_node.rtls.scan()

                if msg.command == 'RTLS_CMD_CONNECT' and msg.type == 'AsyncReq':
                  if msg.payload.status == 'RTLS_SUCCESS':
                      if aoa_supported:
                          # Find the role based on capabilities of sending node
                          role = 'AOA_MASTER' if sending_node.capabilities.get('RTLS_MASTER',
                                                                               False) else 'AOA_PASSIVE'
                          # Send AoA params
                          sending_node.rtls.aoa_set_params(role,
                                                              aoa_run_mode,
                                                              aoa_cte_scan_ovs,
                                                              aoa_cte_offset,
                                                              aoa_cte_time)
                  else:
                      # If the connection failed, keep scanning
                      master_node.rtls.scan()

                # Count the number of nodes that have ToF initialized
                if msg.command == 'RTLS_CMD_TOF_SET_PARAMS' and msg.payload.status == 'RTLS_SUCCESS':
                    sending_node.tof_initialized = True

                    if not passive_nodes:
                        if tof_sample_mode == 'TOF_MODE_DIST':
                            master_node.rtls.tof_calib(True, samplesPerFreq, calibDistance)
                        else:
                            # If we are not in TOF_MODE_DIST we can start immediately
                            master_node.rtls.tof_start(True)
                            master_node.tof_started = True
                    else:
                        # If all nodes have responded then we are ready to move on
                        if all([n.tof_initialized for n in all_nodes]):
                            # Send request for seed to master
                            master_node.rtls.tof_get_sec_seed()

                if msg.command == 'RTLS_CMD_AOA_SET_PARAMS' and msg.payload.status == 'RTLS_SUCCESS':
                    sending_node.aoa_initialized = True
                    if all([n.aoa_initialized for n in all_nodes]):
                        # Start AoA on the master and passive nodes
                        for node in all_nodes:
                            node.rtls.aoa_start(True)

                # Wait for security seed
                if msg.command == 'RTLS_CMD_TOF_GET_SEC_SEED' and msg.payload.seed is not 0:
                    seed = msg.payload.seed
                    for node in passive_nodes:
                        node.rtls.tof_set_sec_seed(seed)

                # Wait until passives have security seed set
                if msg.command == 'RTLS_CMD_TOF_SET_SEC_SEED' and msg.payload.status == 'RTLS_SUCCESS':
                    sending_node.seed_initialized = True

                    # Only need to calibrate in distance mode
                    if tof_sample_mode == 'TOF_MODE_DIST':
                        if sending_node in passive_nodes:
                            sending_node.tof_calibration_configured = True
                            sending_node.rtls.tof_calib(True, samplesPerFreq, calibDistance)

                        # Once all passives have calibration configured, we can configure master
                        if all([n.tof_calibration_configured for n in passive_nodes]):
                            # Master will do infinite calibration until passive is done
                            master_node.rtls.tof_calib(True, 0, calibDistance)
                    else:
                        # If we are not in TOF_MODE_DIST we can start immediately
                        if sending_node in passive_nodes:
                            sending_node.rtls.tof_start(True)
                            sending_node.tof_started = True

                        # Passives must start well before Master does since they must "hear" the first ToF exchange
                        if all([n.tof_started for n in passive_nodes]):
                            master_node.rtls.tof_start(True)
                            master_node.tof_started = True

                if msg.command == 'RTLS_CMD_TOF_CALIBRATE' and msg.type == 'SyncRsp':
                        if sending_node in passive_nodes:
                            sending_node.rtls.tof_start(True)
                            sending_node.tof_started = True

                            # Passives must start well before Master does since they must "hear" the first ToF exchange
                            if all([n.tof_started for n in passive_nodes]):
                                master_node.rtls.tof_start(True)
                                master_node.tof_started = True
                        else:
                            if not passive_nodes:
                                master_node.rtls.tof_start(True)
                                master_node.tof_started = True

                if msg.command == 'RTLS_CMD_TOF_CALIBRATE' and msg.type == 'AsyncReq':
                    if sending_node in passive_nodes:
                        sending_node.tof_calibrated = True

                        # Once all nodes are calibrated we can stop master calibration
                        if all([n.tof_calibrated for n in passive_nodes]):
                            master_node.rtls.tof_calib(False, 0, calibDistance)

                # Saving I/Q samples into csv file
                if msg.command == 'RTLS_CMD_AOA_RESULT_RAW':
                    payload = msg.payload
                    # Extract first sample index in this payload
                    offset = payload.offset

                    # If we have data, and offset is 0, we are done with one dump
                    if offset == 0 and len(dump_rows):
                        pkt_cnt += 1

                    # Make sure the samples are in order
                    dump_rows = sorted(dump_rows, key=lambda sample: sample.sample_idx)

                    # Write to file when we collected all IQ samples
                    if len(dump_rows) == aoa_iq_samples_per_ce:
                        for sample_row in dump_rows:
                            csv_writer.writerow(sample_row._asdict())

                        # Reset payload storage
                        dump_rows = []

                    # Stop script now if there was a limit configured
                    if pkt_limit is not None and pkt_cnt > pkt_limit:
                        break

                    # Save samples for writing when dump is complete
                    for sub_idx, sample in enumerate(payload.samples):
                        sample = SampleRow(pkt=pkt_cnt, sample_idx=offset + sub_idx, rssi=payload.rssi,
                                           ant_array=payload.antenna, channel=payload.channel, i=sample.i, q=sample.q)
                        dump_rows.append(sample)


            except queue.Empty:
                pass

    finally:
        outfile.flush()
        outfile.close()

        if manager:
            manager.stop()
Creative Commons License
This work is licensed under a Creative Commons Attribution-NonCommercial-NoDerivatives 4.0 International License.