Example Summary
The Packet TX example illustrates how to do simple packet transmission using the RF driver. This example is meant to be used with the Packet RX example or SmartRF Studio. For every packet transmitted, Board_PIN_LED1 is toggled. The frequency and other RF settings can be modified using SmartRF Studio.
Peripherals Exercised
Board_PIN_LED1- Toggled when data is transmitted over the RF interface
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433
- 433.92 MHz for the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNXHL
- 868.0 MHz for other launchpads In order to change frequency, modify the smartrf_settings.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default. The user must set USE_SUB1_HIGH_PA_SETTING to 0 in smartrf_settings.h and smartrf_settings_predefined.h, and rebuild the example, to disable the high PA and use the default PA
- On the CC1352P-2 the high PA operation for Sub-1 GHz modes is not supported
- On the CC1352P-4 the default PA is used for all Sub-1 GHz physical modes by default. The user must set USE_SUB1_HIGH_PA_SETTING to 1 in the smartrf_settings.h and smartrf_settings_predefined.h, and rebuild the example, to enable the high PA (high output power) CAUTION
- This will change the center frequency for 2-GFSK to 490 MHz
- The center frequency for SimpleLink long range (SLR) stays at 433.92 MHz, but the high output power violates the maximum power output requirement for this band
- This will change the center frequency for 2-GFSK to 490 MHz
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Example Usage
Run the example. On another board, run the Packet RX example. Board_PIN_LED1 is toggled when data is transmitted.
Application Design Details
This examples consists of a single task and the exported SmartRF Studio radio settings.
When the task is executed it:
- Configures the radio for Proprietary mode
- Gets access to the radio via the RF drivers RF_open
- Sets up the radio using CMD_PROP_RADIO_DIV_SETUP command
- Set the output power to 14 dBm (requires that CCFG_FORCE_VDDR_HH = 1 in ccfg.c), this requirement holds for CC13x2P boards when using the default PA
- Sets the frequency using CMD_FS command
- Create packet (with increasing sequence number and random content)
- Transmit packet using CMD_PROP_TX command with blocking RF driver call
- Toggle Board_PIN_LED1 to indicate packet transmitted
- Power down the radio using the yield function
- Set the main core to sleep for the duration of
PACKET_INTERVALms - Transmit packets forever by repeating step 6-10
Note for IAR users: When using the CC1310DK, the TI XDS110v3 USB Emulator must be selected. For the CC1310_LAUNCHXL, select TI XDS110 Emulator. In both cases, select the cJTAG interface.