References¶
TI 15.4-Stack CoP Interface Guide
ARM Cortex-M3 Devices Generic User’s Guide
Terms and Acronyms¶
TI 15.4-Stack Terms and Acronyms¶
- CCFG
- Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
- IDE
- Integrated Development Environment
- CCS
- Code Composer Studio
- HIB
- Halt In Boot. A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- IAR
- IAR Systems
- MCU
- Microcontroller Unit
- OOB
- Out-Of-Box
- PIB
- Personal-Area-Network Information Bases
- RCFG
- TI-RTOS in ROM Configuration Table
- ROM
- Read-only Memory
- RAM
- Random Access Memory
- RF
- Radio Frequency
- NV
- Non-Volatile Memory
- DFE
- Direct Frame Exchange
- IEEE
- Institute of Electrical and Electronics Engineers
- PHY
- Physical layer of the OSI model
- OSI
- Open Systems Interconnection model
- MAC
- Medium Access Control
- SUN
- Smart Utility Network
- FAN
- Field Area Network
- PAN
- Personal Area Network
- CSMA/CA
- Carrier Sense Multiple Access with Collision Avoidance. This prevents nodes from talking while the air is occupied. Used in all bands except 868MHz
- LBT
- Listen Before Talk. This prevents nodes from talking while the air is occupied. Used in 868MHz band.
- DH1CF
- Direct Hash Channel Function. This is used to produce a psuedo-random channel sequence for frequency hopping devices.
- SNV
- Simple Non-Volatile storage
- ICALL
- Indirect Call
- RTOS
- Real Time Operating System
- FFD
- Full Functionality Device
- RFD
- Reduced Functionality Device
- CLI
- Command Line Interface
- GUI
- Graphical User Interface
- JTAG
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
- cJTAG
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
- VIMS
- A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x0 Technical Reference Manual.
Dynamic Multi-protocol Manager Terms and Acronyms¶
- Dynamic Multi-protocol Manager
- DMM
- An arbiter between multiple protocol stacks that are sharing the multi mode RF driver and thus the radio. The DMM aides in scheduling radio operations by way of application provided state information and timing constraints.
Sensor Controller Terms and Acronyms¶
- SC
- Sensor Controller
- SCS
- Sensor Controller Studio
TI-RTOS Terms and Acronyms¶
- Hwi
- A TI-RTOS Hardware interrupt.
- Idle Task
- A TI-RTOS default task that is executes when no other higher priority thread needs to run.
- ROV
- Runtime Object View
- A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
- RTC
- Real-time Clock
- RTSC
- Real Time Software Componenets. A toolset for creating reusable code, used by TI-RTOS.
- Swi
- A TI-RTOS Software interrupt.
- TI-RTOS
- Texas Instruments Real Time Operating System
- Zero-Latency Interrupts
- An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see this wiki article.
Over the Air Download (OAD) Terms and Acronyms¶
- BIM
- Boot Image Manager
- A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
- CRC
- Cyclic Redundancy Check
- An error-detecting code used to check the integrity of blocks of data.
- ECDSA
- Elliptic Curve Digital Signature Algorithm
- A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography.
- Factory Image
- The factory image is a “golden” image that resides in external flash as a failsafe mechanism.
- HIB
- Halt In Boot. A mechanism in CC26xx and CC13xx devices to ensure that the external emulator can take control of the device before it executes any application code.
- OAD
- Over the Air Download
- The process of performing a device firmware update over the air.
- OAD Target
- The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx device running the TI protocol specific transport for OAD.
- OAD Distributor
- The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.