adcbufcontinuous
Example Summary
Example that uses the ADCBuf driver to make a number of samples and echo them via UART. This example shows how to initialize the ADCBuf driver in continuous mode.
Peripherals Exercised
Board_ADCBUF0- Buffer instance used to manage samples from ADCBuf channel.Board_ADCBUF0CHANNEL0- ADCBuf channel 0.Board_UART0- Used to echo samples to host serial session.
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
- Connect the ADC channel to a sampling source.
- For quick testing, connect
Board_ADCBUF0CHANNEL0toGNDor3V3.
- For quick testing, connect
Important: Caution should be used when connecting the pins to analog inputs greater than 3VDC.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
The target will send packages of 50 samples and a header to the serial session. Adjusted raw values and microvolt values are displayed on respective new lines.
Application Design Details
A single task sets up the UART connection to the serial console and starts a continuous conversion with the ADCBuf driver. After this is completed, the task sleeps forever.
- The ADCBuf driver performs 50 samples at 200 Hz each.
- The driver supports higher sampling rates; however, 200 Hz was chosen for easily interpretable output. The maximum sampling rates are device specific.
The callback function
adcBufCallbackis called whenever an ADC buffer is full. The contents of the buffer are first adjusted so that raw results are comparable between devices of the same make. The adjusted values are then converted into microvolts to be human-readable. Lastly, both the adjusted and microvolt values are displayed via UART.
TI-RTOS:
- When building in Code Composer Studio, the kernel configuration project will be imported along with the example. The kernel configuration project is referenced by the example, so it will be built first. The “release” kernel configuration is the default project used. It has many debug features disabled. These feature include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” kernel configurations and how to switch between them, please refer to the SimpleLink MCU SDK User’s Guide. The “release” and “debug” kernel configuration projects can be found under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.