TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
HCI Function Maps

HCI Function Mapping

This section lists the mapping between stack APIs and function names, as described in the BT core spec. The App column indicates if the command can be called by the application where Y means yes and N means no.

API Function Map
Stack API BT Function App
HCI_DisconnectCmd Disconnect Command N
HCI_HostNumCompletedPktCmd Host Number Of Completed Packets Command N
HCI_LE_AddDeviceToResolvingListCmd LE Add Device to Resolving List Command N
HCI_LE_AddWhiteListCmd LE Add Device To White List Command Y
HCI_LE_ClearWhiteListCmd LE Clear White List Command Y
HCI_LE_ConnUpdateCmd LE Connection Update Command N
HCI_LE_CreateConnCancelCmd LE Create Connection Cancel Command N
HCI_LE_CreateConnCmd LE Create Connection Command N
HCI_LE_EncryptCmd LE Encrypt Command Y
HCI_LE_GenerateDHKeyCmd LE Generate DHKey Command N
HCI_LE_LtkReqNegReplyCmd LE Long Term Key Request Negative Reply Command N
HCI_LE_LtkReqReplyCmd LE Long Term Key Request Reply Command N
HCI_LE_RandCmd LE Rand Command N
HCI_LE_ReadAdvChanTxPowerCmd Read Transmit Power Level Command Y
HCI_LE_ReadBufSizeCmd LE Read Buffer Size Command N
HCI_LE_ReadChannelMapCmd LE Read Channel Map Command Y
HCI_LE_ReadLocalP256PublicKeyCmd LE Read Local P-256 Public Key Command N
HCI_LE_ReadLocalResolvableAddressCmd LE Read Local Resolvable Address Command N
HCI_LE_ReadLocalSupportedFeaturesCmd Read Local Supported Commands Command Y
HCI_LE_ReadMaxDataLenCmd Set Event Mask Command Y
HCI_LE_ReadPeerResolvableAddressCmd LE Read Peer Resolvable Address Command N
HCI_LE_ReadRemoteUsedFeaturesCmd LE Read Remote Used Features Command Y
HCI_LE_ReadResolvingListSizeCmd LE Read Resolving List Size Command N
HCI_LE_ReadSuggestedDefaultDataLenCmd LE Read Suggested Default Data Length Command Y
HCI_LE_ReadSupportedStatesCmd LE Read Supported States Command Y
HCI_LE_ReadWhiteListSizeCmd LE Read White List Size Command Y
HCI_LE_RemoteConnParamReqNegReplyCmd LE Remote Connection Parameter Request Negative Reply Command N
HCI_LE_RemoteConnParamReqReplyCmd LE Remote Connection Parameter Request Reply Command N
HCI_LE_RemoveDeviceFromResolvingListCmd LE Remove Device From Resolving List Command N
HCI_LE_RemoveWhiteListCmd LE Remove Device From White List Command Y
HCI_LE_SetAddressResolutionEnableCmd LE Set Address Resolution Enable Command N
HCI_LE_SetAdvDataCmd LE Set Advertising Data Command N
HCI_LE_SetAdvEnableCmd LE Set Advertise Enable Command N
HCI_LE_SetDataLenCmd LE Set Data Length Command Y
HCI_LE_SetEventMaskCmd LE Set Event Mask Command Y
HCI_LE_SetHostChanClassificationCmd LE Set Host Channel Classification Command Y
HCI_LE_SetRandomAddressCmd LE Set Random Address Command N
HCI_LE_SetResolvablePrivateAddressTimeoutCmd LE Set Resolvable Private Address Timeout Command N
HCI_LE_SetScanEnableCmd LE Set Scan Enable Command N
HCI_LE_SetScanParamCmd LE Set Scan Parameters Command N
HCI_LE_SetAdvDataCmd LE Set Advertising Data Command N
HCI_LE_SetAdvEnableCmd LE Set Advertise Enable Command N
HCI_LE_SetAdvParamCmd LE Set Advertising Parameters Command N
HCI_LE_SetScanRspDataCmd LE Set Scan Response Data Command N
HCI_LE_StartEncyptCmd LE Start Encryption Command N
HCI_LE_TestEndCmd LE Test End Command Y
HCI_LE_TransmitterTestCmd LE Transmitter Test Command Y
HCI_LE_WriteSuggestedDefaultDataLenCmd LE Write Suggested Default Data Length Command Y
HCI_ReadAuthPayloadTimeoutCmd Read Authenticated Payload Timeout Command N
HCI_ReadBDADDRCmd Read BD_ADDR Command Y
HCI_ReadLocalSupportedCommandsCmd Read Local Supported Commands Command Y
HCI_ReadLocalSupportedFeaturesCmd Read Local Supported Features Command Y
HCI_ReadLocalVersionInfoCmd Read Local Version Information Command Y
HCI_ReadRemoteVersionInfoCmd Read Remote Version Information Command Y
HCI_ReadRssiCmd Read RSSI Command Y
HCI_ReadTransmitPowerLevelCmd Read Transmit Power Level Command Y
HCI_ResetCmd Reset Command Y
HCI_SetEventMaskCmd Set Event Mask Command Y
HCI_SetEventMaskPage2Cmd Set Event Mask Page 2 Command Y

This section lists the mapping between stack APIs and function names, as described in the Vendor Specific API guide included with the installer.

Vendor Specific API Function Map
Stack API Vendor Specific Function
HCI_EXT_AdvEventNoticeCmd HCI Extension Advertiser Event Notice
HCI_EXT_BuildRevisionCmd HCI Extension Build Revision
HCI_EXT_DecryptCmd HCI Extension Decrypt
HCI_EXT_DisconnectImmedCmd HCI Extension Disconnect Immediate
HCI_EXT_EnablePTMCmd HCI Extension Enable PTM
HCI_EXT_EndModemTestCmd Set Event Mask Command
HCI_EXT_EndModemTestCmd HCI Extension End Modem Test
HCI_EXT_ModemHopTestTxCmd HCI Extension Modem Hop Test Transmit
HCI_EXT_ModemTestRxCmd HCI Extension Modem Test Receive
HCI_EXT_ModemTestTxCmd HCI Extension Modem Test Transmit
HCI_EXT_NumComplPktsLimitCmd HCI Extension Number Completed Packets Limit
HCI_EXT_OnePktPerEvtCmd HCI Extension One Packet Per Event
HCI_EXT_PacketErrorRateCmd HCI Extension Packet Error Rate
HCI_EXT_PERbyChanCmd HCI Extension Packet Error Rate By Channel
HCI_EXT_SaveFreqTuneCmd HCI Extension Save Frequency Tuning
HCI_EXT_ScanEventNoticeCmd HCI Extension Scan Event Notice
HCI_EXT_ScanReqRptCmd HCI Extension Scan Request Report
HCI_EXT_SetBDADDRCmd HCI Extension Set BDADDR
HCI_EXT_SetFastTxResponseTimeCmd HCI Extension Set Fast Transmit Response Time
HCI_EXT_SetFreqTuneCmd HCI Extension Set Frequency Tuning
HCI_EXT_SetLocalSupportedFeaturesCmd HCI Extension Set Local Supported Features
HCI_EXT_SetMaxDataLenCmd HCI Extension Set Max Data Length
HCI_EXT_SetMaxDtmTxPowerCmd HCI Extension Set Max DTM Transmitter Power
HCI_EXT_SetRxGainCmd HCI Extension Set Receiver Gain
HCI_EXT_SetSCACmd HCI Extension Set SCA
HCI_EXT_SetTxPowerCmd HCI Extension Set Transmitter Power
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale