90 #ifndef ti_drivers_SDFatFS__include 91 #define ti_drivers_SDFatFS__include 101 #include <third_party/fatfs/ff.h> 102 #include <third_party/fatfs/diskio.h> 147 extern SDFatFS_Handle
SDFatFS_open(uint_least8_t idx, uint_least8_t drive);
struct SDFatFS_Config_ SDFatFS_Config
SDFatFS Global configuration.
FATFS filesystem
Definition: SDFatFS.h:111
SD Global configuration.
Definition: SD.h:299
SD_Handle sdHandle
Definition: SDFatFS.h:112
uint_fast32_t driveNum
Definition: SDFatFS.h:109
SDFatFS_Handle SDFatFS_open(uint_least8_t idx, uint_least8_t drive)
Function to open a SDFatFS instance on the specified drive.
SDFatFS Global configuration.
Definition: SDFatFS.h:132
void SDFatFS_close(SDFatFS_Handle handle)
Function to close a SDFatFS instance specified by the SDFatFS handle.
void * object
Definition: SDFatFS.h:134
SDFatFS Object The application must not access any member variables of this structure! ...
Definition: SDFatFS.h:108
struct SDFatFS_Config_ * SDFatFS_Handle
A handle that is returned from a SDFatFS_open() call.
Definition: SDFatFS.h:118
struct SDFatFS_Object_ SDFatFS_Object
SDFatFS Object The application must not access any member variables of this structure! ...
DSTATUS diskState
Definition: SDFatFS.h:110