Routing RF Core Signals to Physical Pins¶
Note
Please see the CC13x0 CC26x0 SimpleLink Wireless MCU Technical Reference Manual for further documentation on these signals including limitations on devices and modes.
The various hardware units on the RF core provide 12 internal hardware signals that indicate various events. These signals are defined in Table 8..
Index | Signal identifier | Default mapping | Description |
---|---|---|---|
0 | CPE_GPO0 | RFC_GPO0 | Controls an external LNA front-end. High when the LNA must be enabled, otherwise low. |
1 | CPE_GPO1 | RFC_GPO1 | Controls an external PA. High when the PA must be enabled and otherwise low. |
2 | CPE_GPO2 | RFC_GPO2 | Goes high when the synthesizer calibration starts and low when the calibration is done. |
3 | CPE_GPO3 | n/a | |
4 | MCE_GPO0† | Binary data signal that goes to the modulator when sending. | |
5 | MCE_GPO1† | Binary data signal that comes from the demodulator when receiving. | |
6 | MCE_GPO2 | n/a | |
7 | MCE_GPO3 | n/a | |
8 | RAT_GPO0 | RFC_GPO3 | Goes high when a transmission is initiated and low when the transmission is done. Can be used for accurate timing synchronization. |
9 | RAT_GPO1* | Goes high when sync word is detected and low either when the packet has been received or reception has been aborted. If the device is in repeat mode, only the first sync word will give an assertion. Requires an additional override (uint32_t)0x008F88B3 . |
|
10 | RAT_GPO2 | General purpose RAT output. Configurable via CMD_SET_RAT_OUTPUT. | |
11 | RAT_GPO3 | General purpose RAT output. Configurable via CMD_SET_RAT_OUTPUT. |
MCE_GPO0 and MCE_GPO1†: These signals are only supported when using 2-GFSK modulation.
RAT_GPO1*: See note in Read Before Using RAT_GPO1.
Each of those 12 signals can be routed to any physical GPIO pin via the RF
core doorbell register SYSGPOCTL
. The doorbell register provides 4
outputs: RFC_GPO0
.. RFC_GPO3
. This means that at most 4 output
signals from Table 8. can be used at the same time. The
signals RFC_GPO0
.. RFC_GPO3
have a default mapping on power up.
In addition, the RF core provides two input signals: RFC_GPI0
and
RFC_GPI1
. These are tied to the radio timer on the RF core and can be
used, for instance, to trigger an RF operation command. For a usage example,
please refer to External triggers TRIG_EXTERNAL.
Read Before Using CPE_GPO1¶
On CC2640R2F, there is a bug with CPE_GPO1. Please use RAT_GPO0 instead. See the CC26xx Technical Reference Manual for more info.
Read Before Using RAT_GPO1¶
On CC2640R2F, CC1310 and CC1350, this signal is not supported when using repeat mode.
The RAT_GPO1 signal is not supported in these scenarios:
- when using the sniff command (
CMD_PROP_RX_SNIFF
orCMD_PROP_RX_ADV_SNIFF
) with preamble correlation enabled (csConf.bEnaCorr = 1
)- when using IEEE 802.15.4 RX commands.
Read Before Using MCE_GPO1¶
This signal is only supported when using 2-GFSK modulation.
The data on MCE_GPO1 tells if the received instantaneous signal frequency is below or above the expected carrier frequency, sampled at four times oversampling of the symbol rate. Note that the signal is inverted compared to normal decoding, so a received 0 is represented with a high level and a received 1 is represented with a low level. This may be inverted in the IO configuration register before it is output on a pin, if necessary.
The signal will contain both the preamble, access address, whitened data and CRC. Note that this signal is taken out of the receiver before frequency error compensation. This means that you may see either 0’s or 1’s being narrower than expected, and some bits may be lost entirely. There are other steps taken in the demodulator as well to improve reception which will not be done on this observed signal. This means that if you try to decode a packet based on this signal, you will get significantly worse sensitivity and frequency error tolerance than with the internal demodulator. Note that the signal on this pin will be noise when the receiver is on with no packet to receive (for instance before the start of the packet).
Routing internal signals to the doorbell register¶
The default mapping from Table 8. can be changed by
writing to the SYSGPOCTL
register. For instance, to map RAT_GPO2 => RFC_GPO0
and
MCE_GPO0 => RFC_GPO1
, use the following code snippet:
#include <ti/devices/${DEVICE_FAMILY}/inc/hw_rfc_dbell.h>
// Map RAT_GPO2 to RFC_GPO0
// Map MCE_GPO0 to RFC_GPO1
HWREG(RFC_DBELL_BASE + RFC_DBELL_O_SYSGPOCTL) =
RFC_DBELL_SYSGPOCTL_GPOCTL0_RATGPO2 | RFC_DBELL_SYSGPOCTL_GPOCTL1_MCEGPO0;
Please note that this can only be done when the RF core is powered up. The signal mapping on the RF core is reset on each power-up cycle. In order to apply a custom mapping automatically during power-up, apply the register change via an override instead:
#include <ti/devices/${DEVICE_FAMILY]/inc/hw_rfc_dbell.h>
// Overrides for CMD_PROP_RADIO_DIV_SETUP
static uint32_t pOverrides[] =
{
// Set the SYSGPOCTL register
HW_REG_OVERRIDE(0x1110, RFC_DBELL_SYSGPOCTL_GPOCTL0_RATGPO2 | RFC_DBELL_SYSGPOCTL_GPOCTL1_MCEGPO0),
// ...
}
Routing doorbell signals to GPIO pins¶
After the signal mapping has been established on the RF core, the doorbell GPIO signal can be routed to a physical pin or vice versa by the help of the PIN driver:
#include <ti/drivers/pin/PINCC26XX.h>
// Map RFC_GPO0 to IO 23
PINCC26XX_setMux(pinHandle, IOID_23, PINCC26XX_MUX_RFC_GPO0);
// Map IO 26 to RFC_GPI1
PINCC26XX_setMux(pinHandle, IOID_26, PINCC26XX_MUX_RFC_GPI1);
This mapping is permanent as long as the GPIO driver is initialized correctly.