# rfWsnNodeOad
SysConfig Notice
All examples will soon be supported by SysConfig, a tool that will help you graphically configure your software components. A preview is available today in the examples/syscfg_preview directory. Starting in 3Q 2019, with SDK version 3.30, only SysConfig-enabled versions of examples will be provided. For more information, click here.
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
EasyLink Stack Configuration
Many parameters of the EasyLink stack can be configured using SysConfig including RX, TX, Radio, and Advanced settings. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name. Alternatively, refer to the System Configuration Tool (SysConfig) section of the Proprietary RF User's guide found in <SDK_INSTALL_DIR>/docs/proprietary-rf/proprietary-rf-users-guide.html.
Example Summary
The WSN Node example illustrates how to create a Wireless Sensor Network Node device which sends packets to a concentrator. This example is meant to be used with the WSN Concentrator example to form a one-to-many network where the nodes send messages to the concentrator.
This examples showcases the use of several Tasks, Semaphores, and Events to get sensor updates and send packets with acknowledgement from the concentrator. For the radio layer, this example uses the EasyLink API which provides an easy-to-use API for the most frequently used radio operations.
Peripherals Exercised
Board_PIN_LED0
- Toggled when the a packet is sentBoard_ADCCHANNEL_A0
- Used to measure the Analog Light Sensor by the SCE taskBoard_PIN_BUTTON0
- Selects fast report or slow report mode. In slow report mode the sensor data is sent every 5s or as fast as every 1s if there is a significant change in the ADC reading. The fast reporting mode sends the sensor data every 1s regardless of the change in ADC value. The default is slow reporting mode.
Resources & Jumper Settings
If you're using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
- Run the example. On another board run the WSN Concentrator example. This node should show up on the LCD of the Concentrator.
The example also supports Over The Air Download (OAD), where new FW can be transferred from the concentrator to the node. There must be an OAD Server, which is included in the concentrator project, and an OAD client, which is included in the node project.
Performing an OAD Image Transfer
To be safe the external flash of the Concentrator should be wiped before running the example. To do this, program both LP boards with erase_extflash_cc13x0lp.hex. The program will flash the LEDs while erasing the external flash. Allow the application to run until the LEDs stop flashing indicating the external flash has been erased.
The FW to erase the external flash can be found in below location and should be loaded
using Uniflash programmer:
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/onChipOad/ccs/erase_extflash_cc13x0lp.hex
In addition, the internal flash of the node should be wiped to ensure no corrupt software already resides on the node. This can be done through the Settings and Utilities tab in Uniflash.
The Concentrator OAD Server and Node OAD Client FW should each be loaded into a CC1310LP/CC1350LP using the Uniflash programmer:
- Load rfWsnConcentratorOadServer (.out) project into a CC1310LP/CC1350LP
- Load
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/onChipOad/ccs/rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_all_v1.bin
into a CC1310LP/CC1350LP
The Concentrator will display the below on the UART terminal:
Nodes Value SW RSSI
*0x0b 0887 0 -080
0xdb 1036 0 -079
0x91 0940 0 -079
Action: Update available FW
Info: Available FW unknown
Use the node display to identify the corresponding node ID:
Node ID: 0x91
Node ADC Reading: 1196
The node OAD image can be loaded into the external flash of the Concentrator through
the UART with the oad_write_bin.py script. The action must first be selected using
BTN-2. Press BTN-2 until the Action is set to Update available FW
, then press BTN-1
and BTN-2 simultaneously to execute the action.
When "Available FW" is selected the terminal will display:
Waiting for Node FW update...
The UART terminal must be closed to free the COM port before the script is run. Then the python script can be run using the following command:
python <SDK>/tools/easylink/oad/oad_write_bin.py /dev/ttyS28 <SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/onChipOad/ccs/rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v2.bin
After the download the UART terminal can be re-opened and the "Info" menu line will be updated to reflect the new FW available for OAD to a node.
The current FW version running on the node can be requested using the Send FW Ver Req
action. This is done by pressing BTN-1 until the desired node is selected (indicated by
the *), then pressing BTN-2 until the Action is set to Send FW Ver Req
. To execute the
action, press BTN-1 and BTN-2 simultaneously.
The next time the node sends data to the concentrator, the FW version of the selected node will appear in the Info section.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Send FW Ver Req
Info: Node 0x91 FW v1.0
The node FW can now be updated to the image stored on the external flash of the
concentrator. Press BTN-1 until the desired node is selected, then press BTN-2 until
the Action is set to Update node FW
. To execute the action, press BTN-1 and BTN-2
simultaneously.
The next time the node sends data, the OAD sequence will begin. As the node requests each image block from the concentrator the Concentrator display is updated to show the progress of the image transfer.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update node FW
Info: OAD Block 14 of 1089
The node display also updates to show the status of the image transfer.
Node ID: 0x91
Node ADC Reading: 3093
OAD Block: 14 of 1089
OAD Block Retries: 0
Once the OAD has completed, the concentrator will indicate that the transfer has
finished with an OAD Complete
status. The node will reset itself with a new node ID.
If the device does not reset itself a manual reset may be necessary.
Generating OAD Images
For generating the images the following tools are required:
Code Composer Studio
-- Download the latest version from http://www.ti.com/tool/CCSTUDIOSimplelink CC13X0 SDK
-- Download the latest version from http://www.ti.com/tool/simplelink-cc13x0-sdkPython 2.7
Python intelhex-2.1
Python crcmod-1.7
Onchip OAD partitions the available flash into two regions denoted as Image A and Image B. The image transferred using OAD should correspond to the image region where the application is not running. For example, if Image A is loaded on the LP, then the OAD should be performed with an Image B binary. The following steps walk through how to create an application binary, a production binary, and how to modify the project to create either Image A or Image B.
Creating the BIM Image
The BIM is generated from the SDK project:
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/bim_onchip/tirtos/ccs/bim_intflash_cc13x0lp_app.projectspec
A prebuilt hex image is located in the SDK:
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/onChipOad/ccs/bim_intflash_cc13x0lp.hex
Creating the Application Image
To generate the application hex file (Image A), the project should be imported and built with the
desired compiler. To change the FW version, update the following string in native_oad/oad_client.c
#define FW_VERSION "v1.0"
The OAD binary can be created from the application hex file using the OAD image tool found in the following location:
<SDK_DIR>/tools/common/oad/oad_image_tool.py
To use the OAD image tool execute the following command:
python oad_image_tool.py -t onchip -i app -v 0x0100 -m 0x1000 -ob rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v1.bin rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v1.hex
The following command-line arguments can be must be used to build the image:
* -t onchip
selects the type of OAD between onchip and offchip
* -i app
is used to indicate the BIM is not in included, use production when the hex file also contains the BIM
* -m 0x1000
indicates the start of the image, use address -m 0x10000
for Image B
* -v 0x0100
refers to the FW version with the format 0xXXYY where XX is the major version and YY the minor version (for example 2.3 would be 0x0203).
Note: The FW Version is defined in native_oad/oad_client.c
Modifying the Project to Create Image B
The linker and compiler flags need to be updated from HAL_IMAGE_A
to HAL_IMAGE_B
to create the Image B application hex.
To update these in Code Composer Studio, navigate to Project → Properties → Build. From the Arm Compiler category update the flag set by selecting Edit Flags. Update the --define=HAL_IMAGE_A
to --define=HAL_IMAGE_B
. Update the linker flags by making the same modification from the ARM Linker category.
To update the compiler and linker flags in IAR Embedded Workbench, navigate to Options → C/C++ Compiler. From the Extra Options tab, update -DHAL_IMAGE_A
to -DHAL_IMAGE_B
. Then from the Extra Options tab under Options → Linker, update --config_def=HAL_IMAGE_A=1
to --config_def=HAL_IMAGE_B=1
.
Make sure to clean the project before building to update the linker.cmd file with the new settings
Build the project to create the application hex file for Image B. To create the application binary, use the OAD image tool and modify the -m flag as shown below.
python oad_image_tool.py -t onchip -i app -v 0x0200 -m 0x10000 -ob rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v2.bin rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v2.hex
Creating the Production Image
The production image (binary) is the image that should be flashed directly to the LP.
First, the application image (hex) is the merged with the BIM (hex) to create the production image (hex).
python /usr/bin/hexmerge.py -o rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_all_v1.hex
"--overlap=error" rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_app_v1.hex
bim_intflash_cc13x0lp.hex
The oad_image_tool creates an OAD image header that contains information used by the application and the BIM. Therefore, the oad_image_tool is used to generate an OAD production binary that contains the onchip BIM, OAD image header, and application for flashing to the device.
python oad_image_tool.py -t onchip -i production -v 0x0100 -m 0x1000 -ob
rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_all_v1.bin
rfWsnNodeIntFlashOadClient_CC1310_LAUNCHXL_all_v1.hex
The production image type (-i) is used so the oad_image_tool can accurately calculate the CRC of the image.
Application Design Details
This examples consists of two tasks, one application task and one radio protocol task. It also consists of a Sensor Controller Engine (SCE) Task which samples the ADC.
On initialization the CM3 application sets the minimum report interval and the minimum change value which is used by the SCE task to wake up the CM3. The ADC task on the SCE checks the ADC value once per second. If the ADC value has changed by the minimum change amount since the last time it notified the CM3, it wakes it up again. If the change is less than the masked value, then it does not wake up the CM3 unless the minimum report interval time has expired.
The NodeTask waits to be woken up by the SCE. When it wakes up it toggles
Board_PIN_LED1
and sends the new ADC value to the NodeRadioTask.The NodeRadioTask handles the radio protocol. This sets up the EasyLink API and uses it to send new ADC values to the concentrator. After each sent packet it waits for an ACK packet back. If it does not get one, then it retries three times. If it did not receive an ACK by then, then it gives up.
RadioProtocol.h can also be used to configure the PHY settings from the following options: IEEE 802.15.4g 50kbit (default), Long Range Mode or custom settings. In the case of custom settings, the smartrf_settings.c file is used. The configuration can be changed by exporting a new smartrf_settings.c file from Smart RF Studio or modifying the file directly.
References
- For more information on the EasyLink API and usage refer to the Proprietary RF User's guide