Stack Configurations¶
Configuring Bluetooth Low Energy Protocol Stack Features¶
The Bluetooth Low Energy protocol stack can be configured to include
or exclude certain Bluetooth Low Energy features by changing the
library configuration in the stack project. The available Bluetooth
Low Energy features are defined in the build_config.opt
file in
the Tools folder of the stack project within the IDE. Based on the
features selected in the build_config.opt
file, the lib_search.exe
tool
selects the respective precompiled library during the build process of the
stack project.
Table 16. lists a summary of configurable features. See
the build_config.opt
file for additional details and supported
configurations. Some features in the BLE-Stack 3.03.02.00 cannot be removed and are
always enabled, these features are:
- V41_CTRL_CFG
- EXT_DATA_LEN_CFG
- PRIVACY_1_2_CFG
- SECURE_CONNS_CFG
Feature | Description |
---|---|
HOST_CONFIG | This option configures the stack’s host layer based on its targeted GAP role.
These combo roles are supported:
- PERIPHERAL_CFG+OBSERVER_CFG
- CENTRAL_CFG+BROADCASTER_CFG
- PERIPHERAL_CFG+CENTRAL_CFG
- BROADCASTER_CFG+OBSERVER_CFG
|
BLE_V41_FEATURES | Features supported from the Bluetooth Core Specification Version 4.1.
These features include:
- Ping (V41_CTRL_CFG)
- Slave feature exchange (V41_CTRL_CFG)
- Connection parameter update request (V41_CTRL_CFG)
- Multirole connections (V41_CTRL_CFG)
- L2CAP Connection Oriented Channels (L2CAP_COC_CFG)
|
BLE_V42_FEATURES | Features supported from the Bluetooth Core Specification Version 4.2.
These include:
- Data Length Extension (EXT_DATA_LEN_CFG)
- Secure Connections (SECURE_CONNS_CFG)
- Privacy 1.2 (PRIVACY_1_2_CFG)
|
HCI_TL_xxxx | Include HCI Transport Layer (FULL, PTM or NONE). |
Note
Selecting the correct stack configuration is essential in optimizing the amount of flash memory available to the application. To conserve memory, exclude certain Bluetooth Low Energy protocol stack features that may not be required.
Run-Time Bluetooth Low Energy Protocol Stack Configuration¶
The Bluetooth Low Energy protocol stack can be configured with
various parameters that control its runtime behavior and RF antenna
layout. The available configuration parameters are described in the
ble_user_config.h
file in the ICallBLE IDE folder of the
application. During initialization, these parameters are supplied to
the Bluetooth Low Energy protocol stack by the user0Cfg structure,
declared in main.c.
#include "ble_user_config.h"
// BLE user defined configuration
bleUserCfg_t user0Cfg = BLE_USER_CFG;
Because the ble_user_config.h
file is shared with projects within
the SDK, TI recommends defining the configuration parameters in the
preprocessor symbols of the application when using a non default
value. For example, to change the maximum PDU size from the default
27 to 162, set the preprocessor symbol MAX_PDU_SIZE=162
in the
preprocessor symbols for the application project. Increasing certain
parameters may increase heap memory use by the protocol stack;
adjust the HEAPMGR_SIZE
as required (if not using auto sized heap).
Table 17. lists the available configuration
parameters.
Parameter | Description |
---|---|
MAX_NUM_BLE_CONNS | Maximum number of simultaneous Bluetooth Low Energy connections. Default is 1 for Peripheral and Central roles. Maximum value is based on GAPRole. |
MAX_NUM_PDU | Maximum number of Bluetooth Low Energy HCI PDUs. Default is 5. If the maximum number of connections is set to 0, then this number should also be set to 0. |
MAX_PDU_SIZE | Maximum size in bytes of the Bluetooth Low Energy HCI PDU. Default is 27. Valid range is 27 to 255. The maximum ATT_MTU is MAX_PDU_SIZE - 4. See Configuring for Larger MTU Values. |
L2CAP_NUM_PSM | Maximum number of L2CAP Protocol/Service Multiplexers (PSM). Default is 3. |
L2CAP_NUM_CO_CHANNELS | Maximum number of L2CAP Connection-Oriented (CO) Channels. Default is 3. |
PM_STARTUP_MARGIN | Defines time in microseconds (us) the system will wake up before the start of the connection event. Default is 300. This value is optimized for the example projects. |
RF_FE_MODE_AND_BIAS | Defines the RF antenna front end and bias configuration. Set
this value to match the actual hardware antenna layout. This
value can be set directly, or through Board.h . For more
information see
Configuring the RF Front-End for Custom Hardware |
ICALL_MAX_NUM_TASKS (App) OSAL_MAX_NUM_PROXY_TASKS (Stack) | Defines the max number of ICall enabled tasks. These defines, although on different sides, (app and stack), must be the same. OSAL_MAX_NUM_PROXY_TASKS defaults to 2. ICALL_MAX_NUM_Tasks defaults to 2. |
ICALL_MAX_NUM_ENTITIES (App) | This Maximum number of entities that use ICall, including service entities and application entities. |
Warning
TI Recommends limiting the number of ICall enabled tasks due to resource usage. For more information on creating ICall enabled tasks, see Creating Additional ICall Enabled Tasks