Application¶
Memory Management¶
BLE5-Stack¶
Table of contents
- Overview
- Generic Access Profile (GAP)
- Generic Attribute Profile (GATT)
- GAP GATT Service (GGS)
- Generic Attribute Profile Service (GATT Service)
- GATTServApp Module
- Building up the Attribute Table
- Implementing Profiles in Attributes Table
- Add Service Function
- Register Application Callback Function
- Read and Write Callback Functions
- Read Request from Client
- Write Request from Client
- Get and Set Functions
- Queued Writes
- Allocating Memory for GATT Procedures
- Registering to Receive Additional GATT Events in the Application
- Delaying an ATT Read Request
- GAP Bond Manager and LE Secure Connections
- Privacy
- Logical Link Control and Adaptation Layer Protocol (L2CAP)
- Link Layer (LL)
- Channel Selection Algorithm #2
- Host Controller Interface (HCI)
- Physical Layer (PHY)
- Stack Configurations
Developing a Custom Application¶
A system designer must have a firm grasp on the general system architecture, application, and Bluetooth Low Energy stack framework to implement a custom Bluetooth Low Energy application. This section provides indications and guidance on where and how to start implementing a custom application based on information presented in the previous sections (Introduction and BLE5-Stack) as well as knowledge of TI-RTOS and CC2640R2F.
Decide what role and purpose the custom application should have. If an application is tied to a specific service or profile, start with that sample application.
A project’s role can be essentially be placed in one of the five (5) categories as described by GAP Roles.