1    /* 
     2     *  Copyright (c) 2008-2017 Texas Instruments Incorporated
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ========= Text.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Text ========
    21     *  Runtime text handling services
    22     *
    23     *  This module efficiently manages a collection of strings that have common
    24     *  substrings.  Collections with a high degree of commonality are stored in
    25     *  much less space than as ordinary table of independent C strings.
    26     *
    27     *  To further save space, the "compressed" representation need not even
    28     *  be loaded in the target's memory; see `{@link #isLoaded}`.
    29     *
    30     *  The total space available for the compressed representation of text strings
    31     *  is limited to 64K characters; each string is represented by a 16-bit
    32     *  "rope id".
    33     */
    34    @Template("./Text.xdt")
    35    @DirectCall
    36    module Text {
    37    
    38        /*!
    39         *  ======== CordAddr ========
    40         *  @_nodoc
    41         */
    42        typedef Types.CordAddr CordAddr;
    43    
    44        /*!
    45         *  ======== Label ========
    46         */
    47        typedef Types.Label Label;
    48    
    49        /*!
    50         *  ======== RopeId ========
    51         *  @_nodoc
    52         *
    53         *  A rope id is a 16-bit value whose most-significant bit indicates
    54         *  whether the lower 15-bits are an offset into the string table
    55         *  `charTab` or an offset into the "node" table `nodeTab`.
    56         *
    57         *  The node id 0 represents the empty string "".
    58         */
    59        typedef Types.RopeId RopeId;
    60    
    61        /*!
    62         *  ======== Module_View ========
    63         *  @_nodoc
    64         */
    65        @XmlDtd
    66        metaonly struct Module_View {
    67            Ptr charBase;
    68            Ptr nodeBase;
    69        };
    70    
    71        /*!
    72         *  ======== nameUnknown ========
    73         *  Default unknowable instance name
    74         *
    75         *  The name of an instance if the module's instances are configured to
    76         *  not have names.
    77         */
    78        config String nameUnknown = "{unknown-instance-name}";
    79    
    80        /*!
    81         *  ======== nameEmpty ========
    82         *  Default `NULL` instance name
    83         *
    84         *  The name used if the instance's name has been set to `NULL`.
    85         */
    86        config String nameEmpty = "{empty-instance-name}";
    87    
    88        /*!
    89         *  ======== nameStatic ========
    90         *  Default static instance name
    91         *
    92         *  The name of an instance if the name exists but it's not loaded
    93         *  on the target.
    94         */
    95        config String nameStatic = "{static-instance-name}";
    96    
    97        /*!
    98         *  ======== isLoaded ========
    99         *  Ensure character-strings are loaded in target memory
   100         *
   101         *  Character strings managed by this module are allocated together
   102         *  with other character strings, and loaded to the target, when this
   103         *  parameter is set to its default value `true`. If this parameter is
   104         *  set to `false`, the character strings managed by Text are removed from
   105         *  the application.
   106         *
   107         * A consequence of setting this parameter to `false` is that all names 
   108         * assigned to static instances are set to NULL, and cannot be displayed by
   109         * the code loaded to the target. Also, the Log Events that automatically
   110         * print instance names will print NULL for any static instance. The same
   111         * code would print the pointers to the names if this parameter is set to
   112         * `true` and 'isLoaded` is set to '`false`.
   113         *
   114         * ROV is not affected by this parameter and it will also correctly display
   115         * names of static instances in their modules' views. ROV detects these
   116         * names from the saved configuration files.
   117         *
   118         * Module and event IDs are still unique and Log.Events within one module
   119         * have consecutive IDs.
   120         */
   121        config Bool isLoaded = true;
   122    
   123        /*!
   124         *  ======== cordText ========
   125         *  Return `NULL` if cord is in `charTab` and `isLoaded` is `FALSE`
   126         *  @_nodoc
   127         */
   128        String cordText(CordAddr cord);
   129    
   130        /*!
   131         *  ======== ropeText ========
   132         *  Convert rope to an ordinary C string
   133         *
   134         *  Convert rope to an ordinary C string or to NULL if rope refers
   135         *  to a node in nodeTab
   136         *
   137         *  @_nodoc
   138         */
   139        CString ropeText(RopeId rope);
   140    
   141        /*!
   142         *  ======== matchRope ========
   143         *  Compare pattern string `pat` to String identified by `rope`.
   144         *  @_nodoc
   145         *
   146         *  @a(pre-conditions)
   147         *  @p(blist)
   148         *      - lenp must be less than or equal to the length of pat
   149         *  @p
   150    
   151         *  @a(post-conditions)
   152         *  @p(blist)
   153         *      - lenp is decreased by the length of any matching prefix
   154         *  @p
   155         *
   156         *  Returns:
   157         *  @p(blist)
   158         *      - -1  `pat` does not match string
   159         *      - 0   string is a prefix of pattern
   160         *      - 1   wildcard match
   161         *  @p
   162         */
   163        Int matchRope(RopeId rope, CString pat, UShort *lenp);
   164    
   165        /*!
   166         *  ======== putLab ========
   167         *  Convert label to an ASCII character sequence
   168         *
   169         *  This function converts a `{@link Types#Label}` to a sequence of
   170         *  ASCII characters, writes the characters to the supplied buffer,
   171         *  updates the buffer pointer to point to the location after the last
   172         *  output character, and returns the number of characters output.
   173         *
   174         *  No more than `len` characters will be output.  If the label would
   175         *  otherwise be longer, the output is truncated at the point where a
   176         *  potential overflow is detected. The return value always reflects the
   177         *  number of characters output, but it may be less than `len`.
   178         *
   179         *  Label structures can be initialized from any module's instance handle
   180         *  using the module's `Mod_Handle_label()` method.  See
   181         *  `{@link Types#Label}` for more information.
   182         *
   183         *  @param(lab)    address of the label to interpret
   184         *  @param(bufp)   address of the output buffer pointer or `NULL`
   185         *
   186         *                 If `bufp` is `NULL`, the label's characters are
   187         *                 output via `{@link System#putch()}`.
   188         *
   189         *  @param(len)    maximum number of characters to generate
   190         *
   191         *                 If `len` is negative, the number of characters to be
   192         *                 generated is not limited.
   193         *
   194         *  @a(returns)
   195         *  The return value always reflects the number of characters output,
   196         *  but it may be less than `len`.
   197         *
   198         *  @see Types#Label
   199         */
   200        Int putLab(Types.Label *lab, Char **bufp, Int len);
   201    
   202        /*!
   203         *  ======== putMod ========
   204         *  Convert module ID to its ASCII name
   205         *
   206         *  This function converts a `{@link Types#ModuleId}` to a sequence of
   207         *  ASCII characters, writes the characters to the supplied buffer,
   208         *  updates the buffer pointer to point to the location after the last
   209         *  output character, and returns the number of characters output.
   210         *
   211         *  No more than `len` characters will be output.  If the module name would
   212         *  otherwise be longer, the output is truncated at the point where a
   213         *  potential overflow is detected. The return value always reflects the
   214         *  number of characters output, but it may be less than `len`.
   215         *
   216         *  @param(mid)    ID of the module
   217         *  @param(bufp)   address of the output buffer pointer or `NULL`
   218         *
   219         *                 If `bufp` is `NULL`, the module's name characters are
   220         *                 output via `{@link System#putch()}`.
   221         *
   222         *  @param(len)    maximum number of characters to generate
   223         *
   224         *                 If `len` is negative, the number of characters to be
   225         *                 generated is not limited.
   226         *
   227         *  @a(returns)
   228         *  The return value always reflects the number of characters output,
   229         *  but it may be less than `len`.
   230         */
   231        Int putMod(Types.ModuleId mid, Char **bufp, Int len);
   232    
   233        /*!
   234         *  ======== putSite ========
   235         *  Convert call site structure to an ASCII character sequence
   236         *
   237         *  This function converts a `{@link Types#Site}` to a sequence of
   238         *  ASCII characters, writes the characters to the supplied buffer,
   239         *  updates the buffer pointer to point to the location after the last
   240         *  output character, and returns the number of characters output.
   241         *
   242         *  No more than `len` characters will be output.  If the sequence would
   243         *  otherwise be longer, the output is truncated at the point where a
   244         *  potential overflow is detected.
   245         *
   246         *  @param(site)   address of the call site structure to interpret
   247         *  @param(bufp)   address of the output buffer pointer or `NULL`
   248         *
   249         *                 If `bufp` is `NULL`, the site's name characters are
   250         *                 output via `{@link System#putch()}`.
   251         *
   252         *  @param(len)    maximum number of characters to generate
   253         *
   254         *                 If `len` is negative, the number of characters to be
   255         *                 generated is not limited.
   256         *
   257         *  @a(returns)
   258         *  The return value always reflects the number of characters output,
   259         *  but it may be less than `len`.
   260         */
   261        Int putSite(Types.Site *site, Char **bufp, Int len);
   262    
   263    internal:
   264    
   265        struct Node {
   266            Types.RopeId left;
   267            Types.RopeId right;
   268        };
   269    
   270        typedef Bool (*RopeVisitor)(Ptr, CString);
   271    
   272        struct MatchVisState {
   273            CString pat;
   274            UShort  *lenp;
   275            Int     res;
   276        };
   277    
   278        struct PrintVisState {
   279            Char   **bufp;
   280            UShort len;
   281            Int    res;
   282        };
   283    
   284        /* charTab[] and nodeTab[] are the "compressed" representation of
   285         * target strings used to name instances, modules, packages, ...
   286         *
   287         * The predefined node id 0 represents the empty string.
   288         */
   289        config Char charTab[] = [0];
   290        config Node nodeTab[] = [{left: 0, right: 0}];
   291    
   292        config Int16 charCnt = 1;
   293        config Int16 nodeCnt = 1;
   294    
   295        /*
   296         * The module ids are allocated as follows:
   297         * 0x1 - 0x4000     unnamed modules
   298         * 0x4001 - 0x7FFF  registry modules
   299         * 0x8000 - 0xFFFF  named modules
   300         *
   301         * See 'genModNames' in Text.xs
   302         *
   303         * TODO - We may be able to set unnamedModsLastId based on the config
   304         *        to give the Registry more room, but then the Registry id range
   305         *        would not be a constant.
   306         */
   307        config UInt16 unnamedModsLastId = 0x4000;
   308        config UInt16 registryModsLastId = 0x7FFF;
   309    
   310    /* unnamedModCnt can be used to define a constant that allows external
   311     * modules to define their own module IDs that don't conflict with the
   312     * statically configured modules; e.g., the dlog example could use this
   313     */
   314    //    config Int16 unnamedModCnt = 0;
   315    
   316        function defineRopeCord(text); 
   317        function defineRopeNode(left, right);
   318    
   319        function fetchAddr(raddr);
   320        function fetchCord(cid);
   321        function fetchId(rid);
   322        function fetchNode(nid);
   323    
   324        function genModNames();
   325        function genPkgName();
   326    
   327        Bool matchVisFxn(Ptr p, CString s);
   328        Bool printVisFxn(Ptr p, CString s);
   329    
   330        Void visitRope(RopeId rope, Fxn visFxn, Ptr visState);
   331        Void visitRope2(RopeId rope, Fxn visFxn, Ptr visState, CString stack[]);
   332    
   333        typedef Void (*VisitRopeFxn)(RopeId, Fxn, Ptr);
   334        typedef Void (*VisitRopeFxn2)(RopeId, Fxn, Ptr, CString[]);
   335    
   336        config VisitRopeFxn visitRopeFxn = visitRope;
   337    
   338        config VisitRopeFxn2 visitRopeFxn2 = visitRope2;
   339    
   340        Int xprintf(Char **bufp, SizeT len, CString fmt, ...);
   341    
   342        struct Module_State {
   343            CPtr charBase;
   344            CPtr nodeBase;
   345        };
   346    }
   347    /*
   348     *  @(#) xdc.runtime; 2, 1, 0,0; 11-14-2018 15:26:36; /db/ztree/library/trees/xdc/xdc-F05/src/packages/
   349     */
   350