1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Types.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Types ========
    21     *  Basic constants and types
    22     *
    23     *  This module defines basic constants and types used throughout the
    24     *  `xdc.runtime` package and, in some cases, in every module.
    25     *
    26     *  The `{@link #Common$ Common$}` structure defined by the `Types` module
    27     *  is available for (or common to) all modules. Every field of the
    28     *  `Common$` structure is a configuration parameter that may be set within
    29     *  a configuration script for any module (not just the
    30     *  `xdc.runtime` modules). The fields of this structure are typically read
    31     *  by the modules in the `xdc.runtime` package at configuration time to
    32     *  control the generation of data structures that are embedded in the
    33     *  application and referenced by these modules at runtime.
    34     *
    35     *  Every module has a configuration parameter named
    36     *  `{@link #common$ common$}` that is of type `Common$`. This allows the user
    37     *  of any module to control the module's diagnostics, where its instances
    38     *  are allocated, how they are allocated, and (for gated modules) what
    39     *  gate it should use to protect critical sections.
    40     *
    41     *  @a(Examples)
    42     *  Configuration example: The following configuration script specifies
    43     *  that the instance objects managed by the `Memory` module in the
    44     *  `xdc.runtime` package should be placed in the ".fast" memory section
    45     *  and that `ENTRY` diagnostics should be available at runtime.
    46     *
    47     *  @p(code)
    48     *      var Memory = xdc.useModule('xdc.runtime.Memory");
    49     *      Memory.common$.instanceSection = ".fast";
    50     *      Memory.common$.diags_ENTRY = Diags.RUNTIME_OFF
    51     *  @p
    52     *
    53     *  Note that by setting `Memory.common$.diags_ENTRY` to `Diags.RUNTIME_OFF`
    54     *  we are both enabling `ENTRY` events and specifying that they are initially
    55     *  disabled; they must be explicitly enabled at runtime. See the
    56     *  `{@link Diags}` modules for additional information.
    57     */
    58    
    59    @CustomHeader
    60    
    61    module Types {
    62    
    63        /*!
    64         *  ======== ModuleId ========
    65         *  Unique module identifier
    66         *
    67         *  Module IDs are assigned at configuration time based in the set
    68         *  of modules that are "used" in the application.  So, although each
    69         *  module has a unique 16-bit ID at runtime this ID may vary between
    70         *  configurations of the application.
    71         *
    72         *  To save precious data space, module names are managed by the
    73         *  `{@link Text}` module and it is this table that is used to assign
    74         *  module IDs.  If the table is maintained on the target, the module ID
    75         *  is an "index" into this table; otherwise, the module ID is simply
    76         *  a unique integer less than the total number of modules in the
    77         *  application.
    78         *
    79         *  Although module IDs are not independent of an application's
    80         *  configuration, a module's ID may be compared to a runtime value
    81         *  symbolically.  Every module has a (generated) method that returns
    82         *  the module's ID; e.g., a module named `Task` has a method named
    83         *  `Task_Module_id()` which returns `Task`'s module ID.
    84         *
    85         *  @p(code)
    86         *      #include <xdc/runtime/Types.h>
    87         *      #include <ti/sysbios/knl/Task.h>
    88         *         :
    89         *      void checkId(Types_ModuleId modId) {
    90         *          if (Task_Module_id() == modId) {
    91         *              System_printf("Task module");
    92         *          }
    93         *      }
    94         *  @p
    95         */
    96        typedef Bits16 ModuleId;
    97    
    98        typedef Bits16 DiagsMask;
    99    
   100        /*!
   101         *  ======== Event ========
   102         *  `{@link ILogger}` event encoding
   103         *
   104         *  Whereas a `{@link Log#Event}` encodes an event ID and a mask, a
   105         *  `Types_Event` encodes the same event ID and the module ID of the
   106         *  module containing the call site that generated the `Types_Event`.
   107         */
   108        typedef Bits32 Event;
   109    
   110        /*!
   111         *  ======== getEventId ========
   112         *  Get event ID of the specified event
   113         *
   114         *  This method is used to get an ID that can be compared to other
   115         *  "known" IDs.  For example, after a `{@link #Event Types_Event}` is
   116         *  generated, the following code determines if the event
   117         *  corresponds to a `{@link Log#L_create}` event:
   118         *  @p(code)
   119         *      Bool isCreateEvent(Types_Event evt) {
   120         *          return (Log_getEventId(Log_L_create) == Types_getEventId(evt));
   121         *      }
   122         *  @p
   123         *
   124         *  @param(evt) an event created via `{@link #makeEvent}`
   125         *
   126         *  @a(returns) This function returns the event ID of a specified event.
   127         */
   128        @Macro RopeId getEventId(Event evt);
   129    
   130        /*!
   131         *  ======== getModuleId ========
   132         *  Get the module ID for the specified event
   133         *
   134         *  @param(evt) an event created via `{@link #makeEvent}`
   135         *
   136         *  @a(returns) This function returns the module ID of a specified event.
   137         */
   138        @Macro ModuleId getModuleId(Event evt);
   139    
   140        /*!
   141         *  ======== makeEvent ========
   142         *  Make an Event from an Event ID and a module ID
   143         *
   144         *  @param(id)          ID of the event itself
   145         *  @param(callSite)    the module from which this event originated
   146         *
   147         *  @a(returns) This function returns an event.
   148         */
   149        @Macro Event makeEvent(RopeId id, ModuleId callSite);
   150    
   151        /*!
   152         *  ======== EventId ========
   153         *  @_nodoc
   154         *
   155         *  Deprecated name for `Types.Event`; ids are often encoded as a field
   156         *  in the event itself.
   157         */
   158        typedef Event EventId;
   159    
   160        /*! @_nodoc */
   161        struct CordAddr__;
   162    
   163        /*! @_nodoc */
   164        typedef CordAddr__ *CordAddr;
   165    
   166        /*! @_nodoc */
   167        struct GateRef__;
   168    
   169        /*! @_nodoc */
   170        typedef GateRef__ *GateRef;
   171    
   172        /*! @_nodoc */
   173        typedef Bits16 RopeId;
   174    
   175        /*!
   176         *  ======== CreatePolicy ========
   177         *  Instance creation policy
   178         */
   179        enum CreatePolicy {
   180            STATIC_POLICY,  /*! static creation only; no runtime create/delete */
   181            CREATE_POLICY,  /*! dynamic creation, but no deletion */
   182            DELETE_POLICY   /*! dynamic creation and deletion */
   183        };
   184    
   185        /*!
   186         *  ======== OutputPolicy ========
   187         *  Destination file for module's functions
   188         */
   189        enum OutputPolicy {
   190            COMMON_FILE,    /*! functions are in the common C file */
   191            SEPARATE_FILE,  /*! module has its own separate file */
   192            NO_FILE         /*! functions are not generated */
   193        };
   194    
   195        /*!
   196         *  ======== Label ========
   197         *  Instance label struct
   198         *
   199         *  Label structures are used to provide human readable names for
   200         *  instance handles.
   201         *
   202         *  It is possible to initialize a `Label` from any instance handle.  All
   203         *  modules that support instances provide a method named
   204         *  `Mod_Handle_label()` which, given an instance handle and a pointer to
   205         *  a `Label` structure, initializes the structure with all available
   206         *  information.  For example, the following code fragment initializes a
   207         *  `Label` from an instance of the `HeapMin` module.
   208         *  @p(code)
   209         *      HeapMin_Handle heap;
   210         *      Types_Label label;
   211         *      HeapMin_Handle_label(heap, &label);
   212         *  @p
   213         *
   214         *  Unless you explicitly disable it, `{@link System#printf System_printf}`
   215         *  can be used to convert a pointer to a `Label` into an human readable
   216         *  "instance name".  Continuing with the example above, the following
   217         *  line can be used to print an instance's label.
   218         *  @p(code)
   219         *      System_printf("heap instance name: %$L\n", &label);
   220         *  @p
   221         *
   222         *  @see System#printf, System#extendedFormats
   223         *  @see Text#putLabel
   224         */
   225        struct Label {
   226            Ptr handle;         /*! instance object address */
   227            ModuleId modId;     /*! corresponding module id */
   228            String iname;       /*! name supplied during instance creation */
   229            Bool named;         /*! true, if `iname` is available */
   230        };
   231    
   232        /*!
   233         *  ======== Site ========
   234         *  Error site description struct
   235         *
   236         *  This structure describes the location of the line that raised
   237         *  an error.
   238         *
   239         *  @field(mod) the module id of the module containing the call site
   240         *  @field(file) the name of the file containing the call site or `NULL`;
   241         *               some call sites omit the file name to save data space.
   242         *  @field(line) the line number within the file named
   243         */
   244        struct Site {
   245            ModuleId mod;   /*! module id of this site */
   246            CString file;   /*! filename of this site */
   247            Int line;       /*! line number of this site */
   248        };
   249    
   250        /*!
   251         *  ======== Timestamp64 ========
   252         *  64-bit timestamp struct
   253         *
   254         *  Some platforms only support 32-bit timestamps.  In this case,
   255         *  the most significant 32-bits are always set to 0.
   256         */
   257        struct Timestamp64 {
   258            Bits32 hi;      /*! most significant 32-bits of timestamp */
   259            Bits32 lo;      /*! least significant 32-bits of timestamp */
   260        };
   261    
   262        /*! 
   263         *  ======== FreqHz ========
   264         *  Frequency-in-hertz struct
   265         */
   266        struct FreqHz {
   267            Bits32 hi;      /*! most significant 32-bits of frequency */
   268            Bits32 lo;      /*! least significant 32-bits of frequency */
   269        };
   270    
   271        /*!
   272         *  ======== RegDesc ========
   273         *  Registry module descriptor
   274         */
   275        struct RegDesc {
   276            RegDesc         *next;
   277            CString         modName;
   278            Types.ModuleId  id;
   279            DiagsMask       mask;
   280        };
   281    
   282        /*!
   283         *  ======== Common$ ========
   284         *  Common module config struct
   285         *
   286         *  Every module contains this structure during the configuration
   287         *  phase. The fields of this structure are set in configuration scripts
   288         *  and referenced by the modules in the `xdc.runtime` package. For default
   289         *  values of these fields, see `{@link Defaults}`.
   290         *
   291         *  @field(diags_ASSERT) The `{@link Diags#ASSERT}` bit of a module's
   292         *  diagnostics mask.
   293         *
   294         *  @field(diags_ENTRY) The `{@link Diags#ENTRY}` category of a module's
   295         *  diagnostics mask.
   296         *
   297         *  @field(diags_EXIT) The `{@link Diags#EXIT}` category of a module's
   298         *  diagnostics mask.
   299         *
   300         *  @field(diags_INTERNAL) The `{@link Diags#INTERNAL}` bit of a module's
   301         *  diagnostics mask.
   302         *
   303         *  @field(diags_LIFECYCLE) The `{@link Diags#LIFECYCLE}` category of a
   304         *  module's diagnostics mask.
   305         *
   306         *  @field(diags_STATUS) The `{@link Diags#STATUS}` category of a module's
   307         *  diagnostics mask.
   308         *
   309         *  @field(diags_USER1) The `{@link Diags#USER1}` category of a module's
   310         *  diagnostics mask.
   311         *
   312         *  @field(diags_USER2) The `{@link Diags#USER2}` category of a module's
   313         *  diagnostics mask.
   314         *
   315         *  @field(diags_USER3) The `{@link Diags#USER3}` category of a module's
   316         *  diagnostics mask.
   317         *
   318         *  @field(diags_USER4) The `{@link Diags#USER4}` category of a module's
   319         *  diagnostics mask.
   320         *
   321         *  @field(diags_USER5) The `{@link Diags#USER5}` category of a module's
   322         *  diagnostics mask.
   323         *
   324         *  @field(diags_USER6) The `{@link Diags#USER6}` category of a module's
   325         *  diagnostics mask.
   326         *
   327         *  @field(diags_USER7) The `{@link Diags#USER7}` category of a module's
   328         *  diagnostics mask. The bit for this category has been repurposed for the
   329         *  `{@link Diags#INFO}` category, so the use of USER7 has been deprecated.
   330         *
   331         *  @field(diags_INFO) The `{@link Diags#INFO}` category of a module's
   332         *  diagnostics mask.
   333         *
   334         *  @field(diags_USER8) The `{@link Diags#USER8}` category of a module's
   335         *  diagnostics mask. The bit for this category has been repurposed for the
   336         *  `{@link Diags#ANALYSIS}` category, so the use of USER8 has been
   337         *  deprecated.
   338         *
   339         *  @field(diags_ANALYSIS) The `{@link Diags#ANALYSIS}` category of a
   340         *  module's diagnostics mask.
   341         *
   342         *  @field(fxntab)
   343         *  This configuration parameter is only applicable to modules that
   344         *  inherit an interface and have instance objects.  Setting `fxntab`
   345         *  to `false` can save some data space but also prevents the
   346         *  application from using instance objects through abstract interfaces.
   347         *
   348         *  Function tables are used whenever it's necessary to call a module's
   349         *  methods via an abstract interface; e.g., the `{@link Memory}` module
   350         *  calls methods defined by the `{@link IHeap}` interface but there may
   351         *  be several distinct modules that implement this interface.  In order
   352         *  for this type of call to be possible, instance objects contain a
   353         *  reference to a function table containing the instance module's
   354         *  functions; the caller gets the module's function from the instance
   355         *  object and calls through a function pointer.  Every module that
   356         *  inherits an interface has such a table and modules that do not
   357         *  inherit an interface do not have a function table.
   358         *
   359         *  If this configuration parameter is set to `false`, the module's
   360         *  instance objects will NOT be initialized with a reference to their
   361         *  module's function table and, since the function table will not
   362         *  be referenced by the application, the resulting executable will be
   363         *  smaller.  However, if this parameter is `false` you must never
   364         *  attempt to use this module's instance objects via reference this
   365         *  module through an abstract interface.  Since this is often hard to
   366         *  determine, especially as an application evolves over time, you should
   367         *  only set this parameter to `false` when you are absolutely sure that
   368         *  the module's functions are always only being directly called and you
   369         *  need to absolutely minimize the data footprint of your application.
   370         *
   371         *  The default for this parameter is `true`.
   372         *
   373         *  @field(gate) A handle to the module-level `{@link IGateProvider}`
   374         *  instance to be used when this module calls functions from
   375         *  `{@link Gate}`
   376         *
   377         *  @field(gateParams) `Gate` parameters used by this module to create
   378         *  the gates used when this module calls 
   379         *  `{@link Gate#allocInstance() Gate_allocInstance}`
   380         *
   381         *  @field(instanceHeap) Identifies the heap from which this module
   382         *  should allocate memory.
   383         *
   384         *  @field(instanceSection) Identifies the section in which instances
   385         *  created by this module should be placed.
   386         *
   387         *  @field(logger) The handle of the logger instance used by the module.
   388         *  All log events generated by the module are routed to this logger
   389         *  instance. See `{@link ILogger}` for details on the logger interface.
   390         *  See `{@link LoggerBuf}` and `{@link LoggerSys}` for two examples of 
   391         *  logger modules provided by the `{@link xdc.runtime}` package.
   392         *
   393         *  @field(memoryPolicy) Specifies whether this module should allow
   394         *  static object creation only (`{@link #CreatePolicy STATIC_POLICY}`),
   395         *  dynamic object creation but not deletion
   396         *  (`{@link #CreatePolicy CREATE_POLICY}`), or both dynamic object
   397         *  creation and deletion (`{@link #CreatePolicy DELETE_POLICY}`).
   398         *
   399         *  @field(namedInstance) If set to `true`, each instance object is
   400         *  given an additional field to hold a string name that is used
   401         *  when displaying information about an instance. Setting this to
   402         *  `true` increases the size of the module's instance objects by a
   403         *  single word but improves the usability of tools that display
   404         *  instance objects.  If set to `false`, assignments of instance
   405         *  names are silently ignored.  This allows one to remove instance
   406         *  name support to save space without having to change any source code.
   407         *  See `{@link xdc.runtime.IInstance#name IInstance.name}` for details.
   408         *
   409         *  @field(namedModule) If set to `true`, this module's string name
   410         *  is retained on the target so that it can be displayed as part
   411         *  of `{@link Log}` and `{@link Error}` events. Setting this to `false`
   412         *  saves data space in the application at the expense of readability
   413         *  of log and error messages associated with this module.
   414         *
   415         *  Note: setting this to `false` also prevents one from controlling the
   416         *  module's diagnostics at runtime via `{@link Diags#setMask()}`.
   417         *  This method uses the module's name to lookup the module's
   418         *  diagnostics mask.  It is still possible to control the module's
   419         *  diagnostics at design-time from a configuration script.
   420         *
   421         *  @see Diags, Defaults
   422         */
   423        metaonly struct Common$ {
   424            Diags.Mode diags_ASSERT;    /*! module's Diags assert mode */
   425            Diags.Mode diags_ENTRY;     /*! module's function entry Diags mode */
   426            Diags.Mode diags_EXIT;      /*! module's function exit Diags mode */
   427            Diags.Mode diags_INTERNAL;  /*! module's internal assert mode */
   428            Diags.Mode diags_LIFECYCLE; /*! module's instance lifecycle mode */
   429            Diags.Mode diags_STATUS;    /*! module's errors and warnings */
   430            Diags.Mode diags_USER1;     /*! module's user1 Diags mode */
   431            Diags.Mode diags_USER2;     /*! module's user2 Diags mode */
   432            Diags.Mode diags_USER3;     /*! module's user3 Diags mode */
   433            Diags.Mode diags_USER4;     /*! module's user4 Diags mode */
   434            Diags.Mode diags_USER5;     /*! module's user5 Diags mode */
   435            Diags.Mode diags_USER6;     /*! module's user6 Diags mode */
   436            Diags.Mode diags_USER7;     /*! module's user7 Diags mode */
   437            Diags.Mode diags_INFO;      /*! module's informational event mode */
   438            Diags.Mode diags_USER8;     /*! module's user8 Diags mode */
   439            Diags.Mode diags_ANALYSIS;  /*! module's Diags analysis mode */
   440            Bool fxntab;                /*! @_nodoc enable function tables */
   441            IGateProvider.Handle gate;  /*! module's gate */
   442            Ptr gateParams;             /*! gate params for module created gates */
   443            IHeap.Handle instanceHeap;  /*! module's instance heap */
   444            String instanceSection;     /*! memory section for module's instances*/
   445            ILogger.Handle logger;      /*! module's logger */
   446            OutputPolicy outPolicy;     /*! destination file for module's code */
   447            CreatePolicy memoryPolicy;  /*! module's memory policy */
   448            Bool namedInstance;         /*! true => instances have string names */
   449            Bool namedModule;           /*! true => module's name is on target */
   450            Bool romPatchTable;         /*! @_nodoc */
   451        }
   452    
   453        /*!
   454         *  ======== RtaDecoderData ========
   455         *  @_nodoc
   456         *
   457         *  loggers
   458         *    name - Used to identify the logger in GUI
   459         *    bufferSym - For stop-mode; symbol at which the logger's entry
   460         *                buffer can be found
   461         *    bufferLen - For stop-mode; length of the logger's entry buffer in
   462         *                MAUs
   463         */
   464        @XmlDtd metaonly struct RtaDecoderData {
   465            String targetName;
   466            String binaryParser;
   467            String endian;
   468            Int bitsPerChar;
   469            Int argSize;
   470            Int eventSize;
   471            String dataTransportClassName;
   472            String controlTransportClassName;
   473            struct {
   474                String name;
   475                String type;
   476                Any metaArgs;
   477            } loggers[ ];
   478            struct {
   479                Int id;
   480                String logger;
   481                String diagsMask;
   482            } modMap[string];
   483            struct {
   484                Int id;
   485                String msg;
   486            } evtMap[string];
   487        };
   488    
   489        /*!
   490         *  ======== ViewInfo ========
   491         *  @_nodoc
   492         *  XGconf view descriptor.
   493         */
   494        metaonly struct ViewInfo {
   495            String viewType;
   496            String viewFxn;
   497            String fields[];
   498        }
   499    
   500    internal:
   501    
   502        typedef Bits32 LogEvent;
   503    
   504        typedef Void (*LoggerFxn0)(Ptr, LogEvent, ModuleId);
   505        typedef Void (*LoggerFxn1)(Ptr, LogEvent, ModuleId, IArg);
   506        typedef Void (*LoggerFxn2)(Ptr, LogEvent, ModuleId, IArg, IArg);
   507        typedef Void (*LoggerFxn4)(Ptr, LogEvent, ModuleId, IArg, IArg, IArg, IArg);
   508        typedef Void (*LoggerFxn8)(Ptr, LogEvent, ModuleId, IArg, IArg, IArg, IArg,
   509                                   IArg, IArg, IArg, IArg);
   510    
   511        struct Vec {
   512            Int len;
   513            Ptr arr;
   514        };
   515    
   516        /*
   517         *  ======== Link ========
   518         *  Link used to maintain atomic linked lists
   519         */
   520        struct Link {
   521            Link *next;
   522            Link *prev;
   523        };
   524    
   525        /*
   526         *  ======== InstHdr ========
   527         *  Header for all runtime created instance objects
   528         */
   529        struct InstHdr {
   530            Link link;
   531        }
   532    
   533        /*
   534         *  ======== PrmsHdr ========
   535         *  Header for all _Params structures
   536         */
   537        struct PrmsHdr {
   538            SizeT size;     /* size of the entire parameter structure */
   539            Ptr self;       /* pointer to self; used to check params are init'd */
   540            Ptr modFxns;
   541            Ptr instPrms;
   542        }
   543    
   544        /*
   545         *  ======== Base ========
   546         *  Header for all module vtables
   547         */
   548        struct Base {
   549            const Base *base;     /* points to inherited interface base */
   550        }
   551    
   552        /*
   553         *  ======== SysFxns2 ========
   554         *  System data embedded in module's vtable
   555         */
   556        struct SysFxns2 {
   557    
   558            /*
   559             *  ======== __create ========
   560             *  Signature of configuration generated module instance constructor
   561             *
   562             *  This function calls Core_createObject().
   563             *
   564             *  Params:
   565             *      CPtr          - pointer to struct of required create args
   566             *      const UChar * - pointer to struct of default create parameters
   567             *      SizeT         - size of default params structure
   568             *      Error_Block * - caller's error block pointer
   569             */
   570            Ptr (*__create)(CPtr, const UChar *, SizeT, Error.Block *);
   571            // 490928 Ptr (*__create)(CPtr, const UChar *, SizeT, Error.Block *);
   572    
   573            Void (*__delete)(Ptr);
   574            Label *(*__label)(Ptr, Label *);
   575            ModuleId __mid;
   576        }
   577    }
   578    /*
   579     *  @(#) xdc.runtime; 2, 1, 0,0; 11-14-2018 15:26:36; /db/ztree/library/trees/xdc/xdc-F05/src/packages/
   580     */
   581