Please remove power and connect the [[evmName]] to the [[controllerName]]
controller. If already inserted, please double check the header alignment.
Please restart or reload the GUI after inserting the EVM
Unknown EVM(s) Found!
The GUI could not detect a [[controllerName]] controller with a connected [[evmName]]
daughtercard.
Please check that the appropriate EVM is connected or locate the correct EVM GUI from
https://dev.ti.com/gallery/.
If a [[evmName]] is connected, then you may attempt to connect to it
by selecting "Options > Serial Port ..." from the menu bar.
Please restart or reload the GUI after inserting EVM
Incompatible EVM(s) Found!
This GUI is compatible with the [[evmName]] daughtercard.
Please replace the daughtercard or select a compatible GUI from
https://dev.ti.com/gallery/
Please restart or reload the GUI after inserting EVM
WARNING: You are connecting to an unrecognized EVM...
The [[controllerName]] controller could not detect a compatible EVM connected.
Please note that the device you are connecting to may not work as expected!
If you have more that one [[controllerName]] controller
connected to your computer, please disconnect all of them except
for the one with the [[evmName]] and try again.
ERROR: Connection to BULK device timed out...
Please disconnect and reconnect the [[controllerName]] controller and try again.