Do the MODE and GAIN widgets match the MODE and GAIN hardware headers on the EVM?
Warning!
A Sleep to Wake cycle will set the POR flag and configure the device Registers to their default values. Would you like to Save all Registers configuration to a file using “Save Registers” command in the File menu?
Load Register Configuration
Retrieve the device Registers configuration from a saved file using “Load Registers” command in the File menu if desired.
Mode and Gain Value Warning!
Before setting Driver to Awake, make sure the GAIN and MODE widgets match the GAIN and MODE hardware jumpers on the EVM.
Independent Half-Bridge Control Warning!
With a load connected to PVDD and both the Enable Driver bit and the DRVOFF pin are set to 1, the load
will
experience maximum RPM when the duty cycle is set to 0%.
For the load to experience minimum RPM, set the duty cycle to 100%.
Operation Mode Warning!
It is not recommended to change operation mode while driving the load.
Configuration Warning
Please refer to the datasheet, EVM user’s guide, and EVM schematic to make necessary hardware
connections for
VDS, IDRIVE, MODE and Gate configurations. The configurations should be done only when the driver is
asleep
Please select the following diagram as per the hardware connection:
Please select the motor connection:
Motor - 1 is connected to :
PVDD
GND
Motor - 2 is connected to :
PVDD
GND
Please select the motor connection:
Motor - 1 is connected to :
PVDD
GND
Please select the motor connection:
Motor - 2 is connected to :
PVDD
GND
Please select the motor connection:
Motor is connected to :
PVDD
GND
EVM Connection Warning
Going back to the GUI Landing Page will disconnect the EVM. Would you like to proceed?
Please wait while the device connection is in progress...