The connected SCB controller is using an incompatible firmware application or version.
The GUI requires a firmware update to proceed with evaluation.
Load FirmwareDisconnect
Flash Successful
Please wait while the GUI reloads.
Flash Unsuccessful
Ensure that SCB is connected properly. Please try reloading the GUI and
power cycle the device.
No SCB controller detected
Please connect the [[evmName]] + [[controllerName]] controller to your computer.
If connected, please ensure that your [[controllerName]] has been flashed with the relevant firmware
by placing the MCU into DFU Mode. You can then upload the firmware to the [[controllerName]] by selecting
Program Device under the File drop-down menu. For more details, please see the [[evmName]]'s
User's Guide.
Please remove power and connect the [[evmName]] to the [[controllerName]]
controller. If already inserted, please double check the header alignment.
Please restart or reload the GUI after inserting the EVM
Unknown EVM(s) Found!
The GUI could not detect a [[controllerName]] controller with a connected [[evmName]]
daughtercard.
Please check that the appropriate EVM is connected or locate the correct EVM GUI from
https://dev.ti.com/gallery/.
If a [[evmName]] is connected, then you may attempt to connect to it
by selecting "Options > Serial Port ..." from the menu bar.
Please restart or reload the GUI after inserting EVM
Incompatible EVM(s) Found!
This GUI is compatible with the [[evmName]] daughtercard.
Please replace the daughtercard or select a compatible GUI from
https://dev.ti.com/gallery/
Please restart or reload the GUI after inserting EVM
WARNING: You are connecting to an unrecognized EVM...
The [[controllerName]] controller could not detect a compatible EVM connected.
Please note that the device you are connecting to may not work as expected!
If you have more that one [[controllerName]] controller
connected to your computer, please disconnect all of them except
for the one with the [[evmName]] and try again.
ERROR: Connection to BULK device timed out...
Please disconnect and reconnect the [[controllerName]] controller and try again.