GUI Program will disable the converter before reconfiguring the EVM
RSENSE
The average output current limit is dynamically programmable by AVG_ILIM_THRESHOLD (0xD0h).
The programmable range and the programmable step size of the average output current limit are set by RSENSE resistor.
The programmable step size [A] = 400uV/RSENSE
The minimum programmable average output current limit at 0Ah [A] = 4mV/RSENSE
The maximum programmable average output current limit at 96h [A] = 60mV/RSENSE
Example1 : RSENSE = 8mΩ, programmable step size = 50mA, the minimum programmable average output current limit = 0.5A, the maximum programmable average output current limit = 7.5A
Example2 : RSENSE = 2mΩ, programmable step size = 200mA, the minimum programmable average output current limit = 2.0A, the maximum programmable average output current limit = 30A
GUI Program will disable the converter before reconfiguring the EVM