Integration Notes¶
Profiling data is provided below for evaluation. These numbers were taken using the compiler settings and version for the RELEASE build configuration of the library project and the RAM_RELEASE and FLASH_RELEASE configurations of the STA.
Cycle Time¶
The cycle counts shown are based on the configuration of the modules used in the STA. The counts are not necessarily the worst-case cycle count and may vary depending on the module parameters. For example, some of the memory tests have configurable memory ranges over which the test should be performed, meaning the larger the memory section, the longer the test runs.
API |
PASS Cycles (RAM) |
FAIL Cycles (RAM) |
PASS Cycles (Flash) |
FAIL Cycles (Flash) |
|---|---|---|---|---|
STL_PIE_RAM_testHandler |
520 |
429 |
557 |
462 |
STL_LCM_checkRegisterParity |
335 |
335 |
355 |
355 |
STL_LCM_runSelfTest |
1997 |
1997 |
2006 |
2006 |
STL_LCM_checkCompareError |
NA |
NA |
265 |
265 |
STL_CPU_REG_checkCPURegisters |
652 |
54 |
306 |
63 |
STL_CPU_REG_checkFPURegisters |
287 |
123 |
673 |
133 |
STL_CPU_REG_checkVCRCRegisters |
227 |
117 |
242 |
128 |
STL_SP_writeMonitoredRange |
119 |
100 |
133 |
111 |
STL_March_testRAM (16 words) |
403 |
403 |
530 |
530 |
STL_March_testRAMCopy (16 words) |
501 |
501 |
666 |
666 |
STL_CAN_RAM_testRAM (144 words) |
6660 |
6660 |
7552 |
7552 |
STL_CAN_RAM_testRAM (304 words) with copy |
16232 16232 |
16327 16327 |
18838 18838 |
18939 18939 |
STL_MCAN_RAM_testRAM (1024 words) |
83031 |
83032 |
95335 |
95335 |
STL_MCAN_RAM_testRAM (320 words) with copy |
15612 15612 |
15612 15612 |
18337 18337 |
18337 18337 |
STL_CRC_checkCRC (32 words) |
234 |
236 |
243 |
240 |
STL_OSC_CT_startTest & STL_OSC_CT_stopTest |
145 |
144 |
158 |
153 |
STL_OSC_HR_testSFO |
131975 |
131881 |
132004 |
132007 |
Memory Usage¶
The following shows the size in 16-bit words of the STL APIs. These values were obtained from the STA .map file.
API |
Memory (16-bit words) |
|---|---|
STL_CAN_RAM_checkErrorStatus |
14 |
STL_CAN_RAM_injectError |
39 |
STL_CAN_RAM_testRAM |
62 |
STL_CPU_REG_testCPURegisters |
205 |
STL_CPU_REG_testFPURegisters |
106 |
STL_CPU_REG_testVCRCRegisters |
76 |
STL_CRC_checkCRC |
38 |
STL_CRC_calculate |
56 |
STL_CRC_calculateLowBytes |
46 |
STL_CRC_reset |
5 |
STL_LCM_checkCompareError |
104 |
STL_LCM_checkRegisterParity |
109 |
STL_LCM_parityNMIISR |
18 |
STL_LCM_compareErrorNMIISR |
18 |
STL_LCM_runSelfTest |
110 |
STL_March_checkErrorStatus |
38 |
STL_March_injectError |
16 |
STL_March_testRAM |
35 |
STL_March_testRAMCopy |
47 |
STL_MCAN_RAM_checkErrorStatus |
19 |
STL_MCAN_RAM_injectError |
40 |
STL_MCAN_RAM_testRAM |
33 |
STL_OSC_CT_startTest |
66 |
STL_OSC_CT_stopTest |
30 |
STL_OSC_HR_testSFO |
120 |
STL_PIE_RAM_handler |
5 |
STL_PIE_RAM_configHandler |
6 |
STL_PIE_RAM_injectFault |
22 |
STL_PIE_RAM_restoreVector |
10 |
STL_PIE_RAM_testHandler |
110 |
STL_SP_configSP |
81 |
STL_SP_disableWatchpoint |
12 |
STL_SP_restoreVector |
19 |
STL_SP_testISR |
20 |
STL_SP_writeMonitoredRange |
26 |
STL_Util_clearErrorFlag |
6 |
STL_Util_getErrorFlag |
4 |
STL_Util_setErrorFlag |
5 |
There is also a contribution from the non-inline driverlib functions used by the library. Use of the STL_OSC_HR module results in an additional 497 words from the SFO library.