xWRL684x MMWAVE-L-SDK  06.00.05
Introduction

Welcome to MMWAVE-L-SDK for xWRL684x. This SDK contains examples, libraries and tools to develop RTOS and no-RTOS based applications for ARM R5F CPUs and related peripherals.

This SDK also contains examples to interface these ARM R5F applications .

Block Diagram

Given below is a block diagram of the SW modules in this SDK,

Software Block Diagram

The main software components in the block diagram are described below

Software Components Documentation Page Description
OS Kernel
No RTOS NO RTOS Contains modules which implement no-RTOS execution environment consisting of timers, ISR, main thread. Allows software on top to run in bare metal mode.
FreeRTOS Kernel FreeRTOS FreeRTOS Kernel, provides a execution environment consisting of tasks, semaphores, timers, see https://www.freertos.org/RTOS.html
FreeRTOS POSIX FreeRTOS Limited POSIX APIs with FreeRTOS underneath, provides pthreads, mqueue, semaphore, see https://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_POSIX/index.html
Driver Porting Layer (DPL) Driver Porting Layer (DPL) APIs used by drivers to abstract the OS environment. Example, Semaphore, HW interrupts, mutex, clock.
Device Drivers and HAL (Hardware Abstraction Layer)
SOC Peripheral Drivers SOC Drivers Device Drivers library and APIs for peripherals within the SOC. Example, I2C, GPIO, UART.
Board Peripheral Drivers Board Peripheral Drivers Device Drivers library and APIs for peripherals on the board or EVM. Example, Flash, EEPROM.
Datapath Modules
Datapath Modules Datapath Modules

Datapath modules consisting of DPUs and related utilities.

Examples
Examples Examples Examples showing usage of different SW libraries and APIs
Tools (used on host machine)
Code Composer Studio (CCS) Using SDK with CCS Projects IDE used to build projects, debug programs, see
TI CLANG Compiler Toolchain TI CLANG HOMEPAGE CLANG based ARM compiler from TI for ARM R5F
SysConfig Using SDK with SysConfig System configuration tool, used to configure peripherals, pinmux, clocks and generate system initialization code
TI Resource Explorer (TIREX) (TBD) Using SDK with TI Resource Explorer
Web broswer based tool to explore the SDK, select, import and run the examples
SDK Tools and Utilities Tools and Utilities Additional tools and utilities, like flashing tools, booting tools, CCS loading scripts used with the SDK development flow

Directory Structure

Given below is a overview of the directory structure to help you navigate the SDK and related tools.

Folder/Files Description
${SDK_INSTALL_PATH}/
README_FIRST_xWRL684x.html Open this file in a web browser to reach this user guide
makefile Top level makefile to build the whole SDK using "make"
imports.mak Top level makefile to list paths to dependant tools
docs/ Offline browseable HTML documentation
examples/ Example applications for xWRL684x, across multiple boards, CPUs, NO-RTOS, RTOS
firmware/ Contains firmware code for xWRL684x front end
source/ Device drivers, middleware libraries and APIs
tools/ Tools and utilities like CCS loading scripts, initialization scripts.
${SDK_INSTALL_PATH}/source/
control/ Control path library for configuring radar front end
drivers/ SOC peripheral device drivers
kernel/ NO RTOS and RTOS kernel and Driver Porting layer (DPL) for these environments
board/ Board peripheral device drivers
${SDK_INSTALL_PATH}/examples/
control/

Control path examples

datapath/ Data Processing Units (DPU) examples
drivers/ SOC and board level focused device drivers examples. The examples are based on both NO-RTOS and RTOS
kernel/

NO RTOS and RTOS kernel focused examples

${SDK_INSTALL_PATH}/tools/
visualizer/visualizer.exe Tool to configure mmWave sensors and Visualize point cloud objects generated by the mmWave SDK
Flashing Tool Tool to flash examples of the mmWave SDK
syscfg_deviceData/

The device data information used by Sysconfig for pinmuxing

gelfile/ This folder have xwrL684x.gel file. It is used in debugging.
MetaImageGen/ Metaimage generation tool
CCS_SupportFiles/

CCS support file xWRL68xx.xml for Target configuration

Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.

Folder/Files Description
C:/ti/ccs2010 Code composer studio
C:/ti/sysconfig_1.23.0_4000 SysConfig.
C:/ti/ti-cgt-armllvm_4.0.2.LTS TI ARM CLANG compiler tool chain

Licenses

The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [LINK]

Help and Support

For additional help and support, see https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum

Documentation Credits

This user guide is generated using doxygen, v1.8.20. See https://www.doxygen.nl/index.html