Revision History
v0.10.32
- added tool version to output files
- updated warning messages for frequency settings
- set CA Parity to disabled by default in AM64x/AM62x/AM62Lx DDR4 configurations. AM62Lx does not support CA Parity, and thus must be disabled.
v0.10.31
- updated Nanya memory list
- change default bit swizzle in AM62P to point to point (now must choose reference design to get appropriate bit swizzle for SK-AM62P-LP EVM)
- restrict AM62Lx to 800MHz operation
v0.10.30
- adding support for AM62Lx
- added device selections for Nanya DDR4 and LPDDR4 memories for AM64x, AM62x, AM62Ax
- added checks for TCR mode in DDR4 for AM62x
- allow disable of Read DBI for DDR4 memories which don't support DBI (not recommended)
- fixed bug with SOC ODT FSP1
v0.10.20
- adding parameters to support temperature based dynamic refresh (Please refer to SDK Release Notes to determine which SDK versions support this feature)
- All interrupt were unmasked in previous versions. This has been changed so that all interrupts are masked. Driver is now responsible for unmasking interrupts as needed
v0.10.10
- fixed errata associated with CA VREF training range
- restricted some inputs for FSP1 and IO configurations
- removed parameter tDQSCKmin from DDR4
- added support for AM62Dx
- Read DBI can now be disabled to support DDR4 without read DBI feature.
- removed tDQSCKmin parameter. Not used in configuration.
v0.10.02
- fixed CA VREF range1 training search for LPDDR4
- updated README, added DDR4 instructions
- added flexibility in choosing operating frequencies
- added selections for DDR4: LPASR, TCR mode, TCR range, and CA Parity Latency
- alphabetized timing parameters in DDR4
- changed WDQS Extension to enabled by default for LPDDR4. This enables WDQS Read Based Control.
- added periodic ZQ calibration selection for LPDDR4
- added REGION_IDX parameter to properly set Subsystem register
v0.10.01
- new cosmetic changes: including being able to choose reference design as starting point
- added support for "Set B" write latencies in LPDDR4
- updated ODTon/off values per freq
- added support for enabling periodic ZQ Calibration in LPDDR4 memories (only 256ms period)
- added support for separate CK drive setting in LPDDR4
- allow for direct input of operating frequency in DDR4. Added warning and error checking
- updated DFI timings for AM62Ax and AM62Px
- added SDRAM_IDX parameter to properly set Subsystem register
- changed tool version in README from xx.xx to x.xx.xx (was missing leading revision)
v0.9.10
- added AM62Px LPDDR4 support
- added support for swizzle of DMIx along with DQx (AM62x/AM62A/AM62P)
- allow for direct input of operating frequency in LPDDR4
- adjusted RST_DRIVE during initialization
v0.9.09
- added LPDDR4 description in README
- added instructions for offline support in README
- added 1200MHz use case for AM62A
- added auto adjustments of tRAS and tREFI with change in temp selection
- updated changes to latency parameters when frequency changes
- changed CS_MAP parameters to support 16-bit in AM62A
- rx_pclk_clk_sel update
- added WDQ leveling configuration selection
v0.9.08
- added automatic change of RL, WL and nWR when frequency is changed
- added DQ swizzle and byte swap configuration flexibilty for AM62x/AM62A LPDDR4
- PHY_CAL_CLK updated divider values for higher frequencies
- CS ODT fix bug introduced in previous release
v0.9.05:
- cleaned up supported frequencies
v0.9.04:
- changed wrlvl_delay_early_threshold=0x100 to allow write leveling to complete successfully for wider array of layouts
- add cmm output
- LPDDR4: phy_rddqs_latency_adjust changed to 0 default recommendation (this value gets optimized during training)
- LPDDR4: optimized training loops to support 1 operating frequency
- LPDDR4/DDR4: optimized IO calibration configuration based on operating frequency
- LPDDR4/DDR4: optimized internal calibration clock based on operating frequency
- LPDDR4: changed default MR22 ODTE-CS=1
- LPDDR4: changed rx_ctle_cs default to No Boost
- AM62x dual rank support
- updated to use sysconfig v1.15
- public release for AM62A LPDDR4 support
v0.8.80:
- added support for AM62x release.
- Added support for high temp operation.
- CTL_165[11]=1 (LPI_WAKEUP_EN) only applicable for AM62x
- CTL_321[23:8] = 0xFFFF (CS_MSK_1) corrected value when rank 1 disabled
v0.8.40: provides improved operation at 1600MTs for both LPDDR4 and DDR4.
Changes from previous version include:
- changed default value CTRLUPD_AREF_HP_ENABLE=0
- changed default value LPI_\WAKEUP_EN=0
- changed cal_clk divider and PVT calibration interval. This change provides significant stability improvements for LPDDR4 and DDR4 operation at 1600MTs
- fixed TOSCO_F0 calculation for LPDDR4
v0.8.10: initial stable version.
Changes from previous versions include:
- added read/write DBI selection for LPDDR4/DDR4. Default to enable write DBI for LPDDR4, read DBI for DDR4 to improve power supply noise and improve overall signal integrity
- changed default value of CA ODT to 60ohm for both LPDDR4 and DDR4
- updated RTOS output to fix #ifdef
- periodic write DQ leveling disabled to improve realtime performance
- disabled "always-on" mode of the input enables for data bytes for power optimization
- disabled VREF controller for addr/cmd signals for power optimization