3.6.4. EVM Boot Mode Switches#

There are multiple ways (boot modes) to boot Linux on an EVM (from a micro SD card, eMMC, UART, etc.). The boot mode is defined by the boot mode switches on the EVM. The supported boot modes and the corresponding boot mode switch settings can be found in the EVM User’s Guide:

This section provides the boot mode switch settings for a few commonly used boot modes.

Table 3.3 AM62x SK EVM Boot Mode#

Boot Mode

EVM Boot Mode Switches Setting

SD card boot

../_images/am62x_sk_evm_sdcard_boot_mode.jpg

eMMC boot

../_images/am62x_sk_evm_emmc_boot_mode.jpg

USB Peripheral boot

../_images/am62x_sk_evm_dfu_boot_mode.jpg