2.1. What is Needed to Evaluate Linux?#

These components are needed to evaluate Linux on a TI processor:

Hardware

  • An evaluation module (EVM) and associated cables, power supply, etc

  • A computer that can write to an SD card (for example, through a USB card writer)

Software

  • A Linux image to run on the processor

2.1.1. Hardware#

TI provides support for the AM62x Starter Kit.

Note that the TI AM62x EVMs require additional hardware that is not shipped in the box with the EVMs. For a full list of the hardware required for each board, reference the “Hardware Setup” section of the EVM Quick Start Guides:


2.1.2. Software#

Follow the steps in the “Software Setup” section of the EVM Quick Start Guides to download a Linux image to run on AM62x.