4. Porting Linux to Custom Hardware#

This Academy module focuses on porting Linux to a custom platform. This content extends what was done in the Develop Linux on TI EVM module.
These components are needed in order to port Linux to a custom platform:
working hardware
U-Boot
Kernel
device tree binary (DTB)
Root File System
The TI Processor SDK Linux package provides U-Boot and Linux running on TI EVMs. The provided U-Boot and Linux kernel are called the Base Port. The following sections illustrate how to port U-Boot and Linux to a custom platform by modifing the Base Port to match the custom board’s peripheral set and kernel requirements.
U-Boot should be ported first, since U-Boot must run successfully on working hardware in order for the Linux kernel to boot. Once the U-Boot minimum configuration and custom features have been brought up, then the Linux kernel porting can begin.