1.1. Hardware Design Reference

Hardware is a critical part of any embedded system. This section focuses on the collateral that TI provides to help design good hardware.

../_images/Academy_SysDesign_Hardware.png

A Linux system must consider the Linux software support available. Choosing devices that already have good Linux support can dramatically speed the design process and help ensure software robustness.

1.1.1. Hardware Design Collateral

Linux developers may not perform hardware design, but the quality of hardware impacts Linux development. Hardware issues can dramatically impact software schedules. This list of helpful collateral is included to highlight the resources available to help ensure quality hardware for efficient software development.

Document/Resource

Notes

Data Sheet

Foundational document

Technical Reference Manual

Foundational document

Silicon Errata

Important for checking known issues and workarounds

Schematic Review Checklist

Very important as a guide for board design. This document should be well understood before board design.

High-Speed Interface Layout Guidelines

An excellent complement to Schematic Review Checklist above. Required reading for board designers.

DDR Board Design and Layout Guidelines

Another required reading. DDR design can be a challenge for new boards.

SysConfig Configuration Tool

Important for Pin Mux, DDR Config, and MCU+ SDK.

Power Estimation Tool

Useful tool to help estimate power consumption.

BGA Escape Routing

Sample PCB escape routing.

AM62x Starter Kit

Design files serve as good examples.

1.1.2. Linux Software Compatibility

In addition to designing the best hardware for a robust embedded system, it is advantageous to choose hardware that is already well supported by Linux. Linux code that has been used in other systems has already been tested and hardened. If Linux support for a feature is already available, then the Linux developer can avoid developing new drivers and working out the likely bugs in them. This availability and robustness save time and effort by software teams and help keep schedules on track.

TI provides Linux drivers for most SoC functions and peripherals. While this covers the SoC peripherals, it does not cover the individual components that these peripherals are interfacing with. For example, I2C master on AM62x has a Linux driver provided with the Processor SDK for Linux. That does not mean that the I2C GPIO Expander that is chosen for a design has a corresponding driver. The availability of such a driver needs to be checked as well:

It is very important to understand the driver availability of all components being used on a board or project before project commissioning. This makes sure that software project deadlines are planned accordingly. If a component without Linux support is chosen, then the software development efforts to enable that device should be factored into the overall project costs and timelines.