![Logo](ti_logo.svg) |
AM263x MCU+ SDK
08.02.01
|
|
Go to the documentation of this file.
63 #include <priv/core/enet_rm_priv.h>
74 #define ICSSG_PUBLIC_IOCTL(x) (ENET_IOCTL_PER_BASE | \
75 ENET_IOCTL_PER_ICSSG | \
79 #define ICSSG_PORT_NUM (3U)
82 #define ICSSG_MAC_PORT_MAX (ICSSG_PORT_NUM - 1U)
86 #define ICSSG_PER_DUALMAC_PORT_MAX (1U)
89 #define ICSSG_PER_SWITCH_PORT_MAX (ICSSG_MAC_PORT_MAX)
93 #define ICSSG_INSTANCE_NUM (3U)
95 #define ICSSG_INSTANCE_NUM (2U)
99 #define ICSSG_MAX_NUM_BUFFER_POOLS (24U)
102 #define ICSSG_DUALMAC_TX_CH_NUM (4U)
105 #define ICSSG_DUALMAC_RX_FLOW_NUM (8U)
108 #define ICSSG_SWITCH_TX_CH_NUM (8U)
111 #define ICSSG_SWITCH_RX_FLOW_NUM (8U)
114 #define ICSSG_DUALMAC_PORT_BUFFER_POOL_NUM (0U)
117 #define ICSSG_DUALMAC_HOST_BUFFER_POOL_NUM (8U)
120 #define ICSSG_DUALMAC_HOST_EGRESS_QUEUE_NUM (2U)
123 #define ICSSG_SWITCH_PORT_BUFFER_POOL_NUM (8U)
126 #define ICSSG_SWITCH_HOST_BUFFER_POOL_NUM (16U)
129 #define ICSSG_SWITCH_HOST_EGRESS_QUEUE_NUM (2U)
132 #define ICSSG_HOST_EGRESS_BUFFER_PADDING (2048U)
135 #define ICSSG_SCRATCH_BUFFER_SIZE (2048U)
149 #define ICSSG_FDB_ENTRY_P0_MEMBERSHIP (ENET_BIT(0U))
156 #define ICSSG_FDB_ENTRY_P1_MEMBERSHIP (ENET_BIT(1U))
163 #define ICSSG_FDB_ENTRY_P2_MEMBERSHIP (ENET_BIT(2U))
170 #define ICSSG_FDB_ENTRY_AGEABLE (ENET_BIT(3U))
178 #define ICSSG_FDB_ENTRY_BLOCK (ENET_BIT(4U))
185 #define ICSSG_FDB_ENTRY_SECURE (ENET_BIT(5U))
193 #define ICSSG_FDB_ENTRY_TOUCHED (ENET_BIT(6U))
200 #define ICSSG_FDB_ENTRY_VALID (ENET_BIT(7U))
206 #define ICSSG_RATE_SRC_SEL_FT1_MATCH0 (0U)
207 #define ICSSG_RATE_SRC_SEL_FT1_MATCH1 (1U)
208 #define ICSSG_RATE_SRC_SEL_FT1_MATCH2 (2U)
209 #define ICSSG_RATE_SRC_SEL_FT1_MATCH3 (3U)
210 #define ICSSG_RATE_SRC_SEL_FT1_MATCH4 (4U)
211 #define ICSSG_RATE_SRC_SEL_FT1_MATCH5 (5U)
212 #define ICSSG_RATE_SRC_SEL_FT1_MATCH6 (6U)
213 #define ICSSG_RATE_SRC_SEL_FT1_MATCH7 (7U)
214 #define ICSSG_RATE_SRC_SEL_FT3_MATCH0 (8U)
215 #define ICSSG_RATE_SRC_SEL_FT3_MATCH1 (9U)
216 #define ICSSG_RATE_SRC_SEL_FT3_MATCH2 (10U)
217 #define ICSSG_RATE_SRC_SEL_FT3_MATCH3 (11U)
218 #define ICSSG_RATE_SRC_SEL_FT3_MATCH4 (12U)
219 #define ICSSG_RATE_SRC_SEL_FT3_MATCH5 (13U)
220 #define ICSSG_RATE_SRC_SEL_FT3_MATCH6 (14U)
221 #define ICSSG_RATE_SRC_SEL_FT3_MATCH7 (15U)
222 #define ICSSG_RATE_SRC_SEL_FT3_MATCH8 (16U)
223 #define ICSSG_RATE_SRC_SEL_FT3_MATCH9 (17U)
224 #define ICSSG_RATE_SRC_SEL_FT3_MATCH10 (18U)
225 #define ICSSG_RATE_SRC_SEL_FT3_MATCH11 (19U)
226 #define ICSSG_RATE_SRC_SEL_FT3_MATCH12 (20U)
227 #define ICSSG_RATE_SRC_SEL_FT3_MATCH13 (21U)
228 #define ICSSG_RATE_SRC_SEL_FT3_MATCH14 (22U)
229 #define ICSSG_RATE_SRC_SEL_FT3_MATCH15 (23U)
230 #define ICSSG_RATE_SRC_SEL_FT_RX_UC (24U)
231 #define ICSSG_RATE_SRC_SEL_FT_RX_MC (25U)
232 #define ICSSG_RATE_SRC_SEL_FT_RX_BC (26U)
233 #define ICSSG_RATE_SRC_SEL_FT_RX_SAV (27U)
234 #define ICSSG_RATE_SRC_SEL_FT_RX_FWD (28U)
235 #define ICSSG_RATE_SRC_SEL_FT_RX_RCV (29U)
236 #define ICSSG_RATE_SRC_SEL_FT_RX_VLAN (30U)
237 #define ICSSG_RATE_SRC_SEL_FT_RX_DA_P (31U)
238 #define ICSSG_RATE_SRC_SEL_FT_RX_DA_I (32U)
239 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW0 (33U)
240 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW1 (34U)
241 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW2 (35U)
242 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW3 (36U)
243 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW4 (37U)
244 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW5 (38U)
245 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW6 (39U)
246 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW7 (40U)
247 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW8 (41U)
248 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW9 (42U)
249 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW10 (43U)
250 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW11 (44U)
251 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW12 (45U)
252 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW13 (46U)
253 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW14 (47U)
254 #define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW15 (48U)
257 #define ICCSG_RX_CLASS_DATA_FT3_MATCH0 (0U)
258 #define ICCSG_RX_CLASS_DATA_FT3_MATCH1 (1U)
259 #define ICCSG_RX_CLASS_DATA_FT3_MATCH2 (2U)
260 #define ICCSG_RX_CLASS_DATA_FT3_MATCH3 (3U)
261 #define ICCSG_RX_CLASS_DATA_FT3_MATCH4 (4U)
262 #define ICCSG_RX_CLASS_DATA_FT3_MATCH5 (5U)
263 #define ICCSG_RX_CLASS_DATA_FT3_MATCH6 (6U)
264 #define ICCSG_RX_CLASS_DATA_FT3_MATCH7 (7U)
265 #define ICCSG_RX_CLASS_DATA_FT3_MATCH8 (8U)
266 #define ICCSG_RX_CLASS_DATA_FT3_MATCH9 (9U)
267 #define ICCSG_RX_CLASS_DATA_FT3_MATCH10 (10U)
268 #define ICCSG_RX_CLASS_DATA_FT3_MATCH11 (11U)
269 #define ICCSG_RX_CLASS_DATA_FT3_MATCH12 (12U)
270 #define ICCSG_RX_CLASS_DATA_FT3_MATCH13 (13U)
271 #define ICCSG_RX_CLASS_DATA_FT3_MATCH14 (14U)
272 #define ICCSG_RX_CLASS_DATA_FT3_MATCH15 (15U)
273 #define ICCSG_RX_CLASS_DATA_FT1_MATCH0 (16U)
274 #define ICCSG_RX_CLASS_DATA_FT1_MATCH1 (17U)
275 #define ICCSG_RX_CLASS_DATA_FT1_MATCH2 (18U)
276 #define ICCSG_RX_CLASS_DATA_FT1_MATCH3 (19U)
277 #define ICCSG_RX_CLASS_DATA_FT1_MATCH4 (20U)
278 #define ICCSG_RX_CLASS_DATA_FT1_MATCH5 (21U)
279 #define ICCSG_RX_CLASS_DATA_FT1_MATCH6 (22U)
280 #define ICCSG_RX_CLASS_DATA_FT1_MATCH7 (23U)
281 #define ICCSG_RX_CLASS_DATA_FT_RX_DA_I (24U)
282 #define ICCSG_RX_CLASS_DATA_FT_RX_DA_P (25U)
283 #define ICCSG_RX_CLASS_DATA_FT_RX_VLAN (26U)
284 #define ICCSG_RX_CLASS_DATA_FT_RX_RCV (27U)
285 #define ICCSG_RX_CLASS_DATA_FT_RX_FWD (28U)
286 #define ICCSG_RX_CLASS_DATA_FT_RX_BC (29U)
287 #define ICCSG_RX_CLASS_DATA_FT_RX_MC (30U)
288 #define ICCSG_RX_CLASS_DATA_FT_RX_SAV (31U)
297 typedef enum Icssg_Instance_Num_e
313 typedef struct Icssg_TxTsEvtCbInfo_s
326 typedef enum Icssg_Ioctl_e
708 typedef enum Icssg_QueuePreemptMode_e
720 typedef enum Icssg_QueueForwardMode_e
732 typedef enum Icssg_PortState_e
767 typedef struct IcssgMacPort_SetPortStateInArgs_s
779 typedef enum Icssg_AcceptFrameCheck_e
794 typedef struct Icssg_SetAcceptFrameCheckInArgs_s
806 typedef struct Icssg_MacAddr_s
815 typedef struct IcssgMacPort_SetMacAddressInArgs_s
828 typedef struct IcssgMacPort_PreemptSetMinFragSizeRemoteInArgs_s
840 typedef struct Icssg_VlanFidParams_s
877 typedef struct Icssg_VlanFidEntry_s
889 typedef struct Icssg_FdbEntry_s
905 typedef enum Icssg_PreemptVerifyState_e
929 typedef struct Icssg_DfltVlanCfg_s
944 typedef struct Icssg_MacPortDfltVlanCfgInArgs_s
957 typedef struct Icssg_IngressRateLim_s
1007 typedef struct Icssg_FwPoolMem_s
1058 typedef struct Icssg_Cfg_s
1091 typedef struct IccsgMacPort_Cfg_s
@ ICSSG_QUEUE_FORWARD_MODE_STOREANDFWD
Definition: icssg.h:723
@ ICSSG_MACPORT_IOCTL_ENABLE_MCAST_FLOOD
Enable flooding of multicast packets to host port.
Definition: icssg.h:664
uint8_t type
Definition: icssg.h:972
uint32_t Icssg_getSliceNum(Enet_Type enetType, uint32_t instId, Enet_MacPort macPort)
@ ICSSG_MACPORT_IOCTL_DISABLE_MCAST_FLOOD
Disable flooding of multicast packets to host port.
Definition: icssg.h:675
@ ICSSG_QUEUE_FORWARD_MODE_CUTTHROUGH
Definition: icssg.h:726
@ ICSSG_PORT_STATE_TAS_ENABLE
Definition: icssg.h:755
@ ICSSG_ACCEPT_ALL
Definition: icssg.h:788
@ ICSSG_VERIFYSTATE_FAILED
Definition: icssg.h:920
uint64_t agingPeriod
Definition: icssg.h:1061
uint32_t classDataOrTerm
Definition: icssg.h:969
@ ICSSG_MACPORT_IOCTL_PREEMPT_SET_MIN_FRAG_SIZE_REMOTE
Add minimum fragment size.
Definition: icssg.h:557
uint16_t ft1Start
Definition: icssg.h:973
@ ICSSG_ACCEPT_ONLY_UNTAGGED_PRIO_TAGGED
Definition: icssg.h:785
ICSSG buffer pool memories.
Definition: icssg.h:1008
@ ICSSG_FDB_IOCTL_SET_AGING_PERIOD
Set the aging period of the FDB.
Definition: icssg.h:631
Enet_MacPort macPort
Definition: icssg.h:770
@ ICSSG_PER_IOCTL_TAS_TRIGGER
Definition: icssg.h:574
@ ICSSG_PORT_STATE_TAS_TRIGGER
Definition: icssg.h:752
@ ICSSG_VERIFYSTATE_INITIAL
Definition: icssg.h:911
@ ICSSG_VERIFYSTATE_SUCCEEDED
Definition: icssg.h:917
EnetMacPort_Interface mii
Definition: icssg.h:1082
This file contains the type definitions and helper macros for the MDIO module interface.
Enet_MacPort macPort
Definition: icssg.h:818
Icssg TX timestamp event callback info structure. This is passed to application when TX timestamp is ...
Definition: icssg.h:314
VLAN configuration parameters.
Definition: enet_mod_port.h:68
uint32_t start
Definition: icssg.h:984
@ ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM
Configure ingress rate limiting.
Definition: icssg.h:702
uint8_t * hostBufferPoolMem
Definition: icssg.h:1021
bool mcastFloodEn
Definition: icssg.h:1100
Enet_MacPort macPort
Definition: icssg.h:831
This file contains the type definitions and helper macros for ICSSG Statistics interface.
Icssg_QueueForwardMode
Queue forward mode: cut-through or store-and-forward.
Definition: icssg.h:721
@ ICSSG_MACPORT_IOCTL_ENABLE_UCAST_FLOOD
Enable flooding of unicast packets to host port.
Definition: icssg.h:642
@ ICSSG_MACPORT_IOCTL_DISABLE_PROMISC_MODE
Disable promiscuous mode.
Definition: icssg.h:348
@ ICSSG_VERIFYSTATE_UNKNOWN
Definition: icssg.h:908
bool floodToHost
Definition: icssg.h:871
uint32_t hostEgressPreQueueSize
Definition: icssg.h:1043
uint8_t classIndex
Definition: icssg.h:965
uint32_t len
Definition: icssg.h:988
Input args for ICSSG_MACPORT_IOCTL_PREEMPT_SET_MIN_FRAG_SIZE_REMOTE command.
Definition: icssg.h:829
bool p1Member
Definition: icssg.h:850
Enet_MacPort
MAC port.
Definition: enet_types.h:406
Mdio_Cfg mdioCfg
Definition: icssg.h:1076
@ ICSSG_PER_IOCTL_VLAN_SET_ENTRY
Update a VLAN table entry.
Definition: icssg.h:370
bool hostTagged
Definition: icssg.h:857
MAC address.
Definition: icssg.h:807
@ ICSSG_QUEUE_PREEMPT_MODE_PREEMPT
Definition: icssg.h:714
@ ICSSG_MACPORT_IOCTL_PREEMPT_GET_MIN_FRAG_SIZE_LOCAL
Get minimum fragment size supported by firmware.
Definition: icssg.h:546
uint8_t * hostEgressQueueMem
Definition: icssg.h:1031
uint32_t jmpOffset
Definition: icssg.h:987
uint32_t hostBufferPoolSize
Definition: icssg.h:1024
uint32_t typeMask
Definition: icssg.h:991
Enet_MacPort macPort
Definition: icssg.h:932
Icssg_AcceptFrameCheck acceptFrameCheck
Definition: icssg.h:800
EnetPort_VlanCfg vlanCfg
Definition: icssg.h:1064
@ ICSSG_PER_IOCTL_TAS_ENABLE
Definition: icssg.h:580
This file contains the type definitions and helper macros for the Ethernet PHY interface.
VLAN FID table entry.
Definition: icssg.h:878
Resource manager configuration parameters.
Definition: enet_rm.h:337
@ ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK
Set the criteria for accepting VLAN tagged/untagged packets.
Definition: icssg.h:691
const void * dmaCfg
Definition: icssg.h:1070
uint32_t scratchBufferSize
Definition: icssg.h:1052
Icssg_Ioctl
ICSSG IOCTL commands.
Definition: icssg.h:327
ICSSG mac port configuration parameters.
Definition: icssg.h:1092
@ ICSSG_PORT_STATE_TAS_RESET
Definition: icssg.h:758
@ ICSSG_PER_IOCTL_TAS_DISABLE
Definition: icssg.h:586
@ ICSSG_PER_IOCTL_VLAN_RESET_TABLE
Populate VLAN table with default VLAN entry configuration.
Definition: icssg.h:359
@ ICSSG_MACPORT_IOCTL_PREEMPT_GET_TX_ACTIVE_STATUS
Get status of whether preemption is active or not.
Definition: icssg.h:502
Input arguments for ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID command.
Definition: icssg.h:945
bool p1Tagged
Definition: icssg.h:861
uint8_t fid
Definition: icssg.h:844
#define ICSSG_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for ICSSG per.
Definition: icssg.h:74
uint32_t portBufferPoolNum
Definition: icssg.h:1017
EnetPort_VlanCfg vlanCfg
Definition: icssg.h:951
int16_t vlanId
Definition: icssg.h:895
@ ICSSG_MACPORT_IOCTL_PREEMPT_VERIFY_ENABLE
Enable verify state machine.
Definition: icssg.h:513
uint32_t rateLimit
Definition: icssg.h:962
@ ICSSG_PORT_STATE_TAS_DISABLE
Definition: icssg.h:761
@ ICSSG_MACPORT_IOCTL_PREEMPT_GET_VERIFY_STATE
Get current state of the verify state machine.
Definition: icssg.h:535
This file contains the type definitions and helper macros for the Ethernet PHY interface.
Icssg_PortState
Port states.
Definition: icssg.h:733
@ ICSSG_INSTANCE_NUM_1
Definition: icssg.h:303
uint32_t destAddrLow
Definition: icssg.h:978
@ ICSSG_PER_IOCTL_VLAN_SET_HOSTPORT_DFLT_VID
Set the default VLAN ID and PCP bits for host port.
Definition: icssg.h:607
Icssg_Instance_Num
ICSSG instance numbers.
Definition: icssg.h:298
MDIO module configuration.
Definition: networking/enet/core/include/mod/mdio.h:108
Icssg_PreemptVerifyState
Preemption Verify State Machine states.
Definition: icssg.h:906
@ ICSSG_MACPORT_IOCTL_PREEMPT_GET_TX_ENABLE_STATUS
Get status of preemption on TX.
Definition: icssg.h:491
Icssg_FwPoolMem * EnetCb_getFwPoolMem(Enet_Type enetType, uint32_t instId)
ICSSG memory pool callback function.
#define ENET_PRI_NUM
Packet priority.
Definition: enet_types.h:165
@ ICSSG_VERIFYSTATE_DISABLED
Definition: icssg.h:923
uint8_t notMask
Definition: icssg.h:966
@ ICSSG_FDB_IOCTL_REMOVE_ALL_ENTRIES
Delete all FDB entries.
Definition: icssg.h:436
MAC port interface.
Definition: enet_mod_macport.h:274
@ ICSSG_INSTANCE_NUM_0
Definition: icssg.h:300
Icssg_AcceptFrameCheck acceptFrameCheck
Definition: icssg.h:1103
uint64_t ts
Definition: icssg.h:320
uint8_t * hostEgressPreQueueMem
Definition: icssg.h:1035
Enet_MacPort macPort
Definition: icssg.h:947
uint32_t patternMaskHigh
Definition: icssg.h:995
uint32_t patternLow
Definition: icssg.h:992
@ ICSSG_PER_IOCTL_VLAN_GET_ENTRY
Get VLAN entry for VLAN table for requested VLAN id.
Definition: icssg.h:381
@ ICSSG_MACPORT_IOCTL_ENABLE_PROMISC_MODE
Enable promiscuous mode.
Definition: icssg.h:337
bool p2Tagged
Definition: icssg.h:865
VLAN FID entry parameters.
Definition: icssg.h:841
ICSSG peripheral configuration parameters.
Definition: icssg.h:1059
uint32_t hostEgressQueueNum
Definition: icssg.h:1046
EnetPort_VlanCfg vlanCfg
Definition: icssg.h:1106
@ ICSSG_PORT_STATE_FORWARD
Definition: icssg.h:746
Enet_Type
Ethernet peripheral type.
Definition: enet_types.h:196
bool streamVid
Definition: icssg.h:868
uint16_t preemptMinFrageSizeRemote
Definition: icssg.h:834
Input arguments for ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM command.
Definition: icssg.h:958
@ ICSSG_FDB_IOCTL_REMOVE_AGEABLE_ENTRIES
Remote all ageable entries.
Definition: icssg.h:447
Default VLAN configuration.
Definition: icssg.h:930
@ ICSSG_INSTANCE_NUM_2
Definition: icssg.h:306
uint16_t ft1Cfg
Definition: icssg.h:975
@ ICSSG_PER_IOCTL_TAS_RESET
Definition: icssg.h:592
@ ICSSG_PER_IOCTL_SET_PORT_STATE
Set port state.
Definition: icssg.h:403
uint32_t hostEgressQueueSize
Definition: icssg.h:1039
Icssg_VlanFidParams vlanFidParams
Definition: icssg.h:883
Icssg_AcceptFrameCheck
Acceptable frame check criteria.
Definition: icssg.h:780
void IcssgMacPort_initCfg(IcssgMacPort_Cfg *macPortCfg)
@ ICSSG_MACPORT_IOCTL_PREEMPT_VERIFY_DISABLE
Disable verify state machine.
Definition: icssg.h:524
Icssg_PortState portState
Definition: icssg.h:773
uint32_t patternMaskLow
Definition: icssg.h:994
Input args for ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK command.
Definition: icssg.h:795
TimeSync configuration parameters.
Definition: icssg_timesync.h:93
@ ICSSG_PORT_STATE_DISABLED
Definition: icssg.h:736
EnetRm_ResCfg resCfg
Definition: icssg.h:1073
uint32_t startLen
Definition: icssg.h:986
@ ICSSG_PORT_STATE_FORWARD_WO_LEARNING
Definition: icssg.h:749
bool ucastFloodEn
Definition: icssg.h:1097
uint32_t rateSrcSel
Definition: icssg.h:963
@ ICSSG_ACCEPT_ONLY_VLAN_TAGGED
Definition: icssg.h:782
uint16_t vlanId
Definition: icssg.h:935
uint8_t rateIndex
Definition: icssg.h:964
@ ICSSG_FDB_IOCTL_ADD_ENTRY
Add FDB entry.
Definition: icssg.h:414
@ ICSSG_MACPORT_IOCTL_DISABLE_UCAST_FLOOD
Disable flooding of unicast packets to host port.
Definition: icssg.h:653
uint8_t * scratchBufferMem
Definition: icssg.h:1049
uint32_t destAddrMaskLow
Definition: icssg.h:980
uint16_t ft1Len
Definition: icssg.h:974
@ ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID
Set the default VLAN ID and PCP bits for specified MAC port.
Definition: icssg.h:618
uint8_t classSel
Definition: icssg.h:967
uint8_t pcp
Definition: icssg.h:938
@ ICSSG_QUEUE_PREEMPT_MODE_EXPRESS
Definition: icssg.h:711
This file contains the type definitions and helper macros for ICSSG TimeSync.
@ ICSSG_PORT_STATE_BLOCKING
Definition: icssg.h:741
bool promiscEn
Definition: icssg.h:1094
uint32_t portBufferPoolSize
Definition: icssg.h:1014
Input args for ICSSG_MACPORT_IOCTL_SET_PORT_STATE command.
Definition: icssg.h:768
#define ENET_MAC_ADDR_LEN
MAC address length in bytes/octets.
Definition: enet_types.h:153
uint32_t txTsId
Definition: icssg.h:317
@ ICSSG_MACPORT_IOCTL_SET_MACADDR
Add MAC address of the interface.
Definition: icssg.h:458
@ ICSSG_FDB_IOCTL_REMOVE_ENTRY
Delete FDB entry.
Definition: icssg.h:425
uint32_t destAddrMaskHigh
Definition: icssg.h:981
uint32_t patternHigh
Definition: icssg.h:993
IcssgTimeSync_Cfg timeSyncCfg
Definition: icssg.h:1079
uint16_t vlanId
Definition: icssg.h:880
@ ICSSG_MACPORT_IOCTL_PREEMPT_TX_DISABLE
Disable preemption on TX.
Definition: icssg.h:480
uint32_t config
Definition: icssg.h:989
@ ICSSG_HOSTPORT_IOCTL_SET_MACADDR
Add MAC address of the host port interface.
Definition: icssg.h:568
uint32_t cycleTimeNs
Definition: icssg.h:1085
Icssg_QueuePreemptMode
Queue preemptive mode: express or preemptive.
Definition: icssg.h:709
uint8_t * portBufferPoolMem
Definition: icssg.h:1011
Enet_MacPort macPort
Definition: icssg.h:960
bool p2Member
Definition: icssg.h:853
uint32_t hostBufferPoolNum
Definition: icssg.h:1027
uint32_t destAddrHigh
Definition: icssg.h:979
bool hostMember
Definition: icssg.h:847
FDB entry configuration.
Definition: icssg.h:890
uint8_t index
Definition: icssg.h:971
uint32_t classDataAndTerm
Definition: icssg.h:968
@ ICSSG_VERIFYSTATE_VERIFYING
Definition: icssg.h:914
uint32_t startAuto
Definition: icssg.h:985
uint32_t type
Definition: icssg.h:990
Input args for ICSSG_MACPORT_IOCTL_SET_MACADDR command.
Definition: icssg.h:816
@ ICSSG_MACPORT_IOCTL_PREEMPT_TX_ENABLE
Enable preemption on TX.
Definition: icssg.h:469
uint8_t specialFramePrio
Definition: icssg.h:1114
Enet_MacPort macPort
Definition: icssg.h:797