![Logo](ti_logo.svg) |
AM263x MCU+ SDK
08.02.01
|
|
Go to the documentation of this file.
81 #define MDIO_MAX_PHY_CNT (31U)
90 typedef enum Mdio_OpMode_e
107 typedef struct Mdio_Cfg_s
uint32_t c45EnMask
Definition: networking/enet/core/include/mod/mdio.h:126
Mdio_OpMode mode
Definition: networking/enet/core/include/mod/mdio.h:110
This file contains the type definitions and helper macros for the Enet MDIO module.
Mdio_OpMode
MDIO operating mode.
Definition: networking/enet/core/include/mod/mdio.h:91
uint32_t phyStatePollFreqHz
Definition: networking/enet/core/include/mod/mdio.h:116
void Mdio_initCfg(Mdio_Cfg *mdioCfg)
Initialize MDIO configuration parameters.
@ MDIO_MODE_MANUAL
Definition: networking/enet/core/include/mod/mdio.h:99
@ MDIO_MODE_NORMAL
Definition: networking/enet/core/include/mod/mdio.h:93
MDIO module configuration.
Definition: networking/enet/core/include/mod/mdio.h:108
uint32_t mdioBusFreqHz
Definition: networking/enet/core/include/mod/mdio.h:113
bool isMaster
Definition: networking/enet/core/include/mod/mdio.h:134
uint32_t pollEnMask
Definition: networking/enet/core/include/mod/mdio.h:122
@ MDIO_MODE_STATE_CHANGE_MON
Definition: networking/enet/core/include/mod/mdio.h:96