MCSPI channel object.
Data Fields | |
| MCSPI_ChConfig | chCfg |
| uint32_t | isOpen |
| const uint8_t * | curTxBufPtr |
| uint8_t * | curRxBufPtr |
| uint32_t | curTxWords |
| uint32_t | curRxWords |
| uint8_t | bufWidthShift |
| uint32_t | dataWidthBitMask |
| uint32_t | txFifoTrigLvl |
| uint32_t | rxFifoTrigLvl |
| uint32_t | effTxFifoDepth |
| uint32_t | effRxFifoDepth |
| uint32_t | intrMask |
| MCSPI_ChConfig MCSPI_ChObject::chCfg |
Channel configuration as provided by user
| uint32_t MCSPI_ChObject::isOpen |
Flag to indicate whether the instance is opened already
| const uint8_t* MCSPI_ChObject::curTxBufPtr |
Current TX buffer pointer
| uint8_t* MCSPI_ChObject::curRxBufPtr |
Current RX buffer pointer
| uint32_t MCSPI_ChObject::curTxWords |
Number of words transmitted. We need seperate counters for TX/RX because when FIFO in enabled, TX writes happen in advance where as RX will happen on actual received data.
| uint32_t MCSPI_ChObject::curRxWords |
Number of words received
| uint8_t MCSPI_ChObject::bufWidthShift |
Width of buffer in bytes - used for accessing the TX/RX buffer. When dataWidth <= 8, bufWidth = uint8_t (1 byte - 0 shift) When dataWidth > 8 && <= 16, bufWidth = uint16_t (2 bytes - 1 shift) When dataWidth > 16 && <= 32, bufWidth = uint32_t (4 bytes - 2 shift)
| uint32_t MCSPI_ChObject::dataWidthBitMask |
Data width mask depending on SPI word size
| uint32_t MCSPI_ChObject::txFifoTrigLvl |
TX FIFO trigger level in bytes
| uint32_t MCSPI_ChObject::rxFifoTrigLvl |
RX FIFO trigger level in bytes
| uint32_t MCSPI_ChObject::effTxFifoDepth |
Effective TX FIFO depth in words - depends on dataWidth
| uint32_t MCSPI_ChObject::effRxFifoDepth |
Effective RX FIFO depth in words - depends on dataWidth
| uint32_t MCSPI_ChObject::intrMask |
Interrupt mask to be used for enabling / checking interrupts.