Features Supported
- APIs to setup region based address translation using RAT HW on supported SOCs
- APIs to translate 48b SOC view system addr to 32b local CPU view address.
- When no address mapping is specified, no translation is done.
Features NOT Supported
NA
Important Usage Guidelines
- The translation API AddrTranslateP_getLocalAddr is meant to be used to translate SOC specified peripheral MMR base addresses to local CPU accesible addresses, within device drivers. The API internally searches through a small array to find the address translations, hence to be efficient, this API should typically be called once during driver init to find the local address that CPU should use.
- This module is not normally required on R5F CPUs since all peripherals are typically mapped within the 32b address space of R5F.
- This module is needed for M4F to access peripherals on the MainSS side of the SOC.
Example Usage
Include the below file to access the APIs,
Example to translate a system address to local CPU address,
uint64_t systemAddr = 0x029060000ul;
void *localAddr;
API
APIs for Region based address translation (RAT) module