![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.02.00
|
|
uint16_t ddrssCtlRegCount
Definition: ddr/v0/ddr.h:93
uint16_t * ddrssPhyRegNum
Definition: ddr/v0/ddr.h:91
uint32_t * ddrssPhyReg
Definition: ddr/v0/ddr.h:87
uint16_t ddrssPhyRegCount
Definition: ddr/v0/ddr.h:95
void DDR_Params_init(DDR_Params *prms)
Set default values to DDR_Params.
uint64_t clk2Freq
Definition: ddr/v0/ddr.h:83
uint32_t * ddrssPhyIndepReg
Definition: ddr/v0/ddr.h:86
uint16_t ddrssPhyIndepRegCount
Definition: ddr/v0/ddr.h:94
uint8_t fshcount
Definition: ddr/v0/ddr.h:97
uint16_t * ddrssPhyIndepRegNum
Definition: ddr/v0/ddr.h:90
int32_t DDR_init(DDR_Params *prms)
DDR4 Initialization function.
uint64_t clk1Freq
Definition: ddr/v0/ddr.h:82
DDR config structure.
Definition: ddr/v0/ddr.h:81
uint16_t * ddrssCtlRegNum
Definition: ddr/v0/ddr.h:89
uint32_t * ddrssCtlReg
Definition: ddr/v0/ddr.h:85