Presence And Motion Users Guide
Table of Contents
Introduction
The Presence and Motion Detection Demo is the TI mmWave SDK5 out-of-box demo project for low power architecture EVMs, like the xWRL6432 and xWRL1432. It is designed to showcase the capabilities of TI’s mmWave low power sensors by using the SDK5 APIs and tools to form an application that includes device configuration, processing, and visualization of the processed data.
You can choose between two visualizer tools provided by TI for this demo:
- MMWAVE-L-SDK (SDK 5.x.x.x) Low Power Visualizer
- Found in the SDK, this visualizer enables quick configuration and visualization of the data from SDK5 devices.
- To get started, follow the Using the SDK Low Power Visualizer section below.
- Radar Toolbox Industrial Visualizer
- A more configurable, general-purpose visualizer that provides more control over configuration and visualization, supports more demos, and supports more devices
- To get started, follow the Using the Radar Toolbox Industrial Visualizer section below.
Quickstart xWRLx432 Device
Requirements
| Tool | Version | Download Link |
|---|---|---|
| XDS110 Drivers | Latest | XDS Emulation Software |
| TI mmWave SDK | 5.x.x.x (xWRLx432) | MMWAVE-L-SDK 5.x.x.x |
| UniFlash | Latest | Download UniFlash Access UniFlash through the Cloud |
Using the SDK Low Power Visualizer
1. Connect the device to the PC
Connect your EVM to the micro USB port. You do not need to connect to the barrel jack.
2. Open the MMWAVE-L-SDK Low Power Visualizer
Navigate to the MMWAVE-L-SDK download location and find the Low Power Radar Visualizer at <MMWAVE_SDK5_INSTALL_DIR>\tools\visualizer\Low_power_visualizer_5.x.x.x\visualizer.exe
3. Flash the EVM using the SDK Low Power Visualizer
On the “Flash” tab in the visualizer, follow the steps listed.
Select the COM Port. It should be automatically detected. If not, look for the “XDS110 Class Application/User UART” COM port in your Device Manager, and select this port in the GUI. If you do not see this, you need to install the XDS 110 drivers listed in the Requirements section above.
Select the baud rate. It should be automatically detected.
Select the device in the drop down. It should be automatically detected.
Configure the EVM for Flashing Mode. For more help on device setup, follow the steps in the EVM Setup Guide for your specific EVM.
Place the device into Flashing Mode by setting the switches as shown in the visualizer.
Then, toggle the reset button (circled in green) to latch in the mode.
Press “SWITCH SETTINGS CONFIRMED”
Upload the application image which can be found at
<MMWAVE_SDK5_INSTALL_DIR>\examples\mmw_demo\motion_and_presence_detection\prebuilt_binariesSelect the “FLASH” button. Upon a successful flash, you see the following appear on the bottom of the flashing page:
4. Configure the EVM for Functional Mode
Navigate to the SDK download location and find the Low Power Radar Visualizer at <MMWAVE_SDK5_INSTALL_DIR>\tools\visualizer\Low_power_visualizer_5.x.x.x\visualizer.exe
Move to the “Configuration Dashboard” tab in the visualizer. A pop up will appear which instructs switching the device into functional mode, follow the instructions.
Place the device into Functional Mode by setting the switches as shown in the visualizer. For more help on device setup, follow the steps in the EVM Setup Guide for your specific EVM.
Then, toggle the reset button (circled in green) to latch in the mode.
5. Send Device Configuration
In the “Configuration Dashboard” tab, first confirm the COM port and baud rate are correct. Then, under “Configuration Selection”, select “High Performance Motion Detection”, “Low Power Presence Detection”, “Automated Parking”, or “Object Tracking”. Select “Send Selected Config”. Optionally, the user can load a custom configuration file from their local PC. Use the “Load Config from PC” button to accomplish this.
📝 NOTE
Only the Presence Detection configuration enables the enhanced presence and motion features by default. Please refer to<MMWAVE_SDK5_INSTALL_DIR>\docs\MotionPresenceDetectionDemo_documentation.pdffor more information about enabling these enhanced features through the CLI command guiMonitor.
In the visualizer’s console window commands should be seen being sent to the device.
6. View Plots
Once commands are sent, users can view the Presence Detection plot on the same page (if presence detection is enabled) Users can view other plots in the “Plots” tab. Checkboxes on the left allow control of the visualization.
Using the Radar Toolbox Industrial Visualizer
1. Configure the EVM for Flashing Mode
Connect your EVM to the micro USB port and follow the steps below. You do not need to connect to the barrel jack.
Place the device into Flashing Mode by setting the switches as shown.
Then, toggle the reset button (circled in green) to latch in the mode.
2. Flash the EVM using Uniflash
Flash the appropriate binary from the prebuilt binaries folder using UniFlash. Follow the instructions for using UniFlash Prebuilt release binaries can be found in <MMWAVE_SDK5_INSTALL_DIR>\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries
3. Configure the EVM for Functional Mode
Place the device into Functional Mode by setting the switches as shown in the viualizer. For more help on device setup, follow the steps in the EVM Setup Guide for your specific EVM.
Then, toggle the reset button (circled in green) to latch in the mode.
4. Open the Radar Toolbox Industrial Visualizer
Navigate to the Radar Toolbox download location and find the Industrial Visualizer directory at <RADAR_TOOLBOX_INSTALL_DIR>\tools\visualizers\Industrial_Visualizer\. Then, run the visualizer either directly from source with python gui_main.py, or as an executable by running the mmWaveIndustrialVisualizer.exe
📝 NOTE
In general, running the visualizer from the Python source runs faster and results in fewer errors over long periods of time. If running Python directly from source, use Python version 3.7.3, and run the setUpEnvironment.bat script first to ensure all the correct packages and versions are installed.
5. Connect the Device
Look for the “XDS110 Class Application/User UART” COM port in your Device Manager, and select this port in the GUI. If you do not see this, you need to install the XDS110 drivers listed in the Requirements section above.
Make sure the correct device is selected and choose the COM port found in the previous step, and then select “Connect”.
6. Send Device Configuration
In the “Configuration” section, click on “Select Configuration”. Select one of the pre-written configurations in <RADAR_TOOLBOX_INSTALL_DIR>\source\ti\examples\Presence_and_Motion_Detection\chirp_configs\. Then, click “Start and Send Configuration” In the visualizer’s console window commands should be seen being sent to the device.
7. View Plots
Once commands are sent, users can view the point cloud plot on the same page (if presence detection is enabled). Please refer to the Industrial Visualizer Documentation located at <RADAR_TOOLBOX_INSTALL_DIR>\tools\visualizers\Industrial_Visualizer\docs\mmWave_Industrial_Visualizer_User_Guide.html for more information about how to use this tool.
Getting Started Tuning the Device
For information about getting started tuning the performance of the sensor, please see the mmWave SDK5 Presence and Motion Tuning Guide: <MMWAVE_SDK5_INSTALL_DIR>/docs/MotionPresenceDetectionDemo_TuningGuide.pdf
Build the Firmware from Source Code
1. Software Requirements
| Tool | Version | Download Link |
|---|---|---|
| TI mmWave SDK | 5.x.x.x (xWRLx432) | mmWave SDK 5.x.x.x |
| Code Composer Studio | CCS 12.2 or later | Code Composer Studio |
| XDS110 Drivers | Latest | XDS Emulation Software |
2. Import Project
The mmWave SDK Presence and Motion Detection Demo CCS Project is available on TI Resource Explorer under mmWave Sensors → Radar Toolbox. You can import the project in your CCS workspace using TI Resource Explorer in CCS or by importing the projectspec from a local copy of the toolbox. Both methods of importing projects are defined below. To get started, open CCS and set up your workspace as desired.
Importing via TI Resource Explorer in CCS
- In the top toolbar, navigate to View → Resource Explorer
- In the Resource Explorer side panel (not the main panel with “Welcome to..”), navigate to Software → mmWave Sensors → Radar Toolbox - <ver> → Example Projects →
- Select the Presence and Motion Detection Demo, and then choose the appropriate project for your specific device or EVM
- Click on the project, which should open the project in the right main panel, and then click on the Import to IDE button
.
Importing via CCS Import Projectspecs
- In the top toolbar, navigate to Project → Import CCS Projects…
- With the Select search-directory option enabled, click Browse…, navigate to the Presence_and_Motion_Detection folder at
<RADAR_TOOLBOX_INSTALL_DIR>\source\ti\examples\Presence_and_Motion_Detection\and then click OK.
- Under Discovered projects, select the appropriate project for your device or EVM then click Finish.
📝 NOTE
Project Workspace
When importing projects to a workspace, a copy is created in the workspace. It is important to note that the copy in user’s workspace is the one that gets built and all modifications will only be implemented for the workspace copy. The original project downloaded in the Radar Toolbox is not modified.
3. Build the Project
There is only one project in Project Explorer, right click on the project name and select Rebuild Project.
🛑 Before Continuing!
Build Fails with Errors
If the build fails with errors, please ensure that all the prerequisites are installed as mentioned in the previous steps.
4. Execute the Project
There are two ways to execute the compiled code on the EVM:
- Deployment mode: In this mode, the EVM boots autonomously from flash and starts running the bin image
- Using UniFlash, flash the .bin file (typically in the Debug folder, but the folder name will depend on the project’s configuration)
- The procedure to flash the EVM is the same as detailed in the Flash the EVM section.
- Debug mode: This mode is used for downloading and running the executable (.out) from CCS. This mode enables JTAG connection with CCS while project is running; useful during development and debugging. Follow the instructions at CCS Debug Mode.
Understanding Output Data Formats
The Low Power Visualizer and Industrial Visualizer are used to visualize processed output data from the mmWave radar device. This data is processed on-chip, and packaged into a TLV format. To understand this format, reference Understanding UART Data Output. Additionally, raw ADC data can be saved for offline processing using the DCA1000 EVM.
📝 NOTE
Output Data versus Raw ADC Data
Output data refers to point cloud data (x,y,z,v). Raw ADC data refers to digitally sampled sensor data.
Need More Help?
- Additional resources in the documentation of the mmWave SDK:
- mmWave SDK5 Documentation
<MMWAVE_SDK5_INSTALL_DIR>/docs/MotionPresenceDetectionDemo_documentation.pdf - mmWave SDK5 Presence and Motion Tuning Guide
<MMWAVE_SDK5_INSTALL_DIR>/docs/MotionPresenceDetectionDemo_TuningGuide.pdf - mmWave SDK5 Presence and Motion Tracker Tuning Guide
<MMWAVE_SDK5_INSTALL_DIR>/docs/MotionPresenceDetectionDemo_GroupTracker_TuningGuide.pdf
- mmWave SDK5 Documentation
- Search for your issue or post a new question on the mmWave E2E forum