Skip to main content
Ctrl+K

SimpleLink™ basic_ble examples#

Texas Instruments

23 min read

Introduction#

This workshop offers a deeper dive in the basic_ble example project. Together with basic_ble_oad and basic_ble_ptm, the basic_ble is recommended as starting point for the development of your own system.

Prerequisites#

Hardware#

  • SimpleLink CC2340R5 LaunchPad Target

  • SimpleLink™ LaunchPad™ XDS110 Debugger

  • USB cable

  • SmartPhone or Tablet with a GATT Table viewer application installed (such as TI SimpleLink Connect app)

Note

Here are links to the TI SimpleLink Connect app

  • TI SimpleLink Connect on Apple App Store

  • TI SimpleLink Connect on Google App Store

Find the QR code to download the app below:

Apple_Google_QRCode

Software#

  • CCS 12.3 or IAR 9.32.1 installed with support for CC23xx devices.

  • SIMPLELINK-LOWPOWER-F3-SDK SimpleLink™ Software Development Kit

Agenda#

In this training, we will discuss how to get prepare the basic_ble example for custom development. First, we will discuss how to set up the environment. Afterwards, we will cover how to add a driver example project’s functionality into the basic_ble project along with showing how to interface these tasks together. We will also learn how to take control of the GATT table as well as the BLE5Stack within the basic_ble project.

Environment setup#

The following section will go through how to get the development environment up and running. You may skip this section if you already have your environment setup and working.

Initial Setup (Click here to expand)

All the collaterals required are available on TI website.

  1. Download and Install the SDK found in the software section above.

  2. Follow the Quick Start Guide found inside the BLE5 Stack User’s Guide

PATH =

  C:/ti/simplelink_lowpower_f3_sdk_x_xx_xx_xx/docs/ble5stack/ble_user_guide/html/quickstart-guide/quickstart-intro-cc23xx.html

Setting up the Serial terminal

If you already have a functional serial terminal setup skip this part and go directly to the following section.

  1. Identify the COM port used by the SimpleLink CC2340R5 LaunchPad.

  • Disconnect all the LaunchPads™ you may have connected to your computer leaving only the SimpleLink CC2340R5 LaunchPad.

  • Open the Device Manager. You can do so by typing Device Manager in the Windows start menu.

  • In the Device manager, find the menu Ports (COM & LPT) and unroll it.

  • Observe the line called XDS110 Class Application/User UART. Note down the COM port this interface is using. In my case (see below), the COM port used is called COM27.

../_images/identify_the_com_port_used.png

Identify the COM port used#

  1. Open a serial terminal to observe the COM port identified previously. For this example, I’ll show how to use the serial port provided by Code Composer Studio, but you can use your favorite serial terminal provider.

  • On CSS, click on View → Terminal, or use the shortcut Ctrl+Alt+Shift+T.

  • A pop-up allowing you to configure the terminal will appear. Select the following settings:

    • Choose Terminal: Serial Terminal

    • Serial Port: The serial port identified before (COM27 for me)

    • Baud rate: 115200

    • Data size: 8

    • Parity: None

    • Stop bits: 1

    • Encoding: Default (ISO-8859-1)

../_images/serial_terminal_setting.png

Set up the serial terminal#

  • Once done, click OK.

  • Display the Command Input Field by clicking on Toggle Command Input Field (see label 1), then clear the terminal content by clicking on Clear Terminal (see label 2)

../_images/ccs_serial_terminal.png

Code Composer Studio Serial Terminal#

  • To finish, reset the SimpleLink CC2340R5 LaunchPad by pressing the reset button on the emulator.

../_images/lp_reset.png

Reset#

Note

At this point open Code Composer Studio, create a new Workspace (don’t forget to add the workspace variable FREERTOS_INSTALL_DIR) and import the data_stream project. Then build and flash the code on the device.

If you need help for this, make sure to review Quick Start Guide!

“Merge” drivers examples into basic_ble#

Warning

This lab guides you through “the scenic” route to complete this task. There are more direct ways to “merge” this, but you would not see elements that could be useful for future use

  1. Prepare the environment

  • Import the basic_ble project example. File → Import → Code Composer Studio → CCS Projects

ImportBasicBLE

Browse to find the basic_ble project located at: C:\ti\simplelink_lowpower_f3_sdk_x_xx_xx_xx\examples\rtos\LP_EM_CC2340R5\ble5stack\basic_ble

  • Import the empty project example, making sure to select the same RTOS and Toolchain as for the basic_ble project example.

The empty project located at: C:\ti\simplelink_lowpower_f3_sdk_x_xx_xx_xx\examples\rtos\LP_EM_CC2340R5\drivers\empty

Note

All the code modifications will be done in the basic_ble project example.

  1. Copy the empty.c file

  • empty.cis available at the root of the empty project example

EmptyFile
  • Copy the file into the basic_ble project → app → empty.c

CopyEmpty
  1. Copy the code used for task creation

  • In order to keep the main() function in main_freertos.c clear, all task creations are deferred to other files. The same will be done for our new task.

  • In the newly created empty.c (in the basic_ble project), add the function emptyMain. This function can be placed at the end of the file.

  • Copy-paste into this function the code used in the empty project example to create the task. This code is located in the file main_freertos.c. Don’t forget to add all the includes, variable declarations and other global symbols to your file.

  • Make to ensure the Bluetooth® LE stack is always running with the highest priority. To do so, lower the priority assigned to the newly created task thread.

Header Files and Defines#
 /* POSIX Header files */
  #include <pthread.h>

 /* RTOS header files */
  #include <FreeRTOS.h>
  #include <task.h>

  /* Stack size in bytes */
  #define THREADSTACKSIZE 1024
Code to add in empty.cfile inside the basic_ble project. The emptyMain function handles task creation.#
  void emptyMain(void)
  {
      pthread_t thread;
      pthread_attr_t attrs;
      struct sched_param priParam;
      int retc;

      /* Initialize the attributes structure with default values */
      pthread_attr_init(&attrs);

      /* Set priority, detach state, and stack size attributes */
      priParam.sched_priority = 5; // Lower the priority of this task
      retc = pthread_attr_setschedparam(&attrs, &priParam);
      retc |= pthread_attr_setdetachstate(&attrs, PTHREAD_CREATE_DETACHED);
      retc |= pthread_attr_setstacksize(&attrs, THREADSTACKSIZE);
      if (retc != 0)
      {
          /* failed to set attributes */
          while (1) {}
      }

      retc = pthread_create(&thread, &attrs, mainThread, NULL);
      if (retc != 0)
      {
          /* pthread_create() failed */
          while (1) {}
      }
  }
  
  1. Call the newly added code from the main() function in main_freertos.c

  • main_freertos.cis available at the root of the basic_ble project example

  • Declare the emptyMain function as an extern function in main_freertos.c

The emptyMain function is declared as an extern function#
/*******************************************************************************
 * EXTERNS
 */
extern void appMain(void);
extern void AssertHandler(uint8 assertCause, uint8 assertSubcause);
extern void emptyMain(void); // Add this!
  • Call the emptyMain function right before turning on the RTOS

emptyMain() is called right before turning on the RTOS#
/* Initialize all applications tasks */
appMain();
emptyMain(); // Add this!

/* Start the FreeRTOS scheduler */
 vTaskStartScheduler();
  1. Port over the SysConfig configurations

  • Open the file empty.syscfg from the empty project example

  • Identify the drivers not enabled in the basic_ble project

Here only one instance of the GPIO driver (CONFIG_GPIO_LED_0) is missing in the basic_ble project.

CGPIOinSysconfig

In case you do not manage to identify the missing symbols, you can trigger a build and review the linking errors

  • Copy the missing configuration from empty.syscfg to basic_ble.syscfg in the basic_ble project.

Hint

At this point you can build and flash the code on the device. For more in depth instruction, make sure to review the Quick Start Guide!

Interface with the BLE5Stack#

This section presents methods for interfacing with the BLE5Stack. We will discuss using hook functions to signal other tasks of certain events occurring and and we will show how callbacks can be leveraged to make the device take certain actions.

First, we will be turning an LED off and on based on whenever the device is connected or disconnected.

  • Create a new instance of a GPIO module (the same way it was done for the section above). Name it CONFIG_GPIO_LED_1 and use the Green LaunchpadLED Hardware.

    GPIOGreenLED
  • Open the empty.c file. We will create and define the BLEConnectionEstablished and BLEConnectionTerminated functions here. These functions may be placed at the end of the empty.c file.

Copy these functions into empty.c#
/*********************************************************************
 * @fn      BLEConnectionEstablished
 *
 * @brief   Called when a Bluetooth connection has been established
 *          with a peer device.
 *
 * @param   None
 *
 * @return  None.
 */
void BLEConnectionEstablished(void)
{
// Indicate connection by turning on the green LED
GPIO_write(CONFIG_GPIO_LED_1, CONFIG_LED_ON);
}
/*********************************************************************
 * @fn      BLEConnectionTerminated
 *
 * @brief   Called when the Bluetooth connection has been terminated.
 *
 * @param   None
 *
 * @return  None.
 */
void BLEConnectionTerminated(void)
{
// Indicate disconnection by turning off the LED
GPIO_write(CONFIG_GPIO_LED_1, CONFIG_LED_OFF);
}
  • Open the app_peripheral.c file inside the app folder of the basic_ble project.

  • Add the following extern function declarations to give the app_peripheral.c file access to the newly created functions. The extern function declarations should be added near the top of the file, after the #include statements.

Example of Extern Function#
extern void BLEConnectionEstablished();
extern void BLEConnectionTerminated();
  • Call these functions in the Peripheral_GAPConnEventHandler (this handler takes care of the Bluetooth LE connection events)

Expand to see function code
Functions added to the Perihperal_GAPConnEventHandler#
/*********************************************************************
 * @fn      Peripheral_GAPConnEventHandler
 *
 * @brief   The purpose of this function is to handle connection related
 *          events that rise from the GAP and were registered in
 *          @ref BLEAppUtil_registerEventHandler
 *
 * @param   event - message event.
 * @param   pMsgData - pointer to message data.
 *
 * @return  none
 */
void Peripheral_GAPConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
switch(event)
{
    case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
    {
        BLEConnectionEstablished(); //Add this line!
        /* Check if we reach the maximum allowed number of connections */
        if(linkDB_NumActive() < linkDB_NumConns())
        {
            /* Start advertising since there is room for more connections */
            BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
        }
        else
        {
            /* Stop advertising since there is no room for more connections */
            BLEAppUtil_advStop(peripheralAdvHandle_1);
        }
        break;
    }

    case BLEAPPUTIL_LINK_TERMINATED_EVENT:
    {
        BLEConnectionTerminated(); //Add this line!
        BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
        break;
    }

    default:
    {
        break;
    }
}
}

The BLEConnectionEstablished() and BLEConnectionTerminated() functions act as “hook” functions. The establishment of a Bluetooth LE connection is signaled by the reception of a BLEAPPUTIL_LINK_ESTABLISHED_EVENT event. The termination of a Bluetooth LE connection is signaled by the reception of a BLEAPPUTIL_LINK_TERMINATED_EVENT event. BLEConnectionEstablished() and BLEConnectionTerminated() are then executed respectively when a connection is established (BLEAPPUTIL_LINK_ESTABLISHED_EVENT) and terminated (BLEAPPUTIL_LINK_TERMINATED_EVENT).

Another method to interface with the BLE5Stack is via profile callbacks. In this case, we can use the SimpleGatt_changeCB() callback function to detect when a value as a value change handler and is present in the app_simple_gatt.c file. This means that whenever an attribute is changed in the profile, this function is notified. Let’s add some functionality to the SimpleGatt_changeCB() which turns on and off an LED based on the value present in Characteristic 1 of the Simple Profile.

First, we need to make a small change to the mainThread() function found in the empty.c file. We need to comment out the LED toggling within the while loop. We will do this so we can reuse the LED for the value change functionality. Modify the code as follows:

Modification necessary in empty.c#
/*
 *  ======== mainThread ========
 */
void *mainThread(void *arg0)
{
/* 1 second delay */
uint32_t time = 1;

/* Call driver init functions */
GPIO_init();
// I2C_init();
// SPI_init();
// Watchdog_init();

/* Configure the LED pin */
GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

/* Turn on user LED */
GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);

while (1)
{
    sleep(time);
}
}

Now we must create a new function in empty.c which will determine if the LED should be turned off or on based on the new characteristic value and then proceed to do so. The function will be named evaluateNewCharacteristicValue() and should be placed at the end of the empty.c file. The function body may be found below:

Copy this function to the end of the empty.c file#
/*********************************************************************
 * @fn      evaluateNewCharacteristicValue
 *
 * @brief   Based on the new value of a given characteristic determine
 *          if the LED should be turned off or on.
 *
 * @param   newValue: Value of the characteristic to consider
 *
 * @return  None.
 */
void evaluateNewCharacteristicValue(uint8_t newValue)
{
// If the new value of the characteristic is 0, then we turn off the red LED
if(newValue == 0)
{
    GPIO_write(CONFIG_GPIO_LED_0, CONFIG_LED_OFF);
}
else
{
    GPIO_write(CONFIG_GPIO_LED_0, CONFIG_LED_ON);
}
}

We will now navigate towards the app_simple_gatt.c file that was previously mentioned. First, we should add an extern function declaration to allow the app_simple_gatt.c access to the evaluateNewCharacteristicValue() function. The extern declaration is shown below and should be placed near the top of app_simple_gatt.c after the #include statements.

Extern required in app_simple_gatt.c#
extern void evaluateNewCharacteristicValue(uint8_t);

The evaluateNewCharacteristicValue() function should be called inside the SIMPLEGATTPROFILE_CHAR1 case located inside of the SimpleGatt_changeCB() function. The call must be made after the SimpleGattProfile_GetParameter() call and should be passed the newValue variable as a parameter. The function should look as follows:

Expand to see function code
Included evaluateNewCharacteristicValue(newValue) to Characteristic Callback#
static void SimpleGatt_changeCB( uint8_t paramId )
{
  uint8_t newValue = 0;

  switch( paramId )
  {
case SIMPLEGATTPROFILE_CHAR1:
  {
    SimpleGattProfile_getParameter( SIMPLEGATTPROFILE_CHAR1, &newValue );

    // Print the new value of char 1
    MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE, 0, "Profile status: Simple profile - "
                      "Char 1 value = " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
                      newValue);

    evaluateNewCharacteristicValue(newValue); // Add this line!
  }
  break;
default:
  // should not reach here!
  break;
  }
}

The function call is able to take data from the BLE5Stack, in this case the new value of Characteristic 1, and pass it to the empty.c file during runtime. This allows the empty.c to make decisions based on BLE5 activity, even if it does not have direct access to the BLE5Stack.

Hint

At this point you can build and flash the code on the device. For more in depth instruction, make sure to review the Quick Start Guide!

To test your code, a central device must connect to the BLE Basic board. An easy way to do this is by using a Smartphone or Tablet device with a GATT Table viewer application. In this example we will be using the TI SimpleLink Connect application.

With this application, one should be able to scan and connect to the BLE Basic device as well as interact with the characteristics present in the BLE Basic project.

The following steps will showcase how to connect and change the value of Characteristic 1 by using the application.

  1. Scan and locate the Basic BLE project device.

Scanned devices in BLE Scanner
  1. Connect to the Basic BLE project device by tapping on it. The GATT table should now be visible. At this point, the red LED on the LP-EM-CC2340R5 should turn on.

GATT table of BLE Basic project
  1. Expand the “TI Simple Peripheral Service” tab, this tab contains the Simple Profile service and can be identified by the UUID of FFF0 which is visible in the hex string underneath the “TI Simple Peripheral Service” text.

Simple Profile GATT table
  1. Characteristic 1 in the “Simple Profile” service can be identified by its UUID of 0xFFF1 which can be seen in the first characteristic. To write a value to this characteristic, press the “Write” button. In this case, we want to write a hex value, so we can write 00 for 0x00 and 01 for 0x01 as shown in the images below. For this example, lets write 01 for 0x01.

Simple Profile Write ASCII
  1. At this point, the written characteristic can be seen in the 0xFFF1 characteristic and the Red LED should have turned on.

Write 0x01

Take control over Advertising#

One is also able to configure the settings such as the device name, address mode, maximum number of connections, bonding, advertising parameters, connection parameters, advertising data, scanning parameters, among others.

Advertising Parameters#

The following table summarizes the parameters that can be configured for advertising.

Advertising Parameter

Description

Advertising Interval

Time between the start of two consecutive advertising events

Advertising Types

Different PDUs are sent for different types of advertising

Advertising Channels

Legacy advertising packets are sent on three channels

Advertising Task – Change Advertising Parameters with SysConfig#

Settings related to advertising are found in the Broadcaster Configuration section of the BLE configuration SysConfig tab, under RF STACKS.

In some cases we want to save power. One way to do this is by increasing the advertisement interval (advertise less frequently), and just advertise on one channel. In this task, we will configure the device to advertise on one channel every 500 ms using the basic_ble project. Per default, the basic_ble project advertises with two different advertisement sets. The default values of the advertising set 1 are shown below:

Adv Example
  • You can read more about these values in gap_advertiser.h

In order to change the advertising interval, simply change the value for Primary PHY Interval Minimum and Primary PHY Interval Maximum. In this case we will set them to 500 (ms).

If you press the Show Generated Files button in the upper right corner of SysConfig and open ti_ble_config.c, you will see that the primIntMin, primIntMax and primChanMap values of the GapAdv_params_t advParams1 struct have changed:

Note

In the Bluetooth Specifications, advertisement intervals are given in units of 0.625 ms. Thus, 500 ms is given as 800 * 0.625 ms.

ti_ble_config.c :: advParams1 – Generated code for Advertisement Set 1 configuration.#
  // Advertisement Params 1
  GapAdv_params_t advParams1 = {
.eventProps =   GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_LEGACY | GAP_ADV_PROP_SCANNABLE,
.primIntMin =   800,
.primIntMax =   800,
.primChanMap =  GAP_ADV_CHAN_37,
.peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID,
.peerAddr =     { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa },
.filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ,
.txPower =      GAP_ADV_TX_POWER_NO_PREFERENCE,
.primPhy =      GAP_ADV_PRIM_PHY_1_MBPS,
.secPhy =       GAP_ADV_SEC_PHY_1_MBPS,
.sid =          0
  };
  

Take control over the GATT Table#

The GATT Table (GATT is an acronym for the Generic ATTribute Profile) defines the way that two Bluetooth LE devices transfer data back and forth using concepts called Services and Characteristics. It makes use of a generic data protocol called the Attribute Protocol (ATT), which is used to store Services, Characteristics and related data in a simple lookup table

The attributes stored in the GATT table can be written or read and are one of the primary ways that Bluetooth LE devices communicate with one another. To learn more about the GATT Table, please reference the GATT chapter of the User Guide.

In this section, we will discuss a few ways one can interact with the GATT table and how custom functionality can be added that interacts with the GATT Table or is controlled by the GATT table.

GATT Task – Increment and Decrement Attribute in the GATT Table#

In this task we will use the Launchpad GPIOs to increment or decrement a value on the GATT Table which can be read using a GATT Table viewer application.

  1. The first step is to add the GPIOs in the basic_ble.syscfg. Set to any availabe Header Pin on Launchpad.

Create 2 GPIO input instances
  1. In the empty.c file include the following code into the mainThread which has the GPIO configurations and callbacks

**empty.c : GPIO Configurations#
/*
  *  ======== mainThread ========
  */
  void *mainThread(void *arg0)
  {
  /* 1 second delay */
  uint32_t time = 1;

  /* Call driver init functions */
  GPIO_init();
  // I2C_init();
  // SPI_init();
  // Watchdog_init();

  /* Configure the LED pin */
  GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

  GPIO_setConfig(CONFIG_GPIO_Increment, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING); //Add this Line!
  GPIO_setConfig(CONFIG_GPIO_Decrement, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING); //Add this Line!

  /* Turn on user LED */
  GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);
  
  /* Install Button callback */
  GPIO_setCallback(CONFIG_GPIO_ButtonIncrement, IncrementGatt); //Add this Line!
  GPIO_setCallback(CONFIG_GPIO_ButtonDecrement, DecrementGatt); //Add this Line!
  
  /* Enable interrupts */
  GPIO_enableInt(CONFIG_GPIO_Increment); //Add this Line!
  GPIO_enableInt(CONFIG_GPIO_Decrement); //Add this Line!
  
  while (1)
  {
      sleep(time);
      GPIO_toggle(CONFIG_GPIO_LED_0);
  }
  }
  
  1. Next we must also add the IncrementGatt and DecrementGatt extern functions in empty.c

Extern GPIOCallback functions: Add them before mainThread()#
  extern void IncrementGatt();
  extern void DecrementGatt();

  
  1. We will need to define these GPIO callbacks in the app_simple_gatt.c file located inside the app folder. Include the function definition at the end of the file.

GPIO Callbacks: place in app_simple_gatt.c#
  void IncrementGatt()
  {
  Count++;
  SimpleGattProfile_setParameter(SIMPLEGATTPROFILE_CHAR1, sizeof(uint8_t), &Count);
  }
  void DecrementGatt()
  {
  if(Count > 0){
      Count--;
  }
  SimpleGattProfile_setParameter(SIMPLEGATTPROFILE_CHAR1, sizeof(uint8_t), &Count);
  }
  

Using the function SimpleGattProfile_setParameter we are able to update the value and either increment or decrement depending on which GPIO is toggled. Remember to make the variable Count global by defining it at the begining of this file outside any function.

Hint

At this point you can build and flash the code on the device. For more in depth instruction, make sure to review the Quick Start Guide!

Verifying using GATT Table Viewer Application (TI SimpleLink connect)#

  1. Find the device and connect to it on BLE Scanner as done before.

  2. Once Connected open the custom characteristic section. We will be focusing on the first custom characteristic. Press the Read button in order to read the value of the characteristic. It will look like below.

Default Hex Value
  1. Next Increment the characteristic by toggling the Increment GPIO. On the phone app Press the Read again to read the new updated Hex Value.

Updated Hex Value

Hint

Congratulations! You have completed this lab 🏆 Keep reading for a few Bonus tasks…

[BONUS] Implement a Bluetooth® LE Beacon#

  1. Change the configuration of the BLEStack to Broadcaster using SysConfig

Set the stack as Broadcaster
  1. In General Configuration, set-up the name of the beacon

Configure your beacon
  1. In Broadcaster, set-up the Advertisement Parameters, Advertisement Data and Scan Response Data.

    Here are the settings you can use:

    • Configure your beacon
    • Configure your beacon
    • Configure your beacon
  2. Implement the usage of the scan-response in the embedded code.

    • In the basic_ble project, open the file app → app_broadcaster

    • Find the struct broadcasterInitAdvSet1

    • Update the parameters scanRespDataLen and scanResData1

broadcasterInitAdvSet1 is used to initialize the advertising set#
    const BLEAppUtil_AdvInit_t broadcasterInitAdvSet1 =
    {
        /* Advertise data and length */
        .advDataLen        = sizeof(advData1),
        .advData           = advData1,

        /* Scan respond data and length */
        .scanRespDataLen   = sizeof(scanResData1),
        .scanRespData      = scanResData1,

        .advParam        = &advParams1
    };
  

Hint

At this point you can build and flash the code on the device. For more in depth instruction, make sure to review the Quick Start Guide!

[BONUS] Migrating from projects from Simple Framework to Basic BLE#

Examples based on the Simple Framework (simple_peripheral, simple_central, multi_role) can be migrated to the basic BLE examples. This section will detail how to migrate from simple_peripheral to basic_ble.

  1. Transfer BLE profiles from the simple_peripheral project to the basic_ble project.

    • In the simple_peripheral project, the profiles may be found at the following directory: {PROJECT_LOC}/Profiles

    • In the basic_ble project, the profiles may be found at the following directory: {PROJECT_LOC}/common/Profiles

    • Make sure that any #include statements that reference the simple_peripheral directory structure are updated to use the basic_ble directory structure if needed.

  2. Transfer SysConfig settings

    • Select the desired BLE role. In the case of simple_peripheral, select “Peripheral”

    • Select desired BLE parameters.

    • Add any necessary SysConfig modules (UART, SPI, I2C, etc.)

    • Remove any unneeded SysConfig modules.

  3. Remove any unnecessary application files within the “app” folder

    • For example, if your application will only implement the observer role, then the app_broadcaster.c, app_central, app_data, app_pairing, and app_peripheral may be removed. These additional files implement functionality that may not be useful in an observer-only application.

    • In the case of the simple_peripheral example, only the app_broadcaster.c, app_central, and app_observer should be removed to if only the ``simple_peripheral functionality is desired.

  4. Transfer custom application code to the basic BLE project.

    • Almost all of the application code present in the simple_peripheral project was located in the simple_peripheral.c file. In the basic_ble project, a lot of potentially unnecessary code is removed entirely and the remaining code is placed in modular files that can be expanded or minimized as needed.

    • The functionality of the custom code as well as the location of the custom code in the simple_peripheral project will determine the best location in the basic_ble project to transfer the code to.

  • For example, any custom code added to the pairing process should likely be added to app_pairing.c file

  • Any custom code that deals with peripheral specific functionality such as advertising or connecting should likely be added to the app_peripheral.c file.

  • Any code that is not directly related to the BLE5Stack operation can be placed in its own file within the app or common folders.

    • Highly customized code may require a bit more effort to migrate, but should be relatively straight forward to do so.

  1. Additional details to consider

    • The basic_ble project may be configured to act a peripheral, central, broadcaster, observer, or multirole device. This means that the basic_ble project can implement any and all functionality that the simple_peripheral, simple_central, and multi_role projects can implement.

    • As mentioned previously, any files that are not used for a given application may be safely removed from the project.

    • Custom profile files should require little to no migration effort.

    • Most of the migration effort will likely consist of migrating custom code.

previous

SimpleLink™ data_stream examples

next

Bluetooth Low Energy Scanning and Advertising

On this page
  • Introduction
  • Prerequisites
    • Hardware
    • Software
  • Agenda
  • Environment setup
  • “Merge” drivers examples into basic_ble
  • Interface with the BLE5Stack
  • Take control over Advertising
    • Advertising Parameters
      • Advertising Task – Change Advertising Parameters with SysConfig
  • Take control over the GATT Table
    • GATT Task – Increment and Decrement Attribute in the GATT Table
    • Verifying using GATT Table Viewer Application (TI SimpleLink connect)
  • [BONUS] Implement a Bluetooth® LE Beacon
  • [BONUS] Migrating from projects from Simple Framework to Basic BLE

© Copyright 2024, Texas Instruments.