SimpleLink Audio Plugin Quick Start Guide
Table of Contents
Introduction
This guide is intended to assist users in the initial setup and demonstration of an audio application using the SimpleLink Audio Plugin. The guide explains how to configure the boards, compile the software artifacts, program the devices, and run an audio loop back example.
Hardware Requirements
One of the LaunchPads from the Development Board Support section of the release notes and one of the BoosterPacks or breakout boards.
Note If using a CC13x2 LaunchPad, jumper wires will also be required.
Software Requirements
Setting up the software should follow the steps below:
- Select a LaunchPad from the section above
- Install the device SDK associated with that LaunchPad
- Choose a toolchain (e.g. IAR, CCS) and install it
- Install UNIFLASH if a standalone flash programmer is needed
A device SDK is required to build and run the examples contained in the plugin. At least of one of the SDKs listed in the Dependencies section of the release notes should be installed. The SDK type should match the LaunchPad hardware. For example, to run on a CC3220SF, then the cc32xx SDK should be installed. If instead a cc26x2 or cc13x2 device is to be used then select cc13x2_26x2 SDK.
Installing SimpleLink Audio Plugin
- Download and open the installer (replace M.mm.pp.bb with version number):
- Windows:
simplelink_audio_plugin_M_mm_pp_bb.exe - Linux:
simplelink_audio_plugin_M_mm_pp_bb.run - macOS:
simplelink_audio_plugin_M_mm_pp_bb.app
- Windows:
Select an installation directory. This will be referred to as
<AUDIO_INSTALL_DIR>in the rest of this document. It’s recommended that you install it in your CCS installation directory (defaultC:\tion Windows) so it can be discovered automaticallyClick Next > and finish the installation
Hardware Setup
Codec Setup - CC3200AUDBOOST
This section will detail the steps required to get an audio loop-back example running with the CC3200AUDBOOST. This configuration uses the AudioHAL implementation that is made for I2S based CODEC devices called AudioHALCodec.
Due to pin conflicts with the CC13x2, the hardware setup is slightly different based on LaunchPad selected. Expand the containers below to see the steps for each device.
Note that if I2S slave mode is required, please expand the container and follow the steps there. Note that the hardware modifications for slave mode are needed by all supported devices.
Note it is recommended to first verify the setup using master mode and only switch to slave mode if needed.
CC26xx devices (all variants) may be connected by seating the No further hardware modification is needed if master mode is to be used (default). Slave mode is discussed in the coming sectionCC26xx
CC3200AUDBOOST on the BoosterPack headers of the LaunchPad directly.
The CC32XX device implements a sense-on-power scheme to determine the device operation mode upon power up. The encoding of these pins determines the boot flow and the default mapping for some of the pins (UART, JTAG, etc.) The SOP pins are connected to jumper J13 on the CC32XX LaunchPad, which is shipped in flash and functional mode (010) as shown in the image below. SOP[2…0] mode (100) is used for programming the serial flash with the application binary and/or the service pack. After flashing, the board should be reset and the mode set to (000) (no jumpers in place) to run/execute the contents of flash SOP[2…0] mode (010) is the flash and execute mode which is similar to the (100) mode except that after flashing, the contents of flash are executed immediately without having to reset or remove all jumpers. This mode is also used when using CCS (or IAR) to connect to the device for loading and debugging. CC32xx devices (all variants) may be connected by seating the No further hardware modification is needed if master mode is to be used (default). Slave mode is discussed in the coming section.CC32xx
CC3200AUDBOOST on the BoosterPack headers of the LaunchPad directly.
The following pins are used for the CC13x2. Remember that MCLK is only used in I2S slave mode, else it is assumed that MCLK is tied to BCLK. See the Users Guide for more information. * Note MCLK is only used in I2S slave mode. Note that WCLK is different for P vs R versions of the CC13x2 LaunchPad: When running jumper wires, it is also necessary to provide the AUDBOOST with 5V, 3V3, and GND connections. Additionally it is necessary to connect the I2C lines (SDA, SCL) to J1.19 and J1.17 respectively. Check the The steps to make this modification are below For CC13x2R devices the bottom two pins on J3 should be bent (see picture below). These pins are bent to prevent collision with the RF ports. Note that strictly speaking CC1312R does not require bending the bottom pin, but then IOID_1 must not be used or driven. For CC13x2P devices the bottom 5 pins on J3 should be bent (see picture below). Once the pin has been bent, you can seat the The picture below shows the setting for CC13x2R devices. The picture below shows the setting for CC13x2P devices: Note: The jumper wires should be kept as short and tied as possible (if not they could act as antennas and add noise to the audio pins)CC13x2
CC13x2 LaunchPad Pin
CC3200AUDBOOST Pin
IOID_25 (ADO)
J1.18 (DIN)
IOID_26 (ADI)
J1.20 (DOUT)
IOID_27 (BCLK)
J1.16 (BCLK)
IOID_23 (MCLK)*
TP13 (MCLK)
LaunchPad
Pin
CC3200AUDBOOST Pin
CC13x2R
IOID_28 (WCLK)
J1.14 (WCLK)
CC13x2P
IOID_16 (WCLK)
J1.14 (WCLK)
*_LAUNCHXL.h board file to find the pins of SDA and SCL. An easy way to do this is to bend the pins of LaunchPad that have a collision with the CC3200AUDBOOST. Then the CC3200AUDBOOST can safely be seated on top of the LP.
CC3200AUDBOOST on LaunchPad’s BoosterPack headersCC3200AUDBOOST and set up the jumper wires.
Wire color
Signal
yellow
ADO
green
ADI
blue
BCLK
purple
WCLK
white
MCLK
Wire color
Signal
yellow
ADO
green
ADI
blue
BCLK
purple
WCLK
white
MCLK
By default, the applications in this SDK will use I2S master mode. However, slave mode is supported by both the In slave mode, the CCxxxx device must generate a reference clock for the codec on the The The AudioHAL framework relies on BCLK and MCLK being independent signals, the CC3200AUDBOOST has tied these signals together via a 0 Ohm resistor. This resistor must be removed if I2S slave mode is required. See pictures below on how to find this resistor.(Optional) I2S Slave Mode
AudioHAL and the I2S driver.CC3200AUDBOOST to use as an input to its PLL (MCLK). The AudioHAL may be configured to support MCLK generation in slave mode. See the AudioHAL Doxygen listed above for information on how to configure this.CC3200AUDBOOST ties BCLK and MCLK pins together via a 0-Ohm resistor. Since in slave mode we require separate BCLK and MCLK, this resistor must be removed. Instructions on how to remove this resistor can be found below.
Building and running Examples in CCS
Several examples are provided in the Plugin and can be found in the examples/ subdirectory.
These steps refer to the audiohal_echo application for the CC2642R1 device, but the same procedure applies to any supported device and to other examples as well.
It is assumed that the SimpleLink cc13x2_26x2 SDK has already been installed in a directory we will refer to as
<SIMPLELINK_CC13X2_26X2_SDK_INSTALL_DIR>. You should install it if you have not already done so. See the Dependencies section of the release notes for more informationOpen Code Composer Studio (close and re-open if already running before Plugin or SDK installation).
In CCS, import the
audiohal_echoexample by first selecting Project > Import CCS Projects…In the Import CCS Projects window, hit the browse button to browse to the location corresponding to
<AUDIO_INSTALL_DIR>\examples. Select the checkbox next to theaudiohal_echoexample for tirtos for CCS and hit the Finish button.Two projects should appear in the Project Explorer tab in CCS: one for the
audiohal_echoexample itself (i.e.audiohal_echo_CC26X2R1_LAUNCHXL_tirtos_ccs), and the other is a project corresponding to the OS chosen (e.g.tirtos_builds_CC26X2R1_LAUNCHXL_release_ccs).The example comes with a README.html file that contains more details specific to the example. Be sure to take a look as it may contain additional instructions.
Right-click on the
audiohal_echoproject, and select Build Project to build.
Load and run the Example
Plug the LaunchPad into a USB port on your PC.
Plug 3.5 mm audio jack into LINE IN connector on
CC3200AUDBOOST.Plug headphones to the LINE OUT connector on
CC3200AUDBOOST. Setup should look as below:
Right-click on the
audiohal_echoproject, and select Debug As > Code Composer Debug Session. If using CC32xx note the SOP[2..0] jumper setting on the board must be (010) in order for the CCS debugger to connect.Run the application by pressing F8. Audio will begin playing on the headphones, it is being looped back through the LaunchPad.
Building and running Examples in IAR
Download and Installation
For instructions on downloading and setting up IAR properly for use with the SimpleLink SDK and its plugins, please refer to the Quick Start Guide from the selected dependent device SDK. As part of the procedure, make sure to configure the environmental variables for the SDK.
Configuring the environmental variables
Before starting to work with any of the SimpleLink Audio Plugin example projects, you need to load a set of environment variables that will be set for your current workspace, in addition to the ones from the SimpleLink SDK.
The custom argvars can be found at
If you need to modify the default path argument variables, edit the variables with the correct path.
Open the IAR IDE
Choose Tools > Configure Custom Argument Variables
Click Global > Import
Browse to
/tools/iar. Import the custom argvars.
Importing your First Project
These steps refer to the audiohal_echo application for the CC2642R1 device, but the same procedure applies to any supported device and to other examples as well.
You can choose to open an Example Project by either directly accessing the Example workspace (by double clicking on its *.eww file), or by importing the Example from the Example List in the IDE.
Directly accessing an Example from the Example Folder
All Code Examples that are shipped with the plugin come with an IAR workspace (*.eww file). Double-Clicking the specific workspace allows you to open the project on disk and build it.
Each example comes with a README.html file. Be sure to take a look in case it has additional instruction specific to the example you wish to run. Update the example to use your Azure connection string and WiFi Access Point information, as specified in the section Example Pre-Build Steps.
Importing an Example in the Example List
In the IAR-IDE, select File > Open File… from the menu and open
<AUDIO_INSTALL_DIR>/tools/iar/Examples.htmlAll SimpleLink Audio Plugin example projects that are available in IAR are listed in the html page.
Scroll through the page and click on the project you are interested in. In this guide we choose to work with
audiohal_echofor the CC2642R1 based on TI-RTOS.
When prompted, click
Yesto save a copy of the project workspace in a specific folder,Nowill save the workspace in a default folder.After clicking
Yes, browse to the location where you want to save this workspace. ClickChoose
Building the project
Two projects should appear in the Workspace tab in IAR: one for the
1audiohal_echoexample itself (i.e.audiohal_echo_CC26X2R1_LAUNCHXL_tirtos_iar), and the other is a project corresponding to the OS chosen (e.g.tirtos_builds_CC26X2R1_LAUNCHXL_release).The example comes with a README.html file that contains more details specific to the example. Be sure to take a look as it may contain additional instructions.
Make/Build the Example Project by first selecting the OS project tab on the Workspace window and select Project > Make. Once done, select the
audiohal_echotab on the Workspace window and select Project > Make.
Start a debug session
To start an IAR debug session follow the steps outlined in the Run a debug session section in the QuickStart for IAR IDE chapter of the corresponding SDK’s Quick Start Guide document.
Load and run the Example
Plug the LaunchPad into a USB port on your PC.
Plug 3.5 mm audio jack into LINE IN connector on
CC3200AUDBOOST.Plug headphones to the LINE OUT connector on
CC3200AUDBOOST. Setup should look as below:
Select Project > Download and Debug If using CC32xx note the SOP[2..0] jumper setting on the board must be (010) in order for the CCS debugger to connect.
Run the application by pressing F5. Audio will begin playing on the headphones, it is being looped back through the LaunchPad.
Building with Makefiles
These steps refer to audiohal_echo application, but the same procedure applies to other examples as well.
It is assumed that the SimpleLink CC13x2_26x2 SDK has already been installed in a directory we will refer to as
. You should install it if you have not already done so, as the SimpleLink Audio Plugin depends on it. Update the imports.mak file in the
root folder with the appropriate path(s). You may check the imports.mak inside the dependent device SDK for help. Only relevant paths are required. For example, if IAR is not to be used, this path can be left untouched.
Navigate to the directory corresponding to your OS, board and toolchain of choice. For example, <SIMPLELINK_CC13X2_26X2_SDK_INSTALL_DIR>/kernel/tirtos/builds/CC26X2R1_LAUNCHXL/release/ccs \ for tirtos and TI (CCS) toolchain on the CC26x2 LaunchPad.
Run ‘make’ to build the OS. If you develop on a Windows machine and do not have the ‘make’ utility, you can alternatively run ‘gmake’ from your TI XDCTOOLS installation (e.g. ‘C:\ti\xdctools_x_xx_xx_xx_core\gmake.exe’). XDCTOOLS is a dependency of the device SDKs and the SimpleLink Audio Plugin. See the release notes for the required version.
Navigate to the example folder specific to your board(replace CC26X2R1_LAUNCHXL with your board name):
Read the README.html file of the example, and follow any additional instructions specific to the example if present.
Navigate to the example folder specific to your OS, board and toolchain
To build, run ‘make’ to generate audiohal_echo.out
You can load and debug the generated audiohal_echo.out in CCS (or IAR)