|
TI BLE Stack API Documentation
2.03.06
|
Util layer interface. More...
#include <ti/sysbios/knl/Clock.h>#include <ti/sysbios/knl/Queue.h>#include <ti/sysbios/knl/Semaphore.h>Go to the source code of this file.
Classes | |
| struct | appEvtHdr_t |
| ICALL_EVENTS. More... | |
Functions | |
| Clock_Handle | Util_constructClock (Clock_Struct *pClock, Clock_FuncPtr clockCB, uint32_t clockDuration, uint32_t clockPeriod, uint8_t startFlag, UArg arg) |
| Initialize a TIRTOS Clock instance. More... | |
| void | Util_startClock (Clock_Struct *pClock) |
| Start a clock. More... | |
| void | Util_restartClock (Clock_Struct *pClock, uint32_t clockTimeout) |
| Restart a clock by changing the timeout. More... | |
| bool | Util_isActive (Clock_Struct *pClock) |
| Determine if a clock is currently active. More... | |
| void | Util_stopClock (Clock_Struct *pClock) |
| Stop a clock. More... | |
| void | Util_rescheduleClock (Clock_Struct *pClock, uint32_t clockPeriod) |
| Reschedule a clock by changing the timeout and period values. More... | |
| Queue_Handle | Util_constructQueue (Queue_Struct *pQueue) |
| Initialize an RTOS queue to hold messages from profile to be processed. More... | |
| uint8_t | Util_enqueueMsg (Queue_Handle msgQueue, Semaphore_Handle sem, uint8_t *pMsg) |
| Creates a queue node and puts the node in RTOS queue. More... | |
| uint8_t * | Util_dequeueMsg (Queue_Handle msgQueue) |
| Dequeue the message from the RTOS queue. More... | |
| char * | Util_convertBdAddr2Str (uint8_t *pAddr) |
| Convert Bluetooth address to string. Only needed when LCD display is used. More... | |
Util layer interface.
1.8.12