EasyLink Layer¶
Overview¶
The EasyLink API is a simple abstraction layer on top of the RF Driver and is intended as a starting point for customers creating a proprietary Sub-1 GHz protocol. The EasyLink layer does not support any regional RF conformance such as Listen Before Talk required for the license free frequency band. Customers need to add support for the regional conformance that their product requires under the EasyLink API.
The EasyLink Example can be found in the examples/{rtos or nortos}/{development
board}/easylink folder. You can find descriptions of the examples in the
Examples User’s Guide.
Note
Note that this is an example code, intended to be used as a starting point to develop custom application for specific use-cases and protocols. Security features are not a part of these examples and have to be designed by the customer if needed.
The EasyLink layer also supports a simple network processor configuration. This is showcased in the EasyLink Network Processor (NP) example project. Here, the EasyLink API has been exposed over an AT Command Interface such that it can be used by Host SW (running on a PC, MPU or MCU), or by using a serial terminal emulator over a UART. The specific commands can be found in the rfEasyLinkNp.
The EasyLink API should be used in application code. The EasyLink API is intended to abstract the RF Driver in order to give a simple API as a starting point for customers to develop their application use cases.
For API descriptions, see the EasyLink API reference.
General Behavior¶
Before using the EasyLink API the EasyLink Layer is initialized by calling
EasyLink_init(). This initializes and opens the RF driver and
configures the modulation scheme passed to EasyLink_init.
RX is enabled by calling
EasyLink_receive() or EasyLink_receiveAsync(). Entering RX can
be immediate or scheduled by using the EasyLink_RxPacket::absTime field.
EasyLink_receive() is blocking and EasyLink_receiveAsync() is
nonblocking. The EasyLink API does not queue messages so calling another API
function while in EasyLink_receiveAsync() will return
EasyLink_Status_Busy_Error. An Asynchronous Rx operation can be canceled with
EasyLink_abort().
TX is enabled by calling EasyLink_transmit() or EasyLink_transmitAsync().
TX can be immediate or scheduled by using the EasyLink_TxPacket::absTime field.
EasyLink_transmit() is blocking and EasyLink_transmitAsync()
is nonblocking. The EasyLink API does not queue messages so calling another API
function while in EasyLink_transmitAsync() will return EasyLink_Status_Busy_Error
An Asynchronous operation can be canceled with EasyLink_abort().
Error Handling¶
The EasyLink API will return EasyLink_Status containing success or error code.
The EasyLink_Status code are:
EasyLink_Status_Success |
EasyLink_Status_Config_Error |
EasyLink_Status_Param_Error |
EasyLink_Status_Mem_Error |
EasyLink_Status_Cmd_Error |
EasyLink_Status_Tx_Error |
EasyLink_Status_Rx_Error |
EasyLink_Status_Rx_Timeout |
EasyLink_Status_Busy_Error |
EasyLink_Status_Aborted |
Supported Functions¶
| Generic API function | Description |
|---|---|
EasyLink_init() |
Inits and opens the RF driver and configures the specified modulation |
EasyLink_transmit() |
Blocking Transmit |
EasyLink_transmitAsync() |
Nonblocking Transmit |
EasyLink_receive() |
Blocking Receive |
EasyLink_receiveAsync() |
Nonblocking Receive |
EasyLink_abort() |
Aborts a non blocking call |
EasyLink_EnableRxAddrFilter() |
Enables/Disables RX filtering on the Addr |
EasyLink_GetIeeeAddr() |
Gets the IEEE Address |
EasyLink_SetFreq() |
Sets the frequency |
EasyLink_GetFreq() |
Gets the frequency |
EasyLink_SetRfPwr() |
Sets the Tx Power |
EasyLink_GetRfPwr() |
Gets the Tx Power |
EZLINKPROP-890 Workaround¶
Currently there is a known issue (EZLINKPROP-890) that causes all existing PHYs to be affected when exporting custom settings using SmartRF Studio. The custom settings are only meant to affect the “Custom” EasyLink PHY however, each pre-defined PHY currently shares TX and advanced RX commands with the custom settings. A three step workaround to this issue follows below.
1) Exporting Commands from SmartRF Studio¶
EasyLink requires an advanced RX command to support address filtering and clear channel assessment. This command is not exported by default for EasyLink supported PHYs via SmartRF Studio. To export the command:
- After selecting and modifying a desired PHY in SmartRF Studio, click “Code Export”.
- Select the “Command” view from the upper left corner of the pane that pops-up.
- Check the “Select commands individually” checkbox.
- Select
CMD_PROP_RX_ADVand click the “>” arrow to add it to the list of exported commands. - Save the generated files.
2) Update Project to use Exported Settings¶
In your project there will be two sets of SmartRF Settings;
smartrf_settings_predefined.c/h and smartrf_settings.c/h. The
pre-defined settings are used for all PHYs except the “Custom” EasyLink PHY
whereas the non-prefined settings are used for the “Custom” PHY. The following
modifications are needed to these files:
- Open the contents of the original
smartrf_settings.cand copy the entirety of therfc_CMD_PROP_TX_tcommand. - Open the
smartrf_settings_predefined.cfile and paste the copiedrfc_CMD_PROP_TX_tcommand at the bottom of the file. - Rename the pasted
rfc_CMD_PROP_TX_tcommand tofrom RF_cmdPropTxtoRF_cmdPropTx_preDef. - Open smartrf_settings_predefined.h and add
extern rfc_CMD_PROP_TX_t RF_cmdPropTx_preDef;to the list of extern variables. - Overwrite the contents of the original smartrf_settings.c/h files with the recently exported SmartRF Studio files.
3) Update EasyLink¶
EasyLink uses an array of “EasyLink_RfSetting” to access the individual RF commands for each PHY. This needs to be updated to use the recent changes made to the smartrf_settings files. In addition, the EasyLink source code needs to be modified for the recently exported advanced rx command to use the correct sync word:
- Open
easylink_config.cand locate theEasyLink_supportedPhysarray. Each individual PHY is surrounded by a guard macro indicating the PHY type. - Locate the Custom PHY and modify the
RF_pCmdPropRxAdvelement to:.RF_pCmdPropRxAdv = &RF_cmdPropRxAdv,. - Update all other
RF_pCmdPropTxelements toRF_cmdPropTx_preDefexcept the Custom PHY:.RF_pCmdPropTx = &RF_cmdPropTx_preDef,. - Open
EasyLink.corEasyLink_nortos.cdepending on the projects RTOS support. - Find the
EasyLink_init()function implementation and the lines of code modifying elements of theEasyLink_cmdPropRxAdvstructure. - After the last line modifying this structure add the code snippet below. This will force the advanced RX command to use the same sync word as the TX command that was recently exported from SmartRF Studio:
if(EasyLink_Phy_Custom == EasyLink_params.ui32ModType)
{
EasyLink_cmdPropRxAdv.syncWord0 = EasyLink_cmdPropTxAdv.syncWord;
}
Frame Structure¶
The EasyLink implements a basic header for transmitting and receiving data. This header supports addressing for a star or point-to-point network with acknowledgments.
Packet structure:
1B Length 1-64b Dst Address Payload