Image Metadata¶
All TI OAD images use a 16-byte metadata header. This metadata vector is
embedded at the beginning of the image, occupying the first 16 bytes before
the application code. Metadata checking is done in
OADTarget_validateNewImage(). Table 15.
below shows a description of the metadata vector.
Field |
Size (in bytes) |
Description |
|---|---|---|
CRC |
2 |
Cyclic Redundancy Check (CRC) |
CRC Shadow |
2 |
Place holder for CRC |
Version |
2 |
Version |
Length |
2 |
Length of the image in words* |
UID |
4 |
User Identification |
Start Address |
2 |
The destination address of the image in words* |
Image Type |
1 |
The type of image to be downloaded |
State |
1 |
The status of this image |
Note
The above fields that are marked with an asterisk * are
measured in 32-bit words. For example, an image length of 0x100
describes an image that is 1024 bytes in size. The OAD word size is
defined by EFL_OAD_ADDR_RESOLUTION for off-chip OAD and by
HAL_FLASH_WORD_SIZE for on-chip OAD.
CRC and CRC Shadow¶
The cyclic redundancy check (CRC) is a means to check the integrity of an image. This must be done in two steps. First the CRC must be calculated when the image is generated from the toolchain, this will be stored in the CRC field within the metadata vector.
This initial CRC will be sent over the air via the OAD service. Later, the target will need to ensure that the image has not been corrupted during transfer. The target will then re-calculate the CRC of the downloaded image; this will be stored in the CRC shadow field of the metadata vector.
If the CRC and CRC shadow are equivalent, the target can assume that the image was not corrupted while sending over the air.
The algorithm selected for CRC calculations is the CRC-16-CCITT.
Version¶
The image version field is used to track revisions of images and ensure
upgrade compatibility. Customers may implement their own versioning
scheme; however, there are additional checks imposed by the TI OAD profile.
See the function OADTarget_validateNewImage() within
oad_target_external_flash.c or oad_target_internal_flash.c
how these version checks are done in Off-chip and On-chip OAD, respectively.
Length¶
The length field is the length of the image in words, where the word
size is defined by EFL_OAD_ADDR_RESOLUTION and HAL_FLASH_WORD_SIZE
for On-chip and Off-chip OAD respectively. Off-chip OAD customers who
are using different external flash parts may need to modify
EFL_OAD_ADDR_RESOLUTION to match the word size of their part. For
On-chip OAD, the word size of the CC13x0 is fixed.
User Identification (UID)¶
This field is un-used by the TI OAD profile in the BLE stack only, but the hooks are in place for a customer to add their own implementation of verifying images based on a UID.
For on-chip OAD, the convention is that Image A will embed ‘A’, ‘A’, ‘A’, ‘A’ and Image B will embed ‘B’, ‘B’, ‘B’, ‘B’. Off-chip images use ‘E’, ‘E’, ‘E’, ‘E’ by default.
Start Address¶
The start address is the first address where the proposed image is to be stored in internal flash. Similar to the length field, this is calculated in words. Off-chip OAD solutions put restrictions on the start address based on image type (more on this in the next section).
Note
For On-chip OAD solutions, this field is reserved in the metadata as they use a fixed start address that is based on the internal flash memory map.
Image Type¶
In Off-chip OAD systems with external flash, there are multiple types of images that can be uploaded. They are explained in Table 16.. Note, that OAD via EasyLink supports only Application type as there are no stacks involved.
Image Type |
Value |
Description |
|---|---|---|
EFL_OAD_IMG_TYPE_APP |
1 |
An application or application + stack merged update |
EFL_OAD_IMG_TYPE_STACK |
2 |
A stack only update |
EFL_OAD_IMG_TYPE_NP |
3 |
|
EFL_OAD_IMG_TYPE_FACTORY |
4 |
Describes the permanently resident production image that runs on the device before any OTA updates. |
On-chip OAD solutions determine the image type based on the LSB of the image version field. The image type field is not used in this case.
Image State¶
The image state is a one byte metadata field that is used only by Off-chip OAD solutions. The state informs the bootloader whether or not the image is ready to run or currently running. This prevents the bootloader from copying the same image from external to internal flash on every boot.
Note
For On-chip OAD solutions this field is reserved in the metadata as the OAD reset service handles switching between images in the bootloader.