1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Assert.xdc ========
    15     */
    16    
    17    /*!
    18     *  ======== Assert ========
    19     *  Runtime assertion manager
    20     *
    21     *  The `Assert` module provides configurable diagnostics to the program.
    22     *  Similar to the standard C `assert()` macro, `Assert` methods are
    23     *  interspersed with other code to add diagnostics to a program. Unlike
    24     *  the standard C assert support, the `Assert` module provides greater
    25     *  flexibility in managing the messages displayed, the message string
    26     *  space overhead, and the runtime handling of failures. In addition,
    27     *  because the `Assert` methods build atop the Diags module, you can
    28     *  precisely control which asserts remain in the final application, if any.
    29     *
    30     *  The `Assert` module works in conjunction with the `{@link Diags}` module.
    31     *  `Assert` statements are added to the code using the
    32     *  `{@link #isTrue Assert_isTrue()}` function. Execution of assert
    33     *  statements is controlled by the `{@link Diags#ASSERT}` and
    34     *  `{@link Diags#INTERNAL}` bits in a module's diagnostics mask. By default,
    35     *  all module's `Diags_ASSERT` bit is enabled and the `Diags_INTERNAL` bit
    36     *  is disabled.  See `{@link Types#Common$ Types.Common$}` for the
    37     *  declaration of the bits in the diagnostics mask and
    38     *  `{@link Defaults#common$ Default.common$}` for the default module settings.
    39     *
    40     *  Two types of asserts are supported: public asserts and internal asserts.
    41     *
    42     *  @p(blist)
    43     *  - Public asserts have an assert ID and are, by default, controlled
    44     *  by the `{@link Diags#ASSERT}` bit.
    45     *  - Internal asserts don't have an assert ID (other than NULL) and
    46     *  are active only when both the `{@link Diags#ASSERT}` and
    47     *  `{@link Diags#INTERNAL}` bits of the module's diagnostics mask are set.
    48     *  @p
    49     *
    50     *  `Assert` IDs are small integer values that index into a table of
    51     *  assertion descriptors. These descriptors hold an error message
    52     *  and a diagnostics mask that is used to enable and disable the
    53     *  assertion at runtime.
    54     *
    55     *  You can remap individual public asserts to different bits in the
    56     *  diagnostics mask, or can disable the assert altogether. This is
    57     *  done by setting the mask property of the assert ID. Setting the
    58     *  mask to 0 disables the assert. In all other cases, the `Diags.ASSERT`
    59     *  bit is OR'd together with the mask to define the controlling bits.
    60     *  For example, the module's diagnostics mask must have the `Diags.ASSERT`
    61     *  bit set and any other bit specified in the mask property of the
    62     *  assert ID in order to activate the assert.
    63     *
    64     *  @a(Examples)
    65     *  @p(html)
    66     *  <hr />
    67     *  @p
    68     *  Example 1: The following C code adds an assert to application code
    69     *  which is not in a module. This assert does not have an assert
    70     *  identifier (the second argument is NULL); this makes it an internal
    71     *  assert.
    72     *
    73     *  @p(code)
    74     *  // file.c
    75     *  #include <xdc/runtime/Assert.h>
    76     *
    77     *  Assert_isTrue(count > 0, NULL);
    78     *  @p
    79     *
    80     *  The following XDC configuration statements set both the ASSERT and
    81     *  INTERNAL bits in the diagnostics mask to enable the internal assert
    82     *  created in the previous C code. Since the C code is not in a module,
    83     *  you must set the bits in the diagnostics mask of the
    84     *  `{@link xdc.runtime.Main xdc.runtime.Main}` module. The Main module
    85     *  is used to control all `{@link Log}` and `Assert` statements that are
    86     *  not part of the implementation of a module; for example, top-level
    87     *  application code or any existing sources that simply call the `Log` or
    88     *  `Assert` methods.
    89     *
    90     *  @p(code)
    91     *  // program.cfg
    92     *  var Assert = xdc.useModule('xdc.runtime.Assert');
    93     *  var Diags = xdc.useModule('xdc.runtime.Diags');
    94     *  var Main = xdc.useModule('xdc.runtime.Main');
    95     *
    96     *  Main.common$.diags_ASSERT = Diags.ALWAYS_ON;
    97     *  Main.common$.diags_INTERNAL = Diags.ALWAYS_ON;
    98     *  @p
    99     *
   100     *  @p(html)
   101     *  <hr />
   102     *  @p
   103     *  Example 2: The following example shows how to use and configure an
   104     *  assert ID that is declared by a module. It adds that assert to the
   105     *  application's C source code, and configures the application to
   106     *  execute the assert.
   107     *
   108     *  This is part of the XDC file for the module that declares an `Assert` Id:
   109     *
   110     *  @p(code)
   111     *  // Mod.xdc
   112     *  import xdc.runtime.Assert;
   113     *  import xdc.runtime.Diags;
   114     *
   115     *  config Assert.Id A_nonZero = {
   116     *      msg: "A_nonZero: value must be non-zero"
   117     *  };
   118     *  @p
   119     *
   120     *  This is part of the C code for the application:
   121     *
   122     *  @p(code)
   123     *  // Mod.c
   124     *  #include <xdc/runtime/Assert.h>
   125     *
   126     *  Assert_isTrue(x != 0, Mod_A_nonZero);
   127     *  @p
   128     *
   129     *  This is part of the XDC configuration file for the application:
   130     *
   131     *  @p(code)
   132     *  // program.cfg
   133     *  var Diags = xdc.useModule('xdc.runtime.Diags');
   134     *  var Mod = xdc.useModule('my.pkg.Mod');
   135     *  Mod.common$.diags_ASSERT = Diags.ALWAYS_ON;
   136     *  @p
   137     *
   138     *  The Assert calls can also be completely removed by defining the symbol
   139     *  xdc_runtime_Assert_DISABLE_ALL. This can be done on the compile line, e.g.
   140     *  -Dxdc_runtime_Assert_DISABLE_ALL. This will completely remove the Assert
   141     *  statements from any code compiled with this flag, regardless of the
   142     *  application's configuration or your compiler's optimization settings.
   143     *
   144     *  It is also possible to remove all conditions from Assert calls. As explained
   145     *  above, Assert calls are executed only if certain bits in the module's
   146     *  Diags mask are set. However, if the symbol
   147     *  xdc_runtime_Assert_DISABLE_CONDITIONAL_ASSERT is defined, the module's Diags 
   148     *  mask is not queried at all, and all Assert calls are unconditionally
   149     *  executed.
   150     *  The symbol xdc_runtime_Assert_DISABLE_ALL has a precedence, and if it's
   151     *  set, no Assert calls are executed regardless of any definition of
   152     *  xdc_runtime_Assert_DISABLE_CONDITIONAL_ASSERT.
   153     */
   154    @DirectCall
   155    @CustomHeader
   156    
   157    module Assert {
   158    
   159        /*!
   160         *  ======== Assert_Desc ========
   161         *  Assert descriptor
   162         *
   163         *  Each public assert is defined with an assert descriptor. This
   164         *  structure defines which bits in the module's diagnostics mask
   165         *  control this assert, and the message raised when the assert fails.
   166         *  The mask property is optional, it defaults to the
   167         *  `{@link Diags#ASSERT}` bit.
   168         *
   169         *  @field(mask)    Specifies which bits enable the assert.
   170         *  @field(msg)     The message printed when the assert fails.
   171         */
   172        metaonly struct Desc {
   173            Diags.Mask mask;
   174            String msg;
   175        };
   176    
   177        /*!
   178         *  ======== Assert_Id ========
   179         *  Assert identifier
   180         *
   181         *  Each metaonly assert descriptor is encoded into a target accessable
   182         *  assert Id type which can be passed to the `{@link #isTrue}` function.
   183         */
   184        @Encoded typedef Desc Id;
   185    
   186        /*!
   187         *  ======== E_assertFailed ========
   188         *  The `{@link Error#Id}` raised when an assertion violation is detected
   189         *
   190         *  When an assertion violation is triggered, an error is raised via
   191         *  `Error_raise()`.  `E_assert_Failed` is the `{@link Error#Id}` passed
   192         *  to `Error_raise()`.
   193         *  
   194         *  The first string argument (%s) will be either "", if the assertion Id
   195         *  is `NULL` (for internal asserts), or ": " (for public asserts).
   196         *  The second string argument (%s) is the
   197         *  `Assert.Desc.msg` string associated with the assertion Id; if the
   198         *  Id is `NULL`  (an internal assert) or if text is not loaded 
   199         *  (`!{@link Text#isLoaded}()`), this string is "".
   200         *
   201         *  @see #isTrue
   202         *  @see Error#Id
   203         */
   204        readonly config Error.Id E_assertFailed = {msg: "assertion failure%s%s"};
   205    
   206        /*!
   207         *  ======== Assert_isTrue ========
   208         *  Test an assertion
   209         *
   210         *  `Assert_isTrue()` statements may be conditionally enabled (disabled)
   211         *  on a per module basis by setting the calling module's
   212         *  `{@link IModule#$common $common.diags_ASSERT}` configuration
   213         *  parameter.  If
   214         *  the `Assert_isTrue()` statement is not in a module, the calling
   215         *  module is the `{@link Main}` module.  You must enable the
   216         *  `{@link Diags#ASSERT}` bit in the module's diagnostics mask for this
   217         *  call to be enabled.  If a `NULL` assert id is specified, then you
   218         *  must enable the `{@link Diags#INTERNAL}` in addition to the
   219         *  `ASSERT` bit.  
   220         *
   221         *  If the `Assert_isTrue()` statement is enabled and `expr` evaluates to
   222         *  false, the assert specified by `id` is raised; i.e., the
   223         *  `{@link #E_assertFailed}` error is raised with a `NULL`
   224         *  error block.  In other words, the standard `{@link Error#raise}`
   225         *  handling hooks will be run, `{@link System#abort()}` will be called,
   226         *  and control does not return to the caller.  The `id` may be `null`, in
   227         *  which case you will get a generic assert message.
   228         *
   229         *  @param(expr)    the expression which should evaluate to true
   230         *  @param(id)      identifies the assert being raised
   231         *
   232         *  @a(Examples)
   233         *  C Code
   234         *  @p(code)
   235         *  #include <xdc/runtime/Assert.h>
   236         *
   237         *  Assert_isTrue(count > 0, NULL);
   238         *  @p
   239         */
   240        @Macro Void isTrue(Bool expr, Id id);
   241    
   242    internal:
   243    
   244        Void raise(Types.ModuleId mod, CString file, Int line, Id id);
   245    
   246    }
   247    /*
   248     *  @(#) xdc.runtime; 2, 1, 0,0; 11-8-2017 17:11:25; /db/ztree/library/trees/xdc/xdc-D20.1/src/packages/
   249     */
   250