# rfSynchronizedPacketRx
SysConfig Notice
All examples will soon be supported by SysConfig, a tool that will help you graphically configure your software components. A preview is available today in the examples/syscfg_preview directory. Starting in 3Q 2019, with SDK version 3.30, only SysConfig-enabled versions of examples will be provided. For more information, click here.
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
Example Summary
In this example you will learn how to build a time-synchronized connection between one transmitter and a receiver. Time-synchronization enables both communication partners to transfer data quickly at predictable time points. Unlike the wake-on-radio example, the transmitter does not need to send a very long preamble and the receiver does not need to wait and check for a signal on air. This leads to the lowest possible power consumption on both sides. It also fits very well to the SimpleLink Long-range mode. Time synchronization builds also the foundation for Frequency and Time Division Multiple Access, FDMA and TDMA respectively.
This example project shows the receiver part. The transmission part can be found in the Synchronized Packet TX example.
Peripherals Exercised
Board_BUTTON1- Toggles between periodic and spontaneous beacon mode.Board_LED1- Reflects the status ofBoard_LED1on the transmitter.Board_LED2- On while the receiver is enabled (LNA enable), off when in standby.
Resources & Jumper Settings
This section explains the resource mapping across various boards. If you're
using an IDE (such as CCS or IAR), please refer to Board.html in your project
directory for resources used and board-specific jumper settings. Otherwise,
you can find Board.html in the directory
\ This section is similar for both TX and RX. You need 2 boards: one running the
Build and run the Build and run the Push You may push Explanation: After starting, the RX board goes into When the application on the TX board is started, it starts to send periodic
beacon messages. Once the RX board has received the first beacon message, it
switches the receiver off and goes into When Push Push Explanation: After pushing When pushing Repeat step 6 for a while. After a couple of minutes, you will notice that
Push Push Explanation: Both TX and RX board predict the following wake-up events based
on the time when synchronization happened. If both clocks have a small drift,
then the wake-up time will be incorrect after some time. By pushing This examples consists of a single task and the exported SmartRF Studio radio
settings. The RX application is implemented as a state machine with 3 states: In order to send synchronous packets, the receiver uses absolute start
triggers. Absolute start triggers are explained in the proprietary RF user's
guide and the technical reference manual. In The RX time stamp is the time when the first preamble bit was on air. The RF
core calculates this time based on the internal "sync word found" signal and
the RF settings provided in the SETUP command. The Finally, the application goes into the The RF driver takes care that the RF core is powered up and running before the
start trigger is due. For the end trigger, we use a time relative to the
command start. That means, the timeout is determined by:SmartRF06 in combination with one of the CC13x0 evaluation modules
Resource
Mapping / Notes
BUTTON1BTN_UP (up button)
BUTTON1BTN_DN (down button)
LED1LED1
LED2LED2CC1310 / CC1350 / CC2640R2 Launchpad
Resource
Mapping / Notes
BUTTON1BTN-1 (left button)
BUTTON2BTN_2 (right button)
LED1Green LED
LED2Red LED
Board Specific Settings
Example Usage
rfSynchronizedPacketTx application (TX board) and another one running the
rfSynchronizedPacketRx application (RX board).Initial synchronization
rfSynchronizedPacketRx example on the RX board.
You will see LED2 on the RX board being on all the time.rfSynchronizedPacketTx example on the TX board.
You will see LED2 on the TX board flashing with a period of 500 ms.
On the RX board, you will see that LED2 is flashing synchronously.BUTTON1 on the TX board. LED1 will toggle immediately.
On the RX board, LED1 follows after a short delay.BUTTON1 several times and will see that
LED1 on the RX board will always reflect the state
on the TX board with some delay.WaitingForSync state.
The receiver is switched on end waits for a packet. The LNA signal (LED2) is
enabled to reflect the current receiver state.SyncedRx state. In this state, it
wakes up the receiver right before the next packet from the TX board is
expected.BUTTON1 on the TX board is pushed, the current LED state is sent
in the next available time slot and is shown on the RX board as soon
as the packet has arrived.Sending spontaneous messages after synchronization
BUTTON2 on the TX board. You will see that LED2 on the
TX board stops flashing while LED2 on the RX boards remains
flashing.BUTTON1 on the TX board. You will see that LED1 toggles
on the TX board and with a short delay also on the RX board.
LED2 on the TX board will flash a short while after pushing
the button.BUTTON2 on the TX board, the TX application
goes into SporadicMessage state and stops sending periodic beacons.
The RX application remains in SyncedRx state and wakes up when it
expects a packet. As long as no button on the TX board is pushed,
the RX board will wake up only for a short time and go back to standby
after a very short timeout because no packet is received.BUTTON1 on the TX board, a packet with the new state of LED1
is transmitted. The TX board sends exactly at the same time when the RX board
expects to receive a packet. The RX board receives the message and updates the
state of its own LED1.Error handling: Re-synchronization due to crystal drift
LED1 on the RX board is not updated properly anymore.BUTTON1 on the RX board. LED2 will remain on permanently.BUTTON1 on the TX board. You will see LED1 toggle on both boards
and LED2 on the RX board starting to flash again.BUTTON1 on the RX board, the application goes back into
WaitingForSync state and re-synchronizes to the TX board.Application Design Details
WaitingForSync state, the receiver waits an infinite time in RX state.
That means, the power consumption is high. As soon as it receives a beacon
packet from the transmitter and the packet is valid, it uses the RX time stamp
as an anchor time: /* rxTime contains a calculated time stamp when the first preamble byte
* was sent on air. As a time base for the next wake ups, we calculate
* the time when this RX command would have been started for a synchronized
* wake up. */
RF_cmdPropRx.startTime = rxTime - RX_START_TO_SETTLE_TICKS - RX_START_MARGIN;
RX_START_TO_SETTLE_TICKS
needs to be subtracted because it takes some time between command start and
the receiver being ready to receive. In addition, RX_START_MARGIN is
subtracted to start the RX operation a bit earlier. This is necessary to
compensate possible crystal drifts.SyncedRx state where it calculates the
time for the next RX start based on the latest received packet: /* Start RX command to receive a single packet. Use an absolute start trigger
* and a predicted start time. The end time is calculated to be as tight as possible.
* The compensation margin for RAT drift in both directions needs to be taken into account. */
RF_cmdPropRx.startTrigger.triggerType = TRIG_ABSTIME;
RF_cmdPropRx.startTime += beacon.beaconInterval;
RF_cmdPropRx.endTrigger.triggerType = TRIG_REL_START;
RF_cmdPropRx.endTime = RX_START_TO_SETTLE_TICKS + RX_TIMEOUT_TICKS + RX_TIMEOUT_MARGIN + RX_START_MARGIN;