# rfWsnConcentratorOad
SysConfig Notice
All examples will soon be supported by SysConfig, a tool that will help you graphically configure your software components. A preview is available today in the examples/syscfg_preview directory. Starting in 3Q 2019, with SDK version 3.30, only SysConfig-enabled versions of examples will be provided. For more information, click here.
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
EasyLink Stack Configuration
Many parameters of the EasyLink stack can be configured using SysConfig including RX, TX, Radio, and Advanced settings. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name. Alternatively, refer to the System Configuration Tool (SysConfig) section of the Proprietary RF User's guide found in <SDK_INSTALL_DIR>/docs/proprietary-rf/proprietary-rf-users-guide.html.
Example Summary
The WSN Concentrator example illustrates how to create a simple Wireless Sensor Network Concentrator device which listens for packets from other nodes. This example is meant to be used together with the WSN Node example to form a one- to-many network where the nodes send messages to the concentrator.
This examples showcases the use of several Tasks, Semaphores and Events to receive packets, send acknowledgements and display the received data on the LCD. For the radio layer, this example uses the EasyLink API which provides an easy-to-use API for the most frequently used radio operations.
For more information on the EasyLink API and usage refer to the Proprietary RF User's guide
Peripherals Exercised
Board_PIN_LED0- Toggled when data is received over the RF interfaceBoard_PIN_BUTTON0- Select NodeBoard_PIN_BUTTON1- Select Action
Resources & Jumper Settings
If you're using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
Run the example. On another board (or several boards) run the WSN Node example. The LCD will show the discovered node(s). When the collector receives data from a new node, it is given a new row on the display and the received value is shown. If more than 7 nodes are detected, the device list rolls over, overriding the first. Whenever an updated value is received from a node, it is updated on the LCD display.
The example also supports Over The Air Update (OAD), where new FW can be loaded over OAD. The must be an OAD Server, which is included in the concentrator, and an OAD client which is included in the sensor.
* See rfWsnNode(Int/Ext)FlashOadClient project README for instructions on how to generate OAD images *
Performing an OAD Image Transfer
To be safe the external flash of the Concentrator should be wiped before running the example. To do this, program both LP boards with erase_extflash_cc13x0lp.hex. The program will flash the LEDs while erasing the external flash. Allow the application to run until the LEDs stop flashing indicating the external flash has been erased.
The FW to erase the external flash can be found in below location and should be loaded
using Uniflash programmer:
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/offChipOad/ccs/erase_extflash_cc13x0lp.hex
The Concentrator OAD Server and Node OAD Client FW should each be loaded into a CC1310LP/CC1350LP using the Uniflash programmer:
- Load rfWsnConcentratorOadServer (.out) project into a CC1310LP/CC1350LP
- Load
<SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/offChipOad/ccs/rfWsnNodeExtFlashOadClient_CC1310_LAUNCHXL_all_v1.bininto a CC1310LP/CC1350LP The Concentrator will display the below on the UART terminal:
Nodes Value SW RSSI
*0x0b 0887 0 -080
0xdb 1036 0 -079
0x91 0940 0 -079
Action: Update available FW
Info: Available FW unknown
Use the node display to identify the corresponding node ID:
Node ID: 0x91
Node ADC Reading: 1196
The node OAD image can be loaded into the external flash of the Concentrator through
the UART with the oad_write_bin.py script. The action must first be selected using
BTN-2. Press BTN-2 until the Action is set to Update available FW, then press BTN-1
and BTN-2 simultaneously to execute the action.
When "Available FW" is selected the terminal will display:
Waiting for Node FW update...
The UART terminal must be closed to free the COM port before the script is run. Then the python script can be run using the following command:
python <SDK>/tools/easylink/oad/oad_write_bin.py /dev/ttyS28 <SDK_DIR>/examples/rtos/CC1310_LAUNCHXL/easylink/hexfiles/offChipOad/ccs/rfWsnNodeExtFlashOadClient_CC1310_LAUNCHXL_app_v2.bin
After the download the UART terminal can be re-opened and the "Info" menu line will be updated to reflect the new FW available for OAD to a node.
The current FW version running on the node can be requested using the Send FW Ver Req
action. This is done by pressing BTN-1 until the desired node is selected (indicated by
the *), then pressing BTN-2 until the Action is set to Send FW Ver Req. To execute the
action, press BTN-1 and BTN-2 simultaneously.
The next time the node sends data to the concentrator, the FW version of the selected node will appear in the Info section.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Send FW Ver Req
Info: Node 0x91 FW v1.0
The node FW can now be updated to the image stored on the external flash of the
concentrator. Press BTN-1 until the desired node is selected, then press BTN-2 until
the Action is set to Update node FW. To execute the action, press BTN-1 and BTN-2
simultaneously.
The next time the node sends data, the OAD sequence will begin. As the node requests each image block from the concentrator the Concentrator display is updated to show the progress of the image transfer.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update node FW
Info: OAD Block 14 of 1089
The node display also updates to show the status of the image transfer.
Node ID: 0x91
Node ADC Reading: 3093
OAD Block: 14 of 1089
OAD Block Retries: 0
Once the OAD has completed, the concentrator will indicate that the transfer has
finished with an OAD Complete status. The node will reset itself with a new node ID.
If the device does not reset itself a manual reset may be necessary.
Application Design Details
This examples consists of two tasks, one application task and one radio protocol task.
The ConcentratorRadioTask handles the radio protocol. This sets up the EasyLink API and uses it to always wait for packets on a set frequency. When it receives a valid packet, it sends an ACK and then forwards it to the ConcentratorTask.
The ConcentratorTask receives packets from the ConcentratorRadioTask, displays the data on the LCD and toggles Board_PIN_LED0.
RadioProtocol.h can also be used to change the PHY settings to be either the default IEEE 802.15.4g 50kbit, Long Range Mode or custom settings. In the case of custom settings, the smartrf_settings.c file is used. This can be changed either by exporting from Smart RF Studio or directly in the file.
Note for IAR users: When using the CC1310DK, the TI XDS110v3 USB Emulator must be selected. For the CC1310_LAUNCHXL, select TI XDS110 Emulator. In both cases, select the cJTAG interface.
References
- For more information on the EasyLink API and usage refer to the Proprietary RF User's guide