Network Configurations¶
Changing Stack Parameters¶
The following sections provide the name and description of the most significant variables to be considered when designing a mesh network. They are ordered by project location as can be found in an imported Z-Stack project.
Note
Be sure to perform a clean build (Project → Clean) after configuring a parameter to ensure that the changes take effect.
Zigbee Device¶
Location: Project output folder → default/syscfg/ti_zstack_config.h
DEFAULT_CHANLIST: Set of 2.4-GHz channels that the Zigbee device will first attempt to operate onSECONDARY_CHANLIST: Set of 2.4-GHz channels to use ifDEFAULT_CHANLISTis unsuitableZDAPP_CONFIG_PAN_ID: Default PAN ID the coordinator will use to form the network, setting to 0xFFFF results in a random assignmentNWK_INDIRECT_MSG_TIMEOUT: Maximum time that parent will buffer indirect messages for its sleeping end devicesAPSC_MAX_FRAME_RETRIES: Maximum number of APS layer retries, this value plus one is the maximum number of attemptsNWK_MAX_DATA_RETRIES: Maximum number of NWK layer retriesMAX_RTG_ENTRIES: Maximum number of AODV routing entries, maintained byROUTE_EXPIRY_TIMEDEFAULT_KEY: Default network security key, if set to all 0x00 then a random key will be generatedDEFAULT_TC_LINK_KEY: Pre-configured Trust Center link key and must remain as default for Zigbee Alliance 3.x complianceRFD_RCVC_ALWAYS_ON: Determines whether an end device is allowed to enter standby mode for low power operationPOLL_RATE: End device time delay before requesting data from its parent, must be shorter than theEND_DEV_TIMEOUT_VALUEto avoid being aged out and can be disabled by setting the value to 0xFFFFFFFFMINIMUM_APP_POLL_RATE: Limit to the frequency of end device polls while the application is operationalTXPOWER: Determined output power of the device in dBmNWK_MAX_DEVICE_LIST: Number of direct children supported by the association table, further maintained by child agingZDSECMGR_TC_DEVICE_MAX: Maximum number of unique trust center link keys supported (and therefore Zigbee 3.x devices allowed) in the networkEND_DEV_TIMEOUT_VALUE: Timeout value for child aging as sent by the end device during the NWK association’s end device timeout request
Note
This file is generated automatically from the project’s .syscfg file. Please see Zigbee Configuration.
Network Parameters¶
Location: Stack/nwk/nwk_globals.h
NWK_LINK_STATUS_PERIOD: Interval for which link status reports are broadcast on the network, a jitter mask ofLINK_STATUS_JITTER_MASKis usedMAX_NEIGHBOR_ENTRIES: Number of neighbors supported by the neighbor table, maintained byNWK_ROUTE_AGE_LIMITMAX_RTG_SRC_ENTRIES: Number of cached source routes, coordinator MTO-routing specific and should equal the max number of nodes in the the networkSRC_RTG_EXPIRY_TIME: Hop count for concentrator route discoveries, pertains only to coodinator MTO-routing
Z-Stack Parameters¶
Location: Stack/sys/zglobals.h
MAX_POLL_FAILURE_RETRIES: Maximum retries for an end device not receiving ACKsCONCENTRATOR_ENABLE: Set to TRUE for coordinator MTO routingCONCENTRATOR_DISCOVERY_TIME: MTO RREQ broadcast period in seconds, set to zero to disableCONCENTRATOR_ROUTE_CACHE: Source route cache table, setting to TRUE is recommended for applications with allowable RAM spaceNWK_END_DEVICE_LEAVE_TIMEOUT: Further time for which a leave request will be queued for children who have unknowingly aged out
Base Device Behavior¶
Location: Stack/bdb/bdb.h
TCLK_POLL_RATE: Poll rate for the Trust Center link key exchange processBDB_DEFAULT_TC_LINK_KEY_EXCHANGE_ATTEMPS_MAX: Number of times a device will attempt a link key exchange with the trust centerBDBC_TC_LINK_KEY_EXANGE_TIMEOUT: Time before link exchange fails, at which point the device will try again if attempts remain
Location: Stack/bdb/bdb_interface.h
BDBC_MIN_COMMISSIONING_TIME: Length of time to commission the network for which permit join is enabled, a maximum of 254 seconds is required in accordance with Zigbee 2015 and later specificationBDB_INSTALL_CODE_USE: Defines which method of install code is used if enabledBDB_DEFAULT_JOIN_USES_INSTALL_CODE_KEY: Enables install codes if set to TRUEBDB_DEFAULT_TC_REQUIRE_KEY_EXCHANGE: LeaveFALSEto allow pre-Zigbee 3.x devices to join the network
Determining Project Build Size¶
Project options such as device type (ZC, ZR, ZED, ZNP), features (OTA, UART, etc), and the network configurations provided above will affect the flash and RAM space required to build the application. In order to understand this dependency, it is possible to refer to the MAP file generated after building a Z-Stack project. For CCS this is the MEMORY CONFIGURATION section at the top of the MAP file located inside the default folder, where total Flash is equivalent to the total of the FLASH, FLASH_NV, and FLASH_LAST used rows. With IAR it is the Grand Total at the bottom of the MAP file found within the Output folder by adding the code, ro data, and rw data columns.