Example Applications¶
This section provides an overview of the out-of-box example applications available for DMM and what platforms each example support.
The DMM examples showcase different combinations of the supported TI stacks: BLE, TI 15.4, Zigbee and EasyLink. The BLE connection is setup to demonstrate how the application can be designed to interact with the second stack and its network in order to provide features such as provisioning and reading out network data.
The example applications provided for DMM are developed for CC13x2 or CC26x2 devices. Which devices each example supports are described below. For which development boards are supported, please refer to the example’s README.
Example Application Design¶
In examples where there exists communication between the different stacks, an “application communication interface” has been implemented. While each example defines a unique set of actions in regards to stack-to-stack communication, all of them use the same interface design concept.
In all examples, the BLE application is considered the “Interface master”. In the context of the interface, “master” simply refers to the application responsible for implementing the interface while the “slave” is the other stack.
For each interface, the interface master allows the slave to register a set of callbacks that the master can use to interact with the slave. The set of callbacks varies depending on the use case. In addition to the callbacks, the master may define a few functions which the slave can use to interact with the master.
For example, in the WSN Node + BLE Remote Display example, the WSN Node is acting as the slave and can register callbacks for setting the report interval and reading the current sensor value. The BLE application also provides an API which the WSN Node can use to notify the BLE application that the sensor data has been updated.
The sequence diagram below showcases the typical setup and usage of the
stack-to-stack interfaces. To see which callbacks and APIs that is available
for an example, see the BLE application remote_display.h
header file.
Common User Interface¶
The Common User Interface (CUI) controls the access to User Interface
resources. On a LaunchPad, these resources are made up of Buttons, LEDs and UART
I/O. The CUI allows both of the two stack applications to use the resources. If
you want to read more about the CUI, you can see cui.h
.
2.4 GHz Examples¶
Some of the DMM example projects have a *_2_4g
suffix. These examples are
configured to use the 2.4 GHz PHY for the TI 15.4-Stack application. The
analogy would be the *_2_4g
suffix TI 15.4-Stack example projects.
You can read more about the 2.4 GHz PHY for the TI 15.4-Stack in the TI 15.4-Stack User’s Guide.
OAD Examples¶
The examples that have oad
as part of their names are enabled to do
over-the-air firmware upgrade (OAD) over BLE. You can read more about
OAD in the BLE5-Stack User’s Guide.
SM Examples¶
Examples that have sm
as part of their name showcase the TI 15.4 stack secure
commissioning feature. These examples uses a security manager
which allows
secure commissioning to a TI 15.4 network via a BLE central such as a smartphone.
The SimpleLink Starter
mobile application has built in support for this
service and provides a graphical overview of the commissioning process.
You can read more about how to use the mobile application in the example README
files.
More information on the TI 15.4 Secure Commissioning feature can be found in the TI 15.4-Stack User’s Guide.
Block Mode Examples¶
Most of the examples that operate at least one “end device” stack role allow for evaluation of the Block Mode feature. This include examples that implement at least one of the following stack roles:
- TI 15.4 Sensor
- BLE Peripheral
- Zigbee End-Device
For more information on how to use it for a given example, please see the
README.html
included with the respective application source code.
Running the Applications¶
For information on how to run the example applications below, please see the
README.html
included with the respective application source code.
List of Example Applications¶
WSN Node + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-1/2/4
Stack roles: BLE Peripheral + EasyLink WSN Node
This example project showcases a Bluetooth 5 enabled EasyLink WSN Node. The BLE
profile Remote Display
can be used to interact with the WSN Node as well as
the WSN Concentrator the node is connected to. For information on how to setup
the WSN Concentrator, see the example README.
This example serves as a good starting point for developing a BLE + Proprietary RF stack application.
WSN Node + BLE Simple Peripheral Example Application¶
LaunchPads supported: CC1352R, CC1352P-1/2/4
Stack roles: BLE Peripheral + EasyLink WSN Node
This example project showcases a combination of a Bluetooth 5 peripheral and an EasyLink WSN node were both stacks operate independently of each other. This serves as a demonstration of the minimum additions needed in order to combine two stacks using the DMM. The DMM handles the scheduling of RF commands while keeping the stacks unaware of each other.
TI 15.4 Sensor + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-1/2/4, CC2652R, CC2652RB, CC2652RSIP
Stack roles: BLE Peripheral + TI 15.4 Sensor
These example projects showcase a Bluetooth 5 enabled TI 15.4 Sensor node. The BLE
profile Remote Display
can be used for provisioning the TI 15.4 sensor as
well as monitoring the sensor when connected to a network. The examples
demonstrate a more complex stack combination and DMM policy.
Note
When operating the TI 15.4 sensor in Frequency Hopping mode, provisioning might cause the BLE connection to be dropped. In this case, the BLE connection can be re-established once the sensor has joined the network.
Depending on what platform is used, different variants of the example are available to showcase either a Sub-1 GHz or 2.4 GHz TI 15.4 sensor. The TI 15.4 Sensor can be configured to operate in either Non-beacon, Beacon or Frequency Hopping mode. The default mode of operation for all TI 15.4 examples is Non-beacon mode. How to change between the different modes are described in the project README files.
Note
The TI 15.4 Frequency Hopping mode within DMM applications is validated with 50 channels (Frequency Hopping Channel Mask and Frequency Hopping Asynchronous Channel Mask).
Sub-1 GHz TI 15.4 Sensor: CC1352R, CC1352P-1/2/4
In this example, the TI 15.4 Sensor is operating in the Sub-1 GHz range using non-beacon mode.
- DMM 15.4 Sensor + Remote Display README
- DMM 15.4 Sensor + Remote Display OAD README
- DMM 15.4 Sensor + Remote Display Security Manager README
2.4 GHz TI 15.4 Sensor: CC1352R, CC1352P-2/4, CC2652R, CC2652RB, CC2652RSIP
In this example, the TI 15.4 Sensor is operating in the 2.4 GHz band using non-beacon mode.
TI 15.4 Collector + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-1/2/4, CC2652R, CC2652RB, CC2652RSIP
Stack roles: BLE Peripheral + TI 15.4 Collector
These example projects showcase a Bluetooth 5 enabled TI 15.4 Collector. The BLE
profile Remote Display
can be used for provisioning the TI 15.4 network as
well as monitoring other sensors in the network.
Depending on what platform is used, different variants of the example are available to showcase either a Sub-1 GHz or 2.4 GHz TI 15.4 collector. The TI 15.4 network can be configured to operate in either Non-beacon, Beacon or Frequency Hopping mode. The default mode of operation for all TI 15.4 examples is Non-beacon mode. How to change between the different modes are described in the project README files.
Sub-1 GHz TI 15.4 Collector: CC1352R, CC1352P-1/2/4
In this example, the TI 15.4 Collector is operating in the Sub-1 GHz range using non-beacon mode.
- DMM 15.4 Collector + Remote Display README
- DMM 15.4 Collector + Remote Display OAD README
- DMM 15.4 Collector + Remote Display Security Manager README
2.4 GHz TI 15.4 Collector: CC1352R CC1352P-2/4, CC2652R, CC2652RB, CC2652RSIP
In this example, the TI 15.4 Collector is operating in the 2.4 GHz band using non-beacon mode.
Zigbee Coordinator Switch + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-2, CC2652R, CC2652RB, CC2652RSIP
Stack roles: BLE Peripheral + Zigbee Coordinator
This example project showcases BLE and the Zigbee running together using the DMM. The example enables a concurrent Zigbee coordinator device and a Bluetooth 5 peripheral. A BLE central such as a smart phone can be used to start the Zigbee network and begin commissioning other devices onto the network.
Information on how to provision the Zigbee network and how to use the available BLE characteristics is found in the example README.
Zigbee End Device Switch + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-2, CC2652R, CC2652RB, CC2652RSIP
Stack roles: BLE Peripheral + Zigbee End Device
This example project showcases BLE and the Zigbee running together using the DMM. The Zigbee application is acting as an end device switch while the Bluetooth 5 peripheral provide provisioning and monitoring functionality.
The example is meant to be used in conjunction with a Zigbee light coordinator
example (zc_light
or the Zigbee light DMM example). Information on how to
provision the Zigbee device and how to use the available BLE characteristics is
found in the example README.
Zigbee Router Light + BLE Remote Display Example Application¶
LaunchPads supported: CC1352R, CC1352P-2, CC2652R, CC2652RB, CC2652RSIP
Stack roles: BLE Peripheral + Zigbee Router
This example project showcases BLE and the Zigbee running together using the DMM. The Zigbee application is a router running a light device application while the Bluetooth 5 peripheral provide provisioning and monitoring functionality.
The example is meant to be used in conjunction with a Zigbee light coordinator
example (zc_light
or the Zigbee light DMM example). Information on how to
provision the Zigbee device and how to use the available BLE characteristics is
found in the example README.