ECDSACC26X1.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
49 #ifndef ti_drivers_ecdsa_ECDSACC26X1__include
50 #define ti_drivers_ecdsa_ECDSACC26X1__include
51 
52 #include <stdint.h>
53 #include <stdbool.h>
54 
55 #include <ti/drivers/ECDSA.h>
56 #include <ti/drivers/TRNG.h>
58 
59 #include <ti/devices/DeviceFamily.h>
60 #include DeviceFamily_constructPath(driverlib/rom_ecc.h)
61 
62 #ifdef __cplusplus
63 extern "C" {
64 #endif
65 
72 typedef struct {
85  uint8_t trngIntPriority;
87 
93 typedef struct {
94  bool isOpen;
97  ECC_State eccState;
98  uint32_t eccWorkZone[288];
100 
101 #ifdef __cplusplus
102 }
103 #endif
104 
105 #endif /* ti_drivers_ecdsa_ECDSACC26X1__include */
TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:608
ECDSACC26X1 Object.
Definition: ECDSACC26X1.h:93
uint8_t trngIntPriority
TRNG Peripheral&#39;s interrupt priority.
Definition: ECDSACC26X1.h:85
TRNG driver implementation for the CC26XX family.
bool isOpen
Definition: ECDSACC26X1.h:94
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSACC26X1.h:96
ECDSA_CallbackFxn callbackFxn
Definition: ECDSACC26X1.h:95
ECDSACC26X1 Hardware Attributes.
Definition: ECDSACC26X1.h:72
TRNG driver header.
ECC_State eccState
Definition: ECDSACC26X1.h:97
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale