UDMACC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
102 #ifndef ti_drivers_UDMACC26XX__include
103 #define ti_drivers_UDMACC26XX__include
104 
105 #include <stdint.h>
106 #include <stdbool.h>
107 
108 #include <ti/drivers/Power.h>
110 
111 #include <ti/devices/DeviceFamily.h>
112 #include DeviceFamily_constructPath(inc/hw_types.h)
113 #include DeviceFamily_constructPath(driverlib/udma.h)
114 
115 #ifdef __cplusplus
116 extern "C" {
117 #endif
118 
129 /* Add DMACC26XX_STATUS_* macros here */
130 
143 /* Add DMACC26XX_CMD_* macros here */
144 
148 #if !defined(UDMACC26XX_CONFIG_BASE) && \
149  (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 || \
150  DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X1_CC26X1)
151  #define UDMACC26XX_CONFIG_BASE 0x20001800
152 #elif !defined(UDMACC26XX_CONFIG_BASE)
153  #define UDMACC26XX_CONFIG_BASE 0x20000400
154 #endif
155 
157 #if(UDMACC26XX_CONFIG_BASE & 0x3FF)
158  #error "Base address for DMA control table 'UDMACC26XX_CONFIG_BASE' must be 1024 bytes aligned."
159 #endif
160 
162 #if defined(__IAR_SYSTEMS_ICC__)
163 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
164 __no_init static volatile tDMAControlTable ENTRY_NAME @ UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable)
165 #elif defined(__TI_COMPILER_VERSION__) || defined(__clang__)
166 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
167 static volatile tDMAControlTable ENTRY_NAME __attribute__((retain, location(\
168  UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable))))
169 #elif defined(__GNUC__)
170 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
171  extern int UDMACC26XX_ ## ENTRY_NAME ## _is_placed; __attribute__ ((section("."#ENTRY_NAME))) static volatile tDMAControlTable ENTRY_NAME = {&UDMACC26XX_ ## ENTRY_NAME ## _is_placed}
172 #else
173 #error "don't know how to define ALLOCATE_CONTROL_TABLE_ENTRY for this toolchain"
174 #endif
175 
177 #define UDMACC26XX_SET_TRANSFER_SIZE(SIZE) (((SIZE - 1) << UDMA_XFER_SIZE_S) & UDMA_XFER_SIZE_M)
178 
179 #define UDMACC26XX_GET_TRANSFER_SIZE(CONTROL) (((CONTROL & UDMA_XFER_SIZE_M) >> UDMA_XFER_SIZE_S) + 1)
180 
184 typedef struct {
185  bool isOpen;
186  HwiP_Struct hwi;
188 
192 typedef struct {
193  uint32_t baseAddr;
194  PowerCC26XX_Resource powerMngrId;
195  uint8_t intNum;
217  uint8_t intPriority;
219 
223 typedef struct {
224  void *object;
225  void const *hwAttrs;
227 
232 
233 /* Extern'd hwiIntFxn */
234 extern void UDMACC26XX_hwiIntFxn(uintptr_t callbacks);
235 
248 __STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
249 {
250  UDMACC26XX_Object *object;
251 
252  /* Get the pointer to the object */
253  object = (UDMACC26XX_Object *)(handle->object);
254 
255  /* mark the module as available */
256  object->isOpen = false;
257 }
258 
274 extern UDMACC26XX_Handle UDMACC26XX_open();
275 
289 __STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
290 {
291  UDMACC26XX_HWAttrs const *hwAttrs;
292 
293  /* Get the pointer to the hwAttrs */
294  hwAttrs = (UDMACC26XX_HWAttrs *)(handle->hwAttrs);
295 
296  /* Enable DMA channel */
297  HWREG(hwAttrs->baseAddr + UDMA_O_SETCHANNELEN) = channelBitMask;
298 }
299 
318 __STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
319 {
320  UDMACC26XX_HWAttrs const *hwAttrs;
321 
322  /* Get the pointer to the hwAttrs */
323  hwAttrs = (UDMACC26XX_HWAttrs *)(handle->hwAttrs);
324 
325  /* Check if REQDONE is set for a specific channel */
326  return (uDMAIntStatus(hwAttrs->baseAddr) & channelBitMask) ? true : false;
327 }
328 
346 __STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
347 {
348  UDMACC26XX_HWAttrs const *hwAttrs;
349 
350  /* Get the pointer to the hwAttrs and object */
351  hwAttrs = (UDMACC26XX_HWAttrs *)(handle->hwAttrs);
352 
353  /* Clear UDMA done interrupt */
354  uDMAIntClear(hwAttrs->baseAddr, channelBitMask);
355 }
356 
374 __STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
375 {
376  UDMACC26XX_HWAttrs const *hwAttrs;
377 
378  /* Get the pointer to the hwAttrs */
379  hwAttrs = (UDMACC26XX_HWAttrs *)(handle->hwAttrs);
380 
381  HWREG(hwAttrs->baseAddr + UDMA_O_CLEARCHANNELEN) = channelBitMask;
382 }
383 
404 __STATIC_INLINE void UDMACC26XX_disableAttribute(UDMACC26XX_Handle handle,
405  uint32_t channelNum, uint32_t attr)
406 {
407  UDMACC26XX_HWAttrs const *hwAttrs;
408 
409  /* Get the pointer to the hwAttrs */
410  hwAttrs = (UDMACC26XX_HWAttrs *)(handle->hwAttrs);
411 
412  uDMAChannelAttributeDisable(hwAttrs->baseAddr, channelNum, attr);
413 }
414 
430 extern void UDMACC26XX_close(UDMACC26XX_Handle handle);
431 
432 #ifdef __cplusplus
433 }
434 #endif
435 
436 #endif /* ti_drivers_UDMACC26XX__include */
bool isOpen
Definition: UDMACC26XX.h:185
HwiP_Struct hwi
Definition: UDMACC26XX.h:186
void UDMACC26XX_hwiIntFxn(uintptr_t callbacks)
PowerCC26XX_Resource powerMngrId
Definition: UDMACC26XX.h:194
void UDMACC26XX_close(UDMACC26XX_Handle handle)
Function to close the DMA driver.
__STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:346
Power Manager.
__STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:289
uint8_t intNum
Definition: UDMACC26XX.h:195
__STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
Function to initialize the CC26XX DMA driver.
Definition: UDMACC26XX.h:248
__STATIC_INLINE void UDMACC26XX_disableAttribute(UDMACC26XX_Handle handle, uint32_t channelNum, uint32_t attr)
Definition: UDMACC26XX.h:404
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:223
Power manager interface for CC26XX/CC13XX.
UDMACC26XX_Handle UDMACC26XX_open()
Function to initialize the CC26XX DMA peripheral.
UDMACC26XX hardware attributes.
Definition: UDMACC26XX.h:192
void * object
Definition: UDMACC26XX.h:224
uint8_t intPriority
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral&#39;s interrupt priority...
Definition: UDMACC26XX.h:217
__STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:374
__STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:318
uint32_t baseAddr
Definition: UDMACC26XX.h:193
UDMACC26XX object.
Definition: UDMACC26XX.h:184
UDMACC26XX_Config * UDMACC26XX_Handle
A handle that is returned from a UDMACC26XX_open() call.
Definition: UDMACC26XX.h:231
void const * hwAttrs
Definition: UDMACC26XX.h:225
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale