TI-OpenThread SysConfig

SysConfig with TI-OpenThread provides a graphical interface to configure application-level parameters for the OpenThread stack, such as network credentials and default channel.

All TI-OpenThread examples have a SysConfig-enabled version, located under <SDK>/examples/syscfg_preview/. When imported, the SysConfig tool is opened by double-clicking the *.syscfg file in the project location. In the SysConfig tool, TI-OpenThread is listed as a separate software component under RF-stacks. Click on the component to open the TI-OpenThread configuration view.

../_images/fig-tiop-rf-stacks.png

Figure 84. TI-OpenThread software component in SysConfig

Warning

One important note about TI-OpenThread SysConfig is how SysConfig settings and non-volatile storage settings are applied. If the LaunchPad’s non-volatile storage holds a valid Thread dataset, SysConfig settings will not be applied on boot. SysConfig settings are only applied when non-volatile storage does not hold a valid Thread dataset. To guarantee SysConfig settings are applied, perform a factory reset of the non-volatile storage.

TI-OpenThread Settings

The TI-OpenThread configuration is locked to the device type of the example project. In other words, if the imported example is configured for the FTD device type, the TI-OpenThread SysConfig will be locked for the FTD device type.

View available parameters by expanding parameter groups. Hovering the cursor over a parameter group or a parameter will display a question mark next to the name, which when clicked on will display more information for that particular parameter or parameter group.

../_images/fig-tiop-configuration.png

Figure 85. TI-OpenThread configuration view

You can see the generated files by clicking the <> symbol in the top right corner. The Board.c/h files was generated by the TI DRIVERS components, the smartrf_settings/smartrf_settings.c/h was generated by the RF Driver component, and the tiop_config.c/h files was generated by the TI-OpenThread component.

../_images/fig-tiop-generated-files.png

Figure 86. Generated files from TI-OpenThread configuration

The files are generated when building the project. After the build has completed, you will find the generated files in the output folder of your project.

Attention

Whenever you re-build the project, SysConfig will re-generate the files. Because of this, any changes made directly in the generated files will be overwritten.

tiop_config Reference

TI-OpenThread configuration in SysConfig generates a set of defines which configures the tiop_config file. Below is a compilation of available SysConfig parameters for TI-OpenThread and which corresponding define names are set for that parameter.

Submodule Configurable Name Define Name
Top Level Device Type TIOP_CONFIG_LINK_MODE_D
Power Management Power Mode of Operation TIOP_CONFIG_LINK_MODE_R
Poll Peroid TIOP_CONFIG_POLL_PERIOD
Radio Default Channel TIOP_CONFIG_LINK_CHANNEL
Default Power TIOP_CONFIG_TX_POWER
Network Set Network ID TIOP_CONFIG_SET_NW_ID
PAN ID TIOP_CONFIG_PAN_ID
Extended PAN ID TIOP_CONFIG_EXT_PAN_ID
Thread Master Key TIOP_CONFIG_MASTER_KEY_L TIOP_CONFIG_MASTER_KEY_U
Network Name TIOP_CONFIG_NETWORK_NAME
Security Pre-Shared Key TIOP_CONFIG_PKSD