rfWsnNodeIntFlashOadClientPApp
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
EasyLink Stack Configuration
Many parameters of the EasyLink stack can be configured using SysConfig including RX, TX, Radio, and Advanced settings. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name. Alternatively, refer to the System Configuration Tool (SysConfig) section of the Proprietary RF User's guide found in <SDK_INSTALL_DIR>/docs/proprietary-rf/proprietary-rf-users-guide.html.
Example Summary
The WSN Node Internal Flash OAD Client example illustrates how to create a Wireless Sensor Network Node device which sends sensor data to a Sub-1GHz WSN Concentrator OAD Server and also allows the device to wirelessly update its firmware through an OAD (Over the Air Download).
This examples showcases the use of several Tasks, Semaphores and Events to get sensor updates and send packets with acknowledgement from the concentrator. For the radio layer, this example uses the EasyLink API which provides an easy-to-use API for the most frequently used radio operations. This example builds upon the existing WSN Node; adding the ability to communicate with the OAD server using the OAD protocol. The Agama on-chip OAD client is split between two separate applications, the User App and the Persistent App.
The Persistent App (P-App) is an OAD client that only handles communication with the OAD server including updating the U-App through an OAD. It supports all OAD protocol packets. When the P-App starts up it will attempt to load connection information from NVS (creates a new connection otherwise) and begin communicating with the OAD server. After completing a firmware update it will reset the device and the BIM will boot into the new U-App.
Peripherals Exercised
Board_PIN_RLED
- Toggled when the a packet is sentBoard_ADCCHANNEL_A0
- Used to measure the Analog Light Sensor by the SCE taskBoard_PIN_BTN1
- Selects fast report or slow report mode. In slow report mode the sensor data is sent every 5s or as fast as every 1s if there is a significant change in the ADC reading. The fast reporting mode sends the sensor data every 1s regardless of the change in ADC value. The default is slow reporting mode.
Resources & Jumper Settings
If you're using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
- Run the example. On another board run the WSN Concentrator OAD Server example. This node should show up on the LCD of the Concentrator.
The example also supports Over The Air Download (OAD), where new FW can be transferred from the concentrator to the node. There must be an OAD Server, which is included in the concentrator project, and an OAD client, which is included in the node project.
Performing an OAD Image Transfer
To be safe the external flash of the Concentrator should be wiped before running the example. To do this, program both LP boards with erase_storage_offchip_cc13x2lp.hex. The program will flash the LEDs while erasing the external flash. Allow the application to run until the LEDs stop flashing indicating the external flash has been erased.
The FW to erase the external flash can be found in below location and should be loaded
using Uniflash programmer:
<SDK_DIR>/examples/rtos/CC1352R1_LAUNCHXL/easylink/hexfiles/offChipOad/erase_storage_offchip_cc13x2lp.hex
OAD with Easylink
The Concentrator OAD Server and Node OAD Client FW should each be loaded into a CC1312R1LP/CC1352R1LP using the Uniflash programmer:
- Load rfWsnConcentratorOadServer (.out) project into a CC1312R1LP/CC1352R1LP
- Load
<SDK_DIR>/examples/rtos/CC1352R1_LAUNCHXL/easylink/hexfiles/offChipOad/rfWsnNodeIntFlashOadClientUApp_CC1352R1_LAUNCHXL_app_v1.hex
and<SDK_DIR>/examples/rtos/CC1352R1_LAUNCHXL/easylink/hexfiles/offChipOad/rfWsnNodeIntFlashOadClientPApp_CC1352R1_LAUNCHXL.hex
and<SDK_DIR>/examples/rtos/CC1352R1_LAUNCHXL/easylink/hexfiles/offChipOad/cc13x2r1lp_bim_offchip.hex
into a CC1312R1LP/CC1352R1LP by selecting multiple files in Uniflash
The Concentrator will display the below on the UART terminal:
Nodes Value SW RSSI
*0x0b 0887 0 -080
0xdb 1036 0 -079
0x91 0940 0 -079
Action: Update available FW
Info: Available FW unknown
Use the node display to identify the corresponding node ID:
Node ID: 0x91
Node ADC Reading: 1196
The node OAD image can be loaded into the external flash of the Concentrator through
the UART with the oad_write_bin.py script. The action must first be selected using
BTN-2. Press BTN-2 until the Action is set to Update available FW
, then press BTN-1
and BTN-2 simultaneously to execute the action.
When "Available FW" is selected the terminal will display:
Waiting for Node FW update...
The UART terminal must be closed to free the COM port before the script is run. Then the python script can be run using the following command:
python <SDK>/tools/easylink/oad/oad_write_bin.py /dev/ttyS28 <SDK_DIR>/examples/rtos/CC1352R1_LAUNCHXL/easylink/hexfiles/offChipOad/rfWsnNodeIntFlashOadClientPApp_CC1352R1_LAUNCHXL_app_v2.bin
After the download the UART terminal can be re-opened and the "Info" menu line will be updated to reflect the new FW available for OAD to a node.
The current FW version running on the node can be requested using the Send FW Ver Req
action. This is done by pressing BTN-1 until the desired node is selected (indicated by
the *), then pressing BTN-2 until the Action is set to Send FW Ver Req
. To execute the
action, press BTN-1 and BTN-2 simultaneously.
The next time the node sends data to the concentrator, the FW version of the selected node will appear in the Info section.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Send FW Ver Req
Info: Node 0x91 FW sv:0001, bv:01
Where:
* sv
is the FW version number
* bv
is the version number of the BIM
The node FW can now be updated to the image stored on the external flash of the
concentrator. Press BTN-1 until the desired node is selected, then press BTN-2 until
the Action is set to Update node FW
. To execute the action, press BTN-1 and BTN-2
simultaneously.
The next time the node sends data, the OAD sequence will begin. As the node requests each image block from the concentrator the Concentrator display is updated to show the progress of the image transfer.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0x91 0940 0 -079
Action: Update node FW
Info: OAD Block 14 of 1089
The node display also updates to show the status of the image transfer.
Node ID: 0x91
Node ADC Reading: 3093
OAD Block: 14 of 1089
OAD Block Retries: 0
Once the OAD has completed, the concentrator will indicate that the transfer has
finished with an OAD Complete
status. The node will reset itself with a new node ID.
If the device does not reset itself a manual reset may be necessary.
Nodes Value SW RSSI
0x0b 0887 0 -080
0xdb 1036 0 -079
*0xe2 0940 0 -079
Action: Update node FW
Info: Node 0xe2 FW Unknown
A firmware version request can then be performed to verify the new image.
Generating OAD Images
For generating the images the following tools are required:
- Code Composer Studio
-- Download the latest version from http://www.ti.com/tool/CCSTUDIO
- Simplelink CC13X2 SDK
-- Download the latest version from http://www.ti.com/tool/SIMPLELINK-CC13X2-26x2-SDK
- Python 2.7
- Python intelhex-2.1
- Python crcmod-1.7
Creating the Application Hex Image
To generate the application hex file, the project should be imported and built with the
desired compiler. To change the FW version, update the following string in oad/native_oad/oad_image_header_app.c
#define SOFTWARE_VER {'0', '2', '0', '1'}
where the above would correspond to v2.01 for the software version.
Creating the Application Binary Image
Add the following post build step. In Code Composer Studio, navigate to Project → Properties → Build, then clicking the Steps tab. In IAR Embedded Workbench, navigate to Options → Build Actions and appending the new step with a semicolon separator.
${COM_TI_SIMPLELINK_CC13X2_SDK_INSTALL_DIR}/tools/common/oad/oad_image_tool --verbose <compiler> ${PROJECT_LOC} 7 -hex1 ${ConfigName}/${ProjName}.hex -o ${ConfigName}/${ProjName}
Make sure to replace <compiler>
with the appropriate compiler (ccs, gcc, or iar).
If the application was built with the SECURITY flag then the OAD image tool needs an extra option -k
plus the path to a generated private key. In order to generate a key go to
${COM_TI_SIMPLELINK_CC13X2_SDK_INSTALL_DIR}/tools/common/oad/oad_image_tool --verbose <compiler> ${PROJECT_LOC} 7 -hex1 ${ConfigName}/${ProjName}.hex -o ${ConfigName}/${ProjName} -k ${COM_TI_SIMPLELINK_CC13X2_SDK_INSTALL_DIR}/tools/common/oad/keys/private.pem
* Note The OAD binary will be generated in the Debug dir in the project. The .out file can be used for debugging through CCS without any changes to the BIM. However, if the .out file is flashed to the device the JTAG_DEBUG compiler flag must be defined in the BIM project. *
* Note If building the BIM project only, make sure that either the Debug_unsecure
or Release_unsecure
build configurations are selected *
Application Design Details
This examples consists of two tasks, one application task and one radio protocol task. It also consists of a Sensor Controller Engine (SCE) Task which samples the ADC.
On initialization the CM3 application sets the minimum report interval and the minimum change value which is used by the SCE task to wake up the CM3. The ADC task on the SCE checks the ADC value once per second. If the ADC value has changed by the minimum change amount since the last time it notified the CM3, it wakes it up again. If the change is less than the masked value, then it does not wake up the CM3 unless the minimum report interval time has expired.
The NodeTask waits to be woken up by the SCE. When it wakes up it toggles
Board_PIN_LED1
and sends the new ADC value to the NodeRadioTask.The NodeRadioTask handles the radio protocol. This sets up the EasyLink API and uses it to send new ADC values to the concentrator. After each sent packet it waits for an ACK packet back. If it does not get one, then it retries three times. If it did not receive an ACK by then, then it gives up.
The core of the P-App works the same as the rfWsnNode example. On startup it will check NVS for any valid connection information. If none exists it generates a random node address and begins sending ADC packets to any server that might be listening. If connection data does exist then the P-App will load the Node address and set it as its own. It will then load the server address and send a OADProtocol_PACKET_TYPE_OAD_RESET_RSP packet to respond to the one that the U-App received. In this situation the P-App is picking up the connection where the U-App left off. It appears to the server as the same node and responds to the request that the U-App received. If the P-App loads connection data from NVS it will clear the storage to keep from loading that connection again on future runs. Once an OAD has begun the P-App will begin to overwrite the old U-App image in flash, one block at a time. After all blocks of the new image have been downloaded it will reset the device and the BIM will boot into the new U-App.
RadioProtocol.h can also be used to configure the PHY settings from the following options: IEEE 802.15.4g 50kbit (default), Long Range Mode or custom settings. In the case of custom settings, the ti_radio_config.c file is used. The configuration can be changed by exporting a new ti_radio_config.c file from Smart RF Studio or modifying the file directly.
Internal Flash Layout
|----------------------| 0x58000
| BIM |
|----------------------| 0x56000
| |
| |
| P-App |
| |
| |
|----------------------| 0x44000
| NVS |
|----------------------| 0x42000
| Unused Space |
|----------------------| 0x40000
| |
| |
| |
| U-App |
| |
| |
| |
|----------------------| 0x00000
References
- For more information on the EasyLink API and usage refer to the Proprietary RF User's guide