ADCBufCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file ADCBufCC26XX.h
34  *
35  * @brief ADCBuf driver implementation for a CC26XX analog-to-digital
36  * converter
37  *
38  * # Driver include #
39  * The ADCBuf header file should be included in an application as follows:
40  * @code
41  * #include <ti/drivers/ADCBuf.h>
42  * #include <ti/drivers/adc/ADCBufCC26XX.h>
43  * @endcode
44  *
45  * # Overview #
46  * This is a CC26XX specific implementation of the generic TI-RTOS ADCBuf driver.
47  * The generic ADCBuf API specified in ti/drivers/ADCBuf.h should be called by
48  * the application, not the device specific implementation in
49  * ti/drivers/adcbuf/ADCBufCC26XX. The board file defines the device specific
50  * configuration and casting in the general API ensures the correct device
51  * specific functions are called. You should specify an
52  * ADCBufCC26XX_ParamsExtension in the custom field of the ADCBuf_Params that
53  * suits your application. The default settings work for many, but not all,
54  * use cases.
55  *
56  * # General Behavior #
57  * A timer and the DMA are used to trigger the ADC and fill a buffer in the
58  * background (in hardware) at a specified frequency. The application may
59  * execute other tasks while the hardware handles the conversions. In contrast
60  * to the standard ti/drivers/ADC driver, this driver allows for precise
61  * sampling of waveforms.
62  *
63  * | Driver | Number of samples needed in one call |
64  * |----------------|-----------------------------------------|
65  * | ADC.h | 1 |
66  * | ADCBuf.h | > 1 |
67  *
68  * This ADCBuf driver provides an API interface to using the analog-to-digital
69  * converter directly from the CM3 without going through the sensor controller.
70  * The sensor controller can still use the ADC, support for sharing the ADC
71  * resource between the sensor controller and the CM3 is built into the driver.
72  * There is a hardware semaphore that the driver must acquire before beginning
73  * any number of conversions. This same hardware semaphore also prevents the
74  * simultaneous use of this driver and the basic ADC driver.
75  *
76  * The ADC drivers supports making between one and 1024 measurements once or
77  * continuous measuring with returned buffer sizes between one and 1024
78  * measurements.
79  *
80  * The application should call ADCBuf_init() once by the application to set the
81  * isOpened flag to false, indicating that the driver is ready to use.
82  *
83  * The ADC driver is opened by calling ADCBuf_open() which will
84  * set up interrupts and configure the internal components of the driver.
85  * However, the ADC hardware or analog pins are not yet configured, since the
86  * sensor controller or basic ADC driver might be using the ADC.
87  *
88  * In order to perform an ADC conversion, the application should call
89  * ADCBuf_convert(). This call will request the ADC resource, configure the ADC,
90  * set up the DMA and GPTimer, and perform the requested ADC conversions on the
91  * selected DIO or internal signal. The DIO or internal signal is defined by the
92  * ADCBuf_Conversion structure in the application code and adcBufCC26xxObjects
93  * in the board file.
94  *
95  * @warning If the ADCBUF driver is setup in ADCBuf_RECURRENCE_MODE_CONTINUOUS
96  * mode, the user must assure that the provided callback function is
97  * completed before the next conversion completes. If the next
98  * conversion completes before the callback function finishes, the DMA
99  * will clobber the previous buffer with new data.
100  *
101  * If the sensor controller is using the ADC when the driver requests it at the
102  * start of the ADC_convert() call, the conversion will fail and return false.
103  * The ADC resource may be pre-acquired by calling the control function
104  * ADCBufCC26XX_CMD_ACQUIRE_ADC_SEMAPHORE. It will be released again
105  * automatically after the next conversion completes.
106  *
107  * In both ADCBufCC26XX_SAMPING_MODE_SYNCHRONOUS mode and
108  * ADCBufCC26XX_SAMPING_MODE_ASYNCHRONOUS mode, enough sampling time must be
109  * provided between conversions that each measurement may be completed before
110  * the next trigger arrives.
111  *
112  * @note The ADCBuf driver requires GPTimer0A to function correctly. It
113  * expects it to be configured as position 0 in the GPTimer Config
114  * Table. GPTimer0A will be unavailable for other uses.
115  *
116  * # Supported ADC pins #
117  * Below is a table of the supported ADC IO pins for each package size, for both
118  * CC26xx and CC13xx. It maps a DIO to its corresponding driverlib define for
119  * the CompBInput that it is hardwired to. This table can be used to create
120  * virtual channel entries in the ADCBufCC26XX_adcChannelLut table in the board
121  * file.
122  *
123  * | DIO | CC26xx 7x7 AUXIO CompBInput | CC13xx 7x7 AUXIO CompBInput | CC26xx 5x5 AUXIO CompBInput | CC13xx 5x5 AUXIO CompBInput | CC26xx 4x4 AUXIO CompBInput | CC13xx 4x4 AUXIO CompBInput
124  * |--------|-------------------------------|-------------------------------|-------------------------------|-------------------------------|-------------------------------|-----------------------------
125  * | 0 | No | No | No | No | No | No
126  * | 1 | No | No | No | No | No | No
127  * | 2 | No | No | No | No | No | No
128  * | 3 | No | No | No | No | No | No
129  * | 4 | No | No | No | No | No | No
130  * | 5 | No | No | No | No | ADC_COMPB_IN_AUXIO7 | ADC_COMPB_IN_AUXIO7
131  * | 6 | No | No | No | No | ADC_COMPB_IN_AUXIO6 | ADC_COMPB_IN_AUXIO6
132  * | 7 | No | No | ADC_COMPB_IN_AUXIO7 | ADC_COMPB_IN_AUXIO7 | ADC_COMPB_IN_AUXIO5 | ADC_COMPB_IN_AUXIO5
133  * | 8 | No | No | ADC_COMPB_IN_AUXIO6 | ADC_COMPB_IN_AUXIO6 | ADC_COMPB_IN_AUXIO4 | ADC_COMPB_IN_AUXIO4
134  * | 9 | No | No | ADC_COMPB_IN_AUXIO4 | ADC_COMPB_IN_AUXIO4 | ADC_COMPB_IN_AUXIO3 | ADC_COMPB_IN_AUXIO3
135  * | 10 | No | No | ADC_COMPB_IN_AUXIO5 | ADC_COMPB_IN_AUXIO5 | No | No
136  * | 11 | No | No | ADC_COMPB_IN_AUXIO3 | ADC_COMPB_IN_AUXIO3 | No | No
137  * | 12 | No | No | ADC_COMPB_IN_AUXIO2 | ADC_COMPB_IN_AUXIO2 | No | No
138  * | 13 | No | No | ADC_COMPB_IN_AUXIO1 | ADC_COMPB_IN_AUXIO1 | No | No
139  * | 14 | No | No | ADC_COMPB_IN_AUXIO0 | ADC_COMPB_IN_AUXIO0 | No | No
140  * | 15-22 | No | No | No | No | No | No
141  * | 23 | ADC_COMPB_IN_AUXIO7 | ADC_COMPB_IN_AUXIO7 | No | No | No | No
142  * | 24 | ADC_COMPB_IN_AUXIO6 | ADC_COMPB_IN_AUXIO6 | No | No | No | No
143  * | 25 | ADC_COMPB_IN_AUXIO5 | ADC_COMPB_IN_AUXIO5 | No | No | No | No
144  * | 26 | ADC_COMPB_IN_AUXIO4 | ADC_COMPB_IN_AUXIO4 | No | No | No | No
145  * | 27 | ADC_COMPB_IN_AUXIO3 | ADC_COMPB_IN_AUXIO3 | No | No | No | No
146  * | 28 | ADC_COMPB_IN_AUXIO2 | ADC_COMPB_IN_AUXIO2 | No | No | No | No
147  * | 29 | ADC_COMPB_IN_AUXIO1 | ADC_COMPB_IN_AUXIO1 | No | No | No | No
148  * | 30 | ADC_COMPB_IN_AUXIO0 | ADC_COMPB_IN_AUXIO0 | No | No | No | No
149  *
150  * # Supported Internal Signals #
151  * Below is a table of internal signals that can be measured using the ADC.
152  * Since we are not connecting to a DIO, there is no DIO to internal signal
153  * mapping. The DIO field in the channel lookup table should be marked
154  * PIN_UNASSIGNED. This table can be used to create virtual channel entries in
155  * the ADCBufCC26XX_adcChannelLut table in the board file.
156  *
157  * | DIO | Internal Signal CompBInput |
158  * |--------------------|-------------------------------|
159  * | PIN_UNASSIGNED | ADC_COMPB_IN_DCOUPL |
160  * | PIN_UNASSIGNED | ADC_COMPB_IN_VSS |
161  * | PIN_UNASSIGNED | ADC_COMPB_IN_VDDS |
162  *
163  * # Error handling #
164  * The following errors may occur when opening the ADC without assertions enabled:
165  * - The ADC handle is already open.
166  *
167  * The following errors may occur when requesting an ADC conversion:
168  * - The ADC is currently already doing a conversion.
169  * - The ADC was not available (used by sensor controller or basic ADC).
170  *
171  *
172  * # Power Management #
173  * The TI-RTOS power management framework will try to put the device into the
174  * most power efficient mode whenever possible. Please see the technical
175  * reference manual for further details on each power mode.
176  *
177  * While converting, the ADCBufCC26XX driver sets a power constraint to keep
178  * the device out of standby. When the conversion has finished, the power
179  * constraint is released. The driver also sets a dependency on the DMA to
180  * enable background transfers from the ADC FIFO to memory and to clear the
181  * GPTimer interrupt.
182  * The following statements are valid:
183  * - After ADCBuf_convert(): the device cannot enter standby.
184  * - After ADCBuf_convertCancel(): the device can enter standby again.
185  * - After a conversion finishes: the device can enter standby again.
186  *
187  *
188  * # Supported Functions #
189  * | API function | Description |
190  * |------------------------------------|-----------------------------------------------------------------------|
191  * | ADCBuf_init() | Initialize ADC driver |
192  * | ADCBuf_open() | Open the ADC driver and configure driver |
193  * | ADCBuf_convert() | Perform ADC conversion |
194  * | ADCBuf_convertCancel() | Cancel ongoing ADC conversion |
195  * | ADCBuf_close() | Close ADC driver |
196  * | ADCBuf_Params_init() | Initialise ADCBuf_Params structure to default values |
197  * | ADCBuf_getResolution() | Get the resolution of the ADC of the current device |
198  * | ADCBuf_adjustRawValues() | Adjust the values in a returned buffer for manufacturing tolerances |
199  * | ADCBuf_convertAdjustedToMicroVolts | Convert a buffer of adjusted values to microvolts |
200  * | ADCBuf_control() | Execute device specific functions |
201  *
202  *
203  * # Not Supported Functionality #
204  * - Performing conversions on multiple channels simultaneously is not
205  * supported. In other words, the parameter channelCount must always be
206  * set to 1 when calling ADCBuf_convert(). The ADC on CC26XX devices does
207  * not support time-division multiplexing of channels or pins in hardware.
208  *
209  * # Use Cases #
210  * ## Basic one-shot conversion #
211  * Perform one conversion on CONFIG_ADCCHANNEL_A1 in ::ADCBuf_RETURN_MODE_BLOCKING.
212  * @code
213  * #include <ti/drivers/ADCBuf.h>
214  *
215  * #define ADCBUFFERSIZE 100
216  *
217  * ADCBuf_Handle adcBufHandle;
218  * ADCBuf_Params adcBufParams;
219  * ADCBuf_Conversion blockingConversion;
220  * uint16_t sampleBufferOne[ADCBUFFERSIZE];
221  *
222  * ADCBuf_Params_init(&adcBufParams);
223  * adcBufHandle = ADCBuf_open(CONFIG_ADCBuf0, &adcBufParams);
224  * if (adcBufHandle == NULL) {
225  * // handle error
226  * }
227  *
228  * blockingConversion.arg = NULL;
229  * blockingConversion.adcChannel = CONFIG_ADCCHANNEL_A1;
230  * blockingConversion.sampleBuffer = sampleBufferOne;
231  * blockingConversion.sampleBufferTwo = NULL;
232  * blockingConversion.samplesRequestedCount = ADCBUFFERSIZE;
233  *
234  * if (ADCBuf_convert(adcBufHandle, &blockingConversion, 1) != ADCBuf_STATUS_SUCCESS) {
235  * // handle error
236  * }
237  * @endcode
238  *
239  * ## Using ADCBufCC26XX_ParamsExtension #
240  * This specific configuration performs one conversion on CONFIG_ADCCHANNEL_A1
241  * in ::ADCBuf_RETURN_MODE_BLOCKING. The custom parameters used here are
242  * identical to the defaults parameters. Users can of course define their own
243  * parameters.
244  * @code
245  * #include <ti/drivers/ADCBuf.h>
246  *
247  * #define ADCBUFFERSIZE 100
248  *
249  * ADCBuf_Handle adcBufHandle;
250  * ADCBuf_Params adcBufParams;
251  * ADCBuf_Conversion blockingConversion;
252  * uint16_t sampleBufferOne[ADCBUFFERSIZE];
253  * ADCBufCC26XX_ParamsExtension customParams;
254  *
255  * ADCBuf_Params_init(&adcBufParams);
256  * customParams.samplingDuration = ADCBufCC26XX_SAMPLING_DURATION_2P7_US;
257  * customParams.refSource = ADCBufCC26XX_FIXED_REFERENCE;
258  * customParams.samplingMode = ADCBufCC26XX_SAMPING_MODE_SYNCHRONOUS;
259  * customParams.inputScalingEnabled = true;
260  *
261  * adcBufParams.custom = &customParams;
262  *
263  * adcBufHandle = ADCBuf_open(CONFIG_ADCBuf0, &adcBufParams);
264  * if (adcBufHandle == NULL) {
265  * // handle error
266  * }
267  *
268  * blockingConversion.arg = NULL;
269  * blockingConversion.adcChannel = CONFIG_ADCCHANNEL_A1;
270  * blockingConversion.sampleBuffer = sampleBufferOne;
271  * blockingConversion.sampleBufferTwo = NULL;
272  * blockingConversion.samplesRequestedCount = ADCBUFFERSIZE;
273  *
274  * if (ADCBuf_convert(adcBufHandle, &blockingConversion, 1) != ADCBuf_STATUS_SUCCESS) {
275  * // handle error
276  * }
277  * @endcode
278  *
279  * # Instrumentation #
280  * The ADC driver interface produces log statements if instrumentation is
281  * enabled.
282  *
283  * Diagnostics Mask | Log details |
284  * ---------------- | ----------- |
285  * Diags_USER1 | basic ADCBuf operations performed |
286  * Diags_USER2 | detailed ADCBuf operations performed |
287  *
288  ******************************************************************************
289  */
290 
291 #ifndef ti_drivers_adc_adcbufcc26xx__include
292 #define ti_drivers_adc_adcbufcc26xx__include
293 
294 #include <stdint.h>
295 #include <stdbool.h>
296 
297 #include <ti/drivers/ADCBuf.h>
298 #include <ti/drivers/PIN.h>
302 #include <ti/drivers/Power.h>
304 
305 #include <ti/devices/DeviceFamily.h>
306 #include DeviceFamily_constructPath(driverlib/aux_adc.h)
307 
308 #include <ti/drivers/dpl/HwiP.h>
309 #include <ti/drivers/dpl/ClockP.h>
310 #include <ti/drivers/dpl/SemaphoreP.h>
311 #include <ti/drivers/dpl/SwiP.h>
312 
313 #ifdef __cplusplus
314 extern "C" {
315 #endif
316 
329 /* Add ADCBufCC26XX_CMD_* macros here */
330 
346 #define ADCBufCC26XX_CMD_ACQUIRE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 1
347 
363 #define ADCBufCC26XX_CMD_KEEP_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 2
364 
373 #define ADCBufCC26XX_CMD_KEEP_ADC_SEMAPHORE_DISABLE ADCBuf_CMD_RESERVED + 3
374 
381 #define ADCBufCC26XX_CMD_RELEASE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 4
382 
388 #define ADCBufCC26XX_RESOLUTION 12
389 
390 #define ADCBufCC26XX_BYTES_PER_SAMPLE 2
391 
392 /*
393  * =============================================================================
394  * Constants
395  * =============================================================================
396  */
397 
398 /* ADCBuf function table pointer */
400 
401 
402 /*
403  * =============================================================================
404  * Enumerations
405  * =============================================================================
406  */
407 
423 typedef enum {
427 
438 typedef enum {
439  ADCBufCC26XX_SAMPLING_DURATION_2P7_US = AUXADC_SAMPLE_TIME_2P7_US,
440  ADCBufCC26XX_SAMPLING_DURATION_5P3_US = AUXADC_SAMPLE_TIME_5P3_US,
441  ADCBufCC26XX_SAMPLING_DURATION_10P6_US = AUXADC_SAMPLE_TIME_10P6_US,
442  ADCBufCC26XX_SAMPLING_DURATION_21P3_US = AUXADC_SAMPLE_TIME_21P3_US,
443  ADCBufCC26XX_SAMPLING_DURATION_42P6_US = AUXADC_SAMPLE_TIME_42P6_US,
444  ADCBufCC26XX_SAMPLING_DURATION_85P3_US = AUXADC_SAMPLE_TIME_85P3_US,
445  ADCBufCC26XX_SAMPLING_DURATION_170_US = AUXADC_SAMPLE_TIME_170_US,
446  ADCBufCC26XX_SAMPLING_DURATION_341_US = AUXADC_SAMPLE_TIME_341_US,
447  ADCBufCC26XX_SAMPLING_DURATION_682_US = AUXADC_SAMPLE_TIME_682_US,
448  ADCBufCC26XX_SAMPLING_DURATION_1P37_MS = AUXADC_SAMPLE_TIME_1P37_MS,
449  ADCBufCC26XX_SAMPLING_DURATION_2P73_MS = AUXADC_SAMPLE_TIME_2P73_MS,
450  ADCBufCC26XX_SAMPLING_DURATION_5P46_MS = AUXADC_SAMPLE_TIME_5P46_MS,
451  ADCBufCC26XX_SAMPLING_DURATION_10P9_MS = AUXADC_SAMPLE_TIME_10P9_MS
453 
454 
487 typedef enum {
488  ADCBufCC26XX_FIXED_REFERENCE = AUXADC_REF_FIXED,
489  ADCBufCC26XX_VDDS_REFERENCE = AUXADC_REF_VDDS_REL
491 
492 
493 
494 /*
495  * =============================================================================
496  * Structs
497  * =============================================================================
498  */
499 
508 typedef struct{
509  uint8_t dio;
510  uint8_t compBInput;
512 
521 typedef struct{
523  ADCBufCC26XX_Sampling_Duration samplingDuration;
526  ADCBufCC26XX_Sampling_Mode samplingMode;
529  ADCBufCC26XX_Reference_Source refSource;
547 
568 typedef struct{
575  uint32_t swiPriority;
590  uint8_t intPriority;
595 
596 
597 
603 typedef struct{
604  /* ADC control variables */
606  bool isOpen;
616  uint8_t currentChannel;
618  ADCBufCC26XX_Reference_Source refSource;
620  ADCBufCC26XX_Sampling_Mode samplingMode;
622  ADCBufCC26XX_Sampling_Duration samplingDuration;
631 
632  /* ADC SYS/BIOS objects */
634  HwiP_Struct hwi;
636  SwiP_Struct swi;
638  SemaphoreP_Struct conversionComplete;
641 
642  /* PIN driver state object and handle */
647 
648  /* UDMA driver handle */
651 
652  /* GPTimer driver handle */
655 
661 
662 /*
663  * =============================================================================
664  * Functions
665  * =============================================================================
666  */
667 
668 
669 #ifdef __cplusplus
670 }
671 #endif
672 
673 #endif /* ti_drivers_adc_ADCBufCC26XX__include */
ADCBufCC26XX_Sampling_Mode
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26XX.h:423
Definition: ADCBufCC26XX.h:424
Definition: ADCBufCC26XX.h:489
Definition: ADCBufCC26XX.h:439
GPTimerCC26XX_Handle timerHandle
Definition: ADCBufCC26XX.h:654
GPTimer driver implementation for CC26XX/CC13XX.
ADCBufCC26XX_Reference_Source refSource
Definition: ADCBufCC26XX.h:529
bool inputScalingEnabled
Definition: ADCBufCC26XX.h:545
bool adcSemaphoreInPossession
Definition: ADCBufCC26XX.h:614
Definition: ADCBufCC26XX.h:443
bool isOpen
Definition: ADCBufCC26XX.h:606
ADCBufCC26XX Hardware Attributes.
Definition: ADCBufCC26XX.h:568
ADCBuf_Return_Mode returnMode
Definition: ADCBufCC26XX.h:628
Definition: ADCBufCC26XX.h:450
Power Manager.
Analog to Digital Conversion Buffer (ADCBuf) Input Driver.
Definition: ADCBufCC26XX.h:447
ADCBufCC26XX_Sampling_Mode samplingMode
Definition: ADCBufCC26XX.h:526
uint32_t swiPriority
ADC SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: ADCBufCC26XX.h:575
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:223
Power manager interface for CC26XX/CC13XX.
uint32_t semaphoreTimeout
Definition: ADCBufCC26XX.h:657
CC26XX specfic extension to ADCBuf_Params.
Definition: ADCBufCC26XX.h:521
PIN_Handle pinHandle
Definition: ADCBufCC26XX.h:646
Definition: ADCBufCC26XX.h:444
uint8_t intPriority
ADC peripheral&#39;s interrupt priority.
Definition: ADCBufCC26XX.h:590
ADCBufCC26XX_Reference_Source refSource
Definition: ADCBufCC26XX.h:618
Definition: ADCBufCC26XX.h:446
bool inputScalingEnabled
Definition: ADCBufCC26XX.h:610
Device-specific pin & GPIO driver for CC26xx family [def].
ADCBufCC26XX_Sampling_Duration samplingDuration
Definition: ADCBufCC26XX.h:523
Definition: ADCBufCC26XX.h:445
bool keepADCSemaphore
Definition: ADCBufCC26XX.h:612
ADCBufCC26XX_Sampling_Duration samplingDuration
Definition: ADCBufCC26XX.h:622
ADCBuf_Callback callbackFxn
Definition: ADCBufCC26XX.h:624
ADCBuf_Recurrence_Mode recurrenceMode
Definition: ADCBufCC26XX.h:626
Definition: ADCBufCC26XX.h:448
Definition: ADCBufCC26XX.h:451
struct ADCBufCC26XX_Object * ADCBufCC26XX_Handle
The definition of an ADCBuf function table that contains the required set of functions to control a s...
Definition: ADCBuf.h:603
Definition: ADCBufCC26XX.h:425
UDMACC26XX driver implementation.
Definition: ADCBufCC26XX.h:442
Definition: ADCBufCC26XX.h:488
ADCBufCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26XX.h:487
UDMACC26XX_Handle udmaHandle
Definition: ADCBufCC26XX.h:650
Definition: ADCBufCC26XX.h:440
bool conversionInProgress
Definition: ADCBufCC26XX.h:608
SemaphoreP_Struct conversionComplete
Definition: ADCBufCC26XX.h:638
uint8_t currentChannel
Definition: ADCBufCC26XX.h:616
ADCBufCC26XX_AdcChannelLutEntry const * adcChannelLut
Definition: ADCBufCC26XX.h:593
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:407
underlying data structure for type PIN_State
Definition: PIN.h:708
ADCBufCC26XX_Sampling_Mode samplingMode
Definition: ADCBufCC26XX.h:620
ADCBuf_Recurrence_Mode
Recurrence behavior of a ADCBuf_Conversion specified in the ADCBuf_Params.
Definition: ADCBuf.h:407
ADCBuf_Return_Mode
Return behavior for ADCBuf_convert() specified in the ADCBuf_Params.
Definition: ADCBuf.h:449
uint8_t dio
Definition: ADCBufCC26XX.h:509
PIN_State pinState
Definition: ADCBufCC26XX.h:644
ADCBuf_Conversion * currentConversion
Definition: ADCBufCC26XX.h:640
SwiP_Struct swi
Definition: ADCBufCC26XX.h:636
uint32_t samplingFrequency
Definition: ADCBufCC26XX.h:659
Defines a conversion to be used with ADCBuf_convert().
Definition: ADCBuf.h:315
uint8_t compBInput
Definition: ADCBufCC26XX.h:510
Definition: ADCBufCC26XX.h:441
Definition: ADCBufCC26XX.h:449
ADCBufCC26XX Object.
Definition: ADCBufCC26XX.h:603
const ADCBuf_FxnTable ADCBufCC26XX_fxnTable
HwiP_Struct hwi
Definition: ADCBufCC26XX.h:634
void(* ADCBuf_Callback)(ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel, int_fast16_t status)
The definition of a callback function.
Definition: ADCBuf.h:393
Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal...
Definition: ADCBufCC26XX.h:508
Generic PIN & GPIO driver.
uint16_t * activeSampleBuffer
Definition: ADCBufCC26XX.h:630
ADCBufCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCBufCC26XX.h:438
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale