70 #ifndef ti_drivers_aescbc_AESCBCCC26XX__include 71 #define ti_drivers_aescbc_AESCBCCC26XX__include 78 #include <ti/drivers/dpl/SwiP.h>
int_fast16_t returnStatus
Definition: AESCBCCC26XX.h:116
AESCBC_OperationType operationType
Definition: AESCBCCC26XX.h:118
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_Operation *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:485
Struct containing the parameters required for encrypting/decrypting a message.
Definition: AESCBC.h:436
bool threadSafe
Definition: AESCBCCC26XX.h:115
AESCBC_ReturnBehavior
The way in which CBC function calls return after performing an encryption or decryption operation...
Definition: AESCBC.h:407
AESCBC_Operation * operation
Definition: AESCBCCC26XX.h:121
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: AESCBCCC26XX.h:103
AESCBCCC26XX Object.
Definition: AESCBCCC26XX.h:111
AESCBCCC26XX Hardware Attributes.
Definition: AESCBCCC26XX.h:90
bool isOpen
Definition: AESCBCCC26XX.h:112
uint32_t semaphoreTimeout
Definition: AESCBCCC26XX.h:119
bool operationInProgress
Definition: AESCBCCC26XX.h:113
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:465
AESCBC_ReturnBehavior returnBehavior
Definition: AESCBCCC26XX.h:117
bool operationCanceled
Definition: AESCBCCC26XX.h:114
AESCBC_CallbackFxn callbackFxn
Definition: AESCBCCC26XX.h:120