69 #ifndef ti_drivers_aesctr_AESCTRCC26XX__include 70 #define ti_drivers_aesctr_AESCTRCC26XX__include int_fast16_t returnStatus
Definition: AESCTRCC26XX.h:113
AESCTR_OperationType
Enum for the operation types supported by the driver.
Definition: AESCTR.h:434
AESCTR_ReturnBehavior
The way in which CTR function calls return after performing an encryption or decryption operation...
Definition: AESCTR.h:378
uint32_t semaphoreTimeout
Definition: AESCTRCC26XX.h:116
Struct containing the parameters required for encrypting/decrypting a message.
Definition: AESCTR.h:410
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: AESCTRCC26XX.h:100
bool operationCanceled
Definition: AESCTRCC26XX.h:111
bool isOpen
Definition: AESCTRCC26XX.h:109
bool operationInProgress
Definition: AESCTRCC26XX.h:110
AESCTRCC26XX Object.
Definition: AESCTRCC26XX.h:108
AESCTR_ReturnBehavior returnBehavior
Definition: AESCTRCC26XX.h:114
AESCTRCC26XX Hardware Attributes.
Definition: AESCTRCC26XX.h:87
void(* AESCTR_CallbackFxn)(AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_Operation *operation, AESCTR_OperationType operationType)
The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_C...
Definition: AESCTR.h:478
AESCTR_CallbackFxn callbackFxn
Definition: AESCTRCC26XX.h:117
AESCTR_Operation * operation
Definition: AESCTRCC26XX.h:118
AESCTR_OperationType operationType
Definition: AESCTRCC26XX.h:115
bool threadSafe
Definition: AESCTRCC26XX.h:112