ECJPAKECC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
88 #ifndef ti_drivers_ecjpake_ECJPAKECC26X2__include
89 #define ti_drivers_ecjpake_ECJPAKECC26X2__include
90 
91 #include <stdint.h>
92 #include <stdbool.h>
93 
94 #include <ti/drivers/Power.h>
95 #include <ti/drivers/ECJPAKE.h>
98 
99 #include <ti/drivers/dpl/HwiP.h>
100 #include <ti/drivers/dpl/SwiP.h>
101 #include <ti/drivers/dpl/SemaphoreP.h>
102 
103 #ifdef __cplusplus
104 extern "C" {
105 #endif
106 
107 /* Exit the SWI and wait until an HWI call posts the SWI again */
108 #define ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP ECJPAKE_STATUS_RESERVED - 0
109 /* Execute the next FSM state immediately without waiting for the next HWI */
110 #define ECJPAKECC26X2_STATUS_FSM_RUN_FSM ECJPAKE_STATUS_RESERVED - 1
111 
121 typedef enum {
132 
144 
155 
171 
181 
183 
190 typedef struct {
203  uint8_t intPriority;
205 
211 typedef struct {
212  bool isOpen;
215  int_fast16_t operationStatus;
218  ECJPAKECC26X2_FsmState fsmState;
222  uint32_t resultAddress;
224 
225 #ifdef __cplusplus
226 }
227 #endif
228 
229 #endif /* ti_drivers_ecjpake_ECJPAKECC26X2__include */
Definition: ECJPAKECC26X2.h:146
The CryptoKey type is an opaque representation of a cryptographic key.
Definition: ECJPAKECC26X2.h:147
Definition: ECJPAKECC26X2.h:148
ECJPAKE_OperationType
Enum for the operation types supported by the driver.
Definition: ECJPAKE.h:1047
ECJPAKECC26X2_FsmState fsmState
Definition: ECJPAKECC26X2.h:218
Definition: ECJPAKECC26X2.h:152
bool isOpen
Definition: ECJPAKECC26X2.h:212
Power Manager.
int_fast16_t operationStatus
Definition: ECJPAKECC26X2.h:215
ECJPAKE_ReturnBehavior returnBehavior
Definition: ECJPAKECC26X2.h:217
uint8_t intPriority
PKA Peripheral&#39;s interrupt priority.
Definition: ECJPAKECC26X2.h:203
void(* ECJPAKE_CallbackFxn)(ECJPAKE_Handle handle, int_fast16_t returnStatus, ECJPAKE_Operation operation, ECJPAKE_OperationType operationType)
The definition of a callback function used by the ECJPAKE driver when used in ECJPAKE_RETURN_BEHAVIOR...
Definition: ECJPAKE.h:1073
Definition: ECJPAKECC26X2.h:150
bool operationInProgress
Definition: ECJPAKECC26X2.h:213
Definition: ECJPAKECC26X2.h:137
ECJPAKECC26X2 Object.
Definition: ECJPAKECC26X2.h:211
Definition: ECJPAKECC26X2.h:122
uint32_t resultAddress
Definition: ECJPAKECC26X2.h:222
uint32_t semaphoreTimeout
Definition: ECJPAKECC26X2.h:221
Definition: ECJPAKECC26X2.h:143
ECJPAKECC26X2_FsmState
ECJPAKECC26X2 states.
Definition: ECJPAKECC26X2.h:121
Definition: ECJPAKECC26X2.h:164
Definition: ECJPAKECC26X2.h:154
ECJPAKECC26X2 Hardware Attributes.
Definition: ECJPAKECC26X2.h:190
TI Driver for Elliptic Curve Password Authenticated Key Exchange by Juggling.
Definition: ECJPAKECC26X2.h:170
bool operationCanceled
Definition: ECJPAKECC26X2.h:214
ECJPAKE_Operation operation
Definition: ECJPAKECC26X2.h:219
Definition: ECJPAKECC26X2.h:131
ECJPAKE_ReturnBehavior
The way in which ECJPAKE function calls return after performing an encryption + authentication or dec...
Definition: ECJPAKE.h:800
ECJPAKE_CallbackFxn callbackFxn
Definition: ECJPAKECC26X2.h:216
Definition: ECJPAKECC26X2.h:168
ECJPAKE_OperationType operationType
Definition: ECJPAKECC26X2.h:220
Union containing pointers to all supported operation structs.
Definition: ECJPAKE.h:1036
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale