253 #ifndef ti_drivers_UART__include 254 #define ti_drivers_UART__include 280 #define UART_CMD_RESERVED (32) 294 #define UART_STATUS_RESERVED (-32) 309 #define UART_STATUS_SUCCESS (0) 317 #define UART_STATUS_ERROR (-1) 326 #define UART_STATUS_UNDEFINEDCMD (-2) 345 #define UART_CMD_PEEK (0) 356 #define UART_CMD_ISAVAILABLE (1) 367 #define UART_CMD_GETRXCOUNT (2) 379 #define UART_CMD_RXENABLE (3) 392 #define UART_CMD_RXDISABLE (4) 397 #define UART_ERROR (UART_STATUS_ERROR) 402 #define UART_WAIT_FOREVER (~(0U)) 420 typedef void (*
UART_Callback) (UART_Handle handle,
void *buf,
size_t count);
576 typedef int_fast16_t (*
UART_ControlFxn) (UART_Handle handle, uint_fast16_t cmd,
void *arg);
593 typedef int_fast32_t (*
UART_ReadFxn) (UART_Handle handle,
void *buffer,
613 typedef int_fast32_t (*
UART_WriteFxn) (UART_Handle handle,
const void *buffer,
621 const void *buffer,
size_t size);
738 extern int_fast16_t
UART_control(UART_Handle handle, uint_fast16_t cmd,
void *arg);
835 extern int_fast32_t
UART_write(UART_Handle handle,
const void *buffer,
size_t size);
860 extern int_fast32_t
UART_writePolling(UART_Handle handle,
const void *buffer,
size_t size);
908 extern int_fast32_t
UART_read(UART_Handle handle,
void *buffer,
size_t size);
930 extern int_fast32_t
UART_readPolling(UART_Handle handle,
void *buffer,
size_t size);
ADC_Params params
Definition: Driver_Init.h:11
UART_STOP
UART stop bit settings.
Definition: UART.h:522
void(* UART_CloseFxn)(UART_Handle handle)
A function pointer to a driver specific implementation of UART_CloseFxn().
Definition: UART.h:570
void * object
Definition: UART.h:682
UART_Callback writeCallback
Definition: UART.h:554
int_fast16_t UART_control(UART_Handle handle, uint_fast16_t cmd, void *arg)
Function performs implementation specific features on a given UART_Handle.
UART_LEN dataLength
Definition: UART.h:560
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:634
UART_Callback readCallback
Definition: UART.h:553
UART_PAR
UART parity type settings.
Definition: UART.h:532
UART_ControlFxn controlFxn
Definition: UART.h:639
UART_Mode
UART mode settings.
Definition: UART.h:427
int_fast32_t(* UART_ReadFxn)(UART_Handle handle, void *buffer, size_t size)
A function pointer to a driver specific implementation of UART_ReadFxn().
Definition: UART.h:593
int_fast16_t(* UART_ControlFxn)(UART_Handle handle, uint_fast16_t cmd, void *arg)
A function pointer to a driver specific implementation of UART_ControlFxn().
Definition: UART.h:576
UART_PAR parityType
Definition: UART.h:562
UART_DataMode
UART data mode settings.
Definition: UART.h:482
int_fast32_t UART_writePolling(UART_Handle handle, const void *buffer, size_t size)
Function that writes data to a UART, polling the peripheral to wait until new data can be written...
UART_Echo readEcho
Definition: UART.h:558
UART_ReturnMode
UART return mode settings.
Definition: UART.h:460
UART_WritePollingFxn writePollingFxn
Definition: UART.h:660
void UART_close(UART_Handle handle)
Function to close a UART peripheral specified by the UART handle.
void UART_readCancel(UART_Handle handle)
Function that cancels a UART_read() function call.
UART_Echo
UART echo settings.
Definition: UART.h:500
UART Global configuration.
Definition: UART.h:677
void const * hwAttrs
Definition: UART.h:685
UART_Mode writeMode
Definition: UART.h:550
UART_STOP stopBits
Definition: UART.h:561
UART_ReturnMode readReturnMode
Definition: UART.h:555
UART_CloseFxn closeFxn
Definition: UART.h:636
void UART_init(void)
Function to initialize the UART module.
uint32_t baudRate
Definition: UART.h:559
UART_Handle(* UART_OpenFxn)(UART_Handle handle, UART_Params *params)
A function pointer to a driver specific implementation of UART_OpenFxn().
Definition: UART.h:588
struct UART_Config_ UART_Config
UART Global configuration.
void UART_Params_init(UART_Params *params)
Function to initialize the UART_Params struct to its defaults.
int_fast32_t UART_write(UART_Handle handle, const void *buffer, size_t size)
Function that writes data to a UART with interrupts enabled.
void UART_writeCancel(UART_Handle handle)
Function that cancels a UART_write() function call.
UART_DataMode readDataMode
Definition: UART.h:556
UART_WriteCancelFxn writeCancelFxn
Definition: UART.h:663
int_fast32_t(* UART_WriteFxn)(UART_Handle handle, const void *buffer, size_t size)
A function pointer to a driver specific implementation of UART_WriteFxn().
Definition: UART.h:613
int_fast32_t(* UART_ReadPollingFxn)(UART_Handle handle, void *buffer, size_t size)
A function pointer to a driver specific implementation of UART_ReadPollingFxn().
Definition: UART.h:600
int_fast32_t UART_readPolling(UART_Handle handle, void *buffer, size_t size)
Function that reads data from a UART without interrupts. This API must be used mutually exclusive wit...
void(* UART_InitFxn)(UART_Handle handle)
A function pointer to a driver specific implementation of UART_InitFxn().
Definition: UART.h:582
uint32_t readTimeout
Definition: UART.h:551
UART_Handle UART_open(uint_least8_t index, UART_Params *params)
Function to initialize a given UART peripheral.
UART_ReadPollingFxn readPollingFxn
Definition: UART.h:651
UART_ReadCancelFxn readCancelFxn
Definition: UART.h:654
UART_FxnTable const * fxnTablePtr
Definition: UART.h:679
int_fast32_t(* UART_WritePollingFxn)(UART_Handle handle, const void *buffer, size_t size)
A function pointer to a driver specific implementation of UART_WritePollingFxn(). ...
Definition: UART.h:620
UART_LEN
UART data length settings.
Definition: UART.h:510
void * custom
Definition: UART.h:563
void(* UART_ReadCancelFxn)(UART_Handle handle)
A function pointer to a driver specific implementation of UART_ReadCancelFxn().
Definition: UART.h:607
UART Parameters.
Definition: UART.h:548
struct UART_Config_ * UART_Handle
A handle that is returned from a UART_open() call.
Definition: UART.h:407
UART_ReadFxn readFxn
Definition: UART.h:648
int_fast32_t UART_read(UART_Handle handle, void *buffer, size_t size)
Function that reads data from a UART with interrupt enabled.
UART_OpenFxn openFxn
Definition: UART.h:645
void(* UART_WriteCancelFxn)(UART_Handle handle)
A function pointer to a driver specific implementation of UART_WriteCancelFxn().
Definition: UART.h:627
UART_DataMode writeDataMode
Definition: UART.h:557
UART_Mode readMode
Definition: UART.h:549
UART_WriteFxn writeFxn
Definition: UART.h:657
uint32_t writeTimeout
Definition: UART.h:552
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:420
UART_InitFxn initFxn
Definition: UART.h:642