DMM 15.4 Sensor + BLE Remote Display
Table of Contents
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Dynamic Multi-protocol Manager
- Usage
- DMM Sensor Reboot and Reset
- DMM Limitations
- 5.10.xx Release Notes
Introduction
The dmm_154sensor_remote_display project showcases a dynamic multi-protocol example which enables concurrent proprietary IEEE 802.15.4g frequency hoping (WiSUN FAN) and BLE5. This example implements an IEEE 802.15.4g Sub1Ghz Wireless Network with a BLE Remote Display, using TI's DMM (Dynamic Multi-protocol Manager) to enable the multi-protocol and dual band features of the CC1352.
The BLE remote display allows a SmartPhone App to commission the IEEE 802.15.4g sensor and to see data on the IEEE 802.15.4g Sub1G Wireless Network.
This project has the following app configurations available:
App Build Configuration | Description |
---|---|
FlashROM_Release (default) | All TI-RTOS debug features disabled but application-logging to UART remains enabled. The application uses the config file ble_release.cfg and the defines are in <app name>_FlashROM_Release.opt . |
All application configurations use the stack library configuration, FlashROM_Library. This build configuration will yield additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Stack Library Configuration section of the BLE5-Stack User's Guide provided in the SDK.
This document discusses the procedure for using the DMM IEEE 802.15.4g Sensor Remote Display application when the FlashROM_Release configuration is used.
Note: There is a Launchpad SensorTag (LPSTK) variant of this example located in
/examples/rtos/CC1352R1_LAUNCHXL
. The LPSTK variant is nearly identical to the base example. The only difference is that the sensor sends additional sensor values to the collector. This includes the LPSTK's light, hall effect and accelerometer sensor readings. The LPSTK variant should be flashed to the LPSTK board to read the additional sensor values. The collector by default will not know how to read the additional sensor readings. Adding theLPSTK
define to the project is enough to get the collector ready for the new sensor readings.
Hardware Prerequisites
The default Simple Peripheral configuration uses the LAUNCHXL-CC1352R1. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE5-Stack User's Guide.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the dependencies section of the Release Notes located in the root folder of the SDK.
For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack Quick Start Guide.
Note: If you are running an OAD example, be sure to first build and flash a BIM project located in
/examples/nortos/<BOARD>/bim
. For more instructions on how to do this, please refer to the BLE5-Stack Quick Start Guide.
Dynamic Multi-protocol Manager
The DMM uses 2 main components to dynamically arbitrate the RF resource.
- A Policy Manager
- A Scheduler
TI CC1352 devices are capable of dual band operation, the CC1352 Launchpad (TI development platform) has a dual band antenna which performs well in the 868/916MHz band as well as the 2.4GHz band. Using the DMM on a CC1352 device enables not only multi protocol, but also dual band. The below diagram shows how the DMM allows 2 stacks to run on the same device, which was previously only possible on 2 devices. In the diagram the Stack 1 is shown functioning along side Stack 2, this could be a BLE stack and a proprietary Sub1G stack (called Wireless Sensor Network) or a 15.4 Stack. The Stacks used are defined by the developer.
Single mode setup:
DMM Setup:
The DMM makes scheduling decisions based on Application Level information, Stack Level information, and the Global Priority Table (GPT).
The Stack Level information is embedded in each RF command and it includes: Start Type, Start Time, AllowDelay, Priority, Activity, etc.
The Global Priority Table (GPT) defines relative priorities of the two stacks
based on the activity and priority of RF commands. For details of the GPT,
refer to <SDK_DIR>\source\ti\common\dmm\dmm_priority_ble_154sensor.c/h
.
The Application Level information is the user defined information via the policy
table and inludes: Application State Name, Weight, AppliedActivity, Pause, etc;
the policy table can have multiple policies. A policy defines a specific state
of the DMM application where the user wants to apply different priority based on
an action. A simplified policy table is shown below, it defines the behavior
when Stack 1 is performing an OAD and does not take into account the specific
state of the stack 2 (i.e. any state). It specifies that when Stack 1 is in an
OAD state, the priority of the BLE_CONNECTION
, in this case, is increased by
25. If any RF scheduling conflicts happen during the OAD, they will be resolved
by taking into account the modified priority defined in the policy.
Stack 1 State Name | Stack 2 State Name | Weight | Applied Activity | Description |
---|---|---|---|---|
OAD | Any | 25 | CONNECTION | Increase the priority of CONNECTION activity of Stack 1 by 25 during OAD operation |
The policy used in this example is more complex than the illustration above. For
details of the actual policy used refer to
<SDK_DIR>\source\ti\common\dmm\policy.h
and ti_dmm_application_policy.c/h
as
generated by the SysConfig tool.
The DMM also supports pausing/resuming stacks based on a policy change. This is achieved by an application callback, which is called from the DMM policy manager when a policy change requiring a stack to pause operation is entire. An example of pausing the Zigbee stack during a BLE_OAD is provided in the DMM Zigbee Coordinator Switch + BLE OAD example.
See the DMM chapter in your protocol stack user's guide for more information about DMM.
Usage
This example should be used in conjunction with the 15.4 Stack Collector.
Note: The 15.4 Collector must be built with the same 15.4 mode setting, as configured with the SysConfig tool.
This application uses the UART peripheral to provide an interface for the application.
This document will use PuTTY to serve as the display for the output of the CC1352 LaunchPad. The LightBlue smartphone application will act as the BLE Central device that will connect to the Remote Display service in this example. The LightBlue smartphone application is available on the App Store and Google Play. Note that any other serial terminal and smartphone BLE scanner application may be used. The following default parameters are used for the UART peripheral for display:
UART Param | Default Values |
---|---|
Baud Rate | 115200 |
Data length | 8 bits |
Parity | None |
Stop bits | 1 bit |
Flow Control | None |
Note: If you are using a smartphone as the BLE central device and the same CC1352 LaunchPad was used previously with a different DMM or BLE example then you may need to forget the device in the smartphone BLE settings, then disable and enable BLE. Not doing this could result in the smartphone application displaying incorrect services and characteristics.
Once the 15.4 Sensor Remote Display application starts, the output to the terminal will report its BLE address and the fact that it is advertising which is enabled by default upon startup, as shown below:
The Collector should be showing:
BLE Services Overview
This project contains 2 service: - Provisioning Service used to configure the device for connecting to an IEEE 802.15.4g network. - Remote Display Service used to display sensor reading and configure the sensor reporting interval
The characteristic UUID is a 128b, with 16b that are used to specify the characteristic. The below shows the format of the 128b UUID:
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xB0, 0x00, 0x40, 0x51, 0x04, LOW BYTE OF UUID, HIGH BYTE OF UUID, 0x00, 0xF0
Provisioning Service/Profile Table
The provisioning profile is defined in software_stacks/ble_stack/profiles/provisioning_gatt_profile.c
The Characteristics and properties are shown below.
Characteristic | UUID | Format | Properties |
---|---|---|---|
Network PAN ID | 1191 | 2 Byte Integer | Auth Read/Write |
Network Channel Mask | 1194 | 17 Byte Integer | Auth Read/Write |
Default Network Key | 1196 | 16 Byte Integer | Auth Read/Write |
Start Network Provisioning | 1197 | 1 Byte Integer | Auth Read/Write |
Network Provisioning State | 1198 | 1 Byte Integer | Auth Read |
Sensor Service/Profile Table
The provisioning profile is defined in software_stacks/ble_stack/profiles/remote_display_gatt_profile.c
The Characteristics and properties are shown below.
Characteristic | UUID | Format | Properties |
---|---|---|---|
Sensor Data | 1181 | 2 Byte Integer | Read/Notify |
Sensor Report Interval | 1182 | 4 Byte Integer | Read/Write |
Collector LED Identify | 1183 | 1 Byte Integer | Read/Write |
BLE Multi-Connections
This project is configured by default to make use of Multiple (4) BLE Connections. This means that the DMM project will be able to support 4 BLE connections on top of the secondary stack network.
Updating Multi-Connection Settings
The Multi-Connection Settings can easily be changed via the Sysconfig tool. No application changes are required by the user to go from 1 connection to 4 connections.
As always, with network configuration changes, it's important to recognize that the update could change the bandwidth requirements by the stack. When moving from the default settings to something new, you as the developer should take time to consider how this will effect your network requirements.
Using the Common User Interface
Note: The screenshots in this section were taken from the DMM 15.4 Collector + BLE project. There will be slight differences in the UART terminal depending on which project you are working with.
The Common User Interface (CUI) controls the access to User Interface resources. On a LaunchPad device, these resources are made up of Buttons, LEDs and UART I/O.
Using a UART terminal with the configuration described above, use the arrow keys to navigate the menu. Upon startup, pressing the ENTER key will display the HELP menu, as shown below:
To demonstrate the use of the CUI, let us change the BLE PHY. First, use the
arrow keys to select the TI Remote Display
menu. Pressing the ENTER key
will take us to the TI Remote Display
menu. Next, we see the option to
CONFIGURE
or go BACK
to the previous menu. Make sure CONFIGURE
is
selected and hit the ENTER key to enter the CONFIGURE
menu. Here, we have
the option to SET PHY
. After pressing ENTER once more, we can select a
PHY. Chose the 2M PHY. You should see confirmation of this on the UART
display, as shown below.
Note: When using the CUI, the buttons on the LaunchPad should not be used to navigate the CUI menu. These buttons perform other actions as described in the following section.
Provisioning the 15.4 Sensor to the Network
Before the user can connect the sensor to the 15.4 network, the network must be formed and opened on the 15.4 Collector.
The user has 2 choices regarding the provisioning the sensor to a 15.4 Network:
- Press the LEFT button on the sensor to make the sensor search and join a network with the default provisioning settings as configured with the SysConfig tool.
- Use a BLE central device (such as the LightBLue Smartphone Application) to configure the provisioning settings and make the sensor search and join a network with those settings.
- Use the Common User Interface (CUI) configure the provisioning settings and make the sensor search and join a network with those settings.
Note: The UART terminal output will be similar regardless of which method is used to provision the network and control the connected sensors.
Provisioning the 15.4 Network via BLE
To provision the device using BLE use LightBlue to scan for the device, you should see a device with the name of "DMM 15.4 Sensor RD" (note that the navigation might be slightly different depending on your mobile application):
If there is more than 1 device called Node Remote Display, the RSSI value under the strength bars on the left can be used to find which device you are trying to connect to. Press the "connect" button to connect to the device. When prompted enter the pairing code "123456".
Once connected, the terminal window will show the address of the connected device (smartphone):
In LightBlue, you should be able to see various information about the Node Remote Display device:
You should see the provisioning service, which is labeled as "UUID: F0001190-0451-B000-000000000000" (this may be slightly different for other smartphone applications). Under this service there should be the following characteristics shown:
The following sections detail the functions and operations of each of the characteristics.
Network PAN ID Characteristic (UUID: 1191)
This characteristic sets PAN ID that the 15.4 sensor will join. This is the same as setting CONFIG_PAN_ID in the sensor config.h file.
Setting CONFIG_PAN_ID or Node Data Characteristic to 0xFFFF (the default) on the Sensor allows it to join any network, setting it to a specific valeue forces it to only join a network with that PAN ID. Setting CONFIG_PAN_ID in config.h to 0xFFFF on the Collector allows it to form a network with a random PAN ID, setting it to a specific value forces it to form a network with that specific PAN ID.
Sensor Operating Channels Characteristic (UUID: 1194)
This characteristic sets Channel mask that the 15.4 sensor will use to find a network. This is the same as setting CONFIG_CHANNEL_MASK, CONFIG_FH_CHANNEL_MASK and FH_ASYNC_CHANNEL_MASK in the sensor config.h file.
To successfully discover and join a network the same setting must be used on the Sensor and Collector.
Network Security Key Characteristic (UUID: 1196)
This characteristic sets security key that the 15.4 sensor will use encrypt and decrypt 15.4 packet data payload. This is the same as setting KEY_TABLE_DEFAULT_KEY in the sensor config.h file.
To successfully communicate with the Collector the Network Security Key Characteristic must be set the same as the Collector KEY_TABLE_DEFAULT_KEY in config.h.
Provision Sensor Characteristic (UUID: 1197)
This characteristic is used to make the sensor search for and associate to an IEEE 802.15.4g network or disassociate from the network.
Writing the value 0xAA to this characteristic to start the Joining processes and the sensor will search for and join the IEEE 802.15.4g network using the provisioning settings.
Writing 0xDD to this characteristic while the sensor is connected to a IEEE 802.15.4g network will cause the sensor to disassociate from the network. The sensor can then be re-provisioned and made to join the same network again, or a new network depending on the provisioning settings.
Note: All the above provisioning characteristics default to those configured with the SysConfig Tool. The characteristics only need to be written to if the user requires to change them from the defaults.
Note: In FH mode, the BLE connection may drop while the sensor associates to the IEEE 802.15.4g network. The BLE connection can be resumed once the 15.4 Sensor is associated to a 15.4 network, and full concurrent IEEE 802.15.4g Frequency Hopping and BLE advertisements or connection can be demonstrated.
Sensor Provisioning State (UUID: 1198)
This characteristic is used to read the sensors 802.15.4g network state. The following states will be observed:
- Sensor Provisioning State 0: Waiting to be initialized
- Sensor Provisioning State 1: Joining a network
- Sensor Provisioning State 2: Restoring a network
- Sensor Provisioning State 3: Joined a network
- Sensor Provisioning State 4: Restored a network
- Sensor Provisioning State 5: Orphaned from a network
Provisioning the 15.4 Network via CUI
To provision the device using the CUI, navigate to the TI SENSOR
menu and
press the ENTER key to enter this menu.
Then, navigate to the NETWORK ACTIONS
tab and press the ENTER key to enter
this submenu.
Next, navigate to ASSOCIATE
and press the ENTER key.
The DMM 15.4 sensor will now search and join a 15.4 network with the default provisioning settings as configured with the SysConfig tool.
Note 1: The above screenshot was taken after a BLE connection was established between the LaunchPad and a smartphone.
Note 2: The screenshots shown in this example do not reflect default network settings.
Finally, use the CUI on the collector project to form and open the 15.4 Network, allowing the sensor to join.
Once connected, the following UART output should be displayed:
For more details regarding the use of CUI for 15.4 network configuration,
refer to the sensor project's README.html file, located here: <SDK
DIR>\examples\rtos\CC1352R1_LAUNCHXL\ti154stack\sensor\README.html
Provisioned 15.4 Sensor
The 15.4 Sensor data that is sent to the Collector is also mirrored in a BLE characteristic. The rate at which the sensor wakes and sends data can also be set using a BLE characteristic.
You should see the remote display service, which is labeled as "UUID: F0001180-0451-B000-000000000000" (this may be slightly different for other smartphone applications). Under this service there should be the following characteristics shown:
Sensor Data Characteristic (UUID: 1181)
This characteristic supports read only and notify properties, and it contains a 2-byte-long value indicating the sensor data. In LightBlue the notifications can be enabled by clicking on the Sensor Data characteristic and then clicking on "Listen for notifications", notice that the value is updating every 5s by default. Click on the "Read again" item read the characteristic.
If you disable notifications then make sure you re-enable them as this will be useful when changing the report interval later.
Sensor Report Interval Characteristic (UUID: 1182)
This characteristic supports read and write properties, it contains a 4-byte-long value indicating the sensor report interval in ms. By default this is set to 5s, you will notice that both the Sensor Data on the Collector and the Sensor Data BLE Characteristic is updated every 5s. This 5s update can also be seen on the LightBlue app when notifications are enabled. In the LightBlue application select the Sensor Report Interval characteristic. From here you can read and write the report interval. When a value is written the rate at which node data is updated changes to reflect the new value.
Note: In LightBlue you must write to the characteristic in hex, using the correct number of digits, or the length will be incorrect and the Remote Display profile will reject the write. To set the report interval to 1s write an value of 000003E8.
Collector LED Identify (UUID: 1183)
This characteristic supports read and write properties, it contains a 1-byte-long value used to make the Sub1GHz 802.15.4 Collector Blink its LED. The value represents the duration in seconds to blink. This characteristic can be used to identify the collector that the sensor is connected to.
DMM 15.4 Security Manager (SM) Commissioning
If using either a dmm_154sensor_sm_remote_display_app
or dmm_154collector_sm_remote_display_app
project, these will support secure commissioning of a SM Sensor to a SM Collector. This DMM project will enable remote control and monitoring of the secure commissioning service via a BLE phone application connected to a DMM device. Once the phone is connected to the DMM device, the user will be able to select the Authentication Mode via the BLE phone application. If the user selects the "Passkey" mode, then the user will be able to enter the passkey via the app. This passkey will be passed to the BLE Remote Display application and then passed to the SM Sensor application. This passkey will then be used to begin commissioning of the Sensor to the Collector network. Throughout the commissioning process status updates will be sent to the BLE phone application.
Using DMM SM Commissioning Example
The SimpleLink Starter
mobile application is the easiest way to get started using the DMM SM feature. The steps below outline the how to use the app:
Open the
SimpleLink Starter
mobile application, scan and connect to theDMM 15.4 SM Collec
. Once the services load, select theDMM Provisioning Service
.Click
Form Network
to form a new 15.4 network.Once the network has formed, click
Open Network
to allow devices to connect to the network.Once the DMM SM Collector network has been setup, disconnect the mobile app from the device.
Scan and connect the
DMM 15.4 SM Sensor
device. Wait for all the services to load and select theDMM Provisioning Service
.Once connected, the app will read and display the current SM State in the
TI15.4 Security Manager
section. Tap theAuth Mode Selection
drop down menu to select one of the three desired authentication modes (Passkey, Default Code, Just Allow). If nothing is selected, the "Default Code" mode will be used during the commissioning process.In the
TI DMM Provisioning Interface
section, click theSTART PROVISIONING (CONNECT)
button.Once the SM Sensor associates to the open SM Collector, the SM Commissioning process will start. If "Default Mode" or "Just Allow" was selected the commissioning process will be automatic and the commissioning state will eventually update to
SM Success
if the commissioning process was successful. If the commissioning process fails, it will be re-attempted two more times. If all attempts fail, the Sensor will decommission from the Collector's network.If "Passkey" was selected as the authentication mode, the app will eventually pop-up a module for the user to enter a custom 6-digit passkey.
After the passkey has been entered on the DMM SM Sensor device, disconnect the mobile app from the DMM SM Sensor and connect to the
DMM 15.4 SM Collec
device.Once the services load, select the
DMM Provisioning Service
.The app will eventually pop-up a module for the user to enter the same custom 6-digit passkey entered on the DMM SM Sensor.
After the passkey has been entered, the commissioning process will complete and the commissioning state will eventually update to
SM Success
if the commissioning process was successful. If the commissioning process fails, it will be re-attempted two more times. On each re-attempt, the user will have the ability to re-enter a custom passkey on each device. If all attempts fail, the Sensor will decommission from the Collector's network.If desired, after commissioning, the user may disconnect from the DMM SM Collector and connect to the DMM SM Sensor via the
SimpleLink Starter
app to view the current SM Commissioning State of the sensor.
By default, the DMM examples can support connecting up to 4 BLE centrals devices at a time. Due to the secure nature of the SM Commissioning Profile, it is important to only allow a single device being able to read/write to the SM Auth Mode and Passkey characteristics at a time. This will limit the ability for an attacker to interfere with the SM commissioning process. This will be accomplished by only allowing the first device that has an authenticated BLE bond and is trying to access an SM characteristic. Once this first device disconnects, the next device that aligns with the same criteria will be allowed to read/write the characteristics.
SM Commissioning BLE Service
A separate BLE profile sm_commisioning_gatt_profile
is enabled to control and track all SM related activities. The sm_commisioning_gatt_profile
has the following characeristics and permissions.
Service UUID: 0xf000baaa-0451-4000-b000-000000000000
Below summarizes the characteristics that comprise the SM Service:
- SMCOMMISSIONING_PROFILE_STATECHAR_UUID
- SMCOMMISSIONING_PROFILE_SETAUTHMODECHAR_UUID
- SMCOMMISSIONING_PROFILE_SETPASSKEYCHAR_UUID
SMCOMMISSIONING_PROFILE_STATECHAR_UUID
- Description: BLE characteristic used to define state of the sensor as it is commissioning to a SM Collector.
- UUID: 0xf000baab-0451-4000-b000-000000000000
- Len: 1
- GATT Properties: GATT_PROP_READ, GATT_PROP_NOTIFY
- GATT Val Permissions: GATT_PERMIT_AUTHEN_READ
- Valid Values:
0x0000: SM Idle
0x0001: SM Starting
0x0002: SM Request Passkey
0x0003: SM Passkey Timeout
0x0004: SM Commissioning
0x0005: SM Success
0x0006: SM Error
Otherwise: Error
The software flowchart below describes the different scenarios for the SMCOMMISSIONING_PROFILE_STATECHAR_UUID to be updated. Updates to the SMCOMMISSIONING_PROFILE_STATECHAR_UUID characteristic are illustrated by the green circle objects.
SMCOMMISSIONING_PROFILE_SETAUTHMODECHAR_UUID
- Description: BLE characteristic used to define the Authentication Mode used by the TI154Stack SM commissioning process.
- UUID: 0xf000baac-0451-4000-b000-000000000000
- Len: 1
- GATT Properties: GATT_PROP_READ, GATT_PROP_WRITE
- GATT Val Permissions: GATT_PERMIT_AUTHEN_READ, GATT_PERMIT_AUTHEN_WRITE
- Valid Values:
0x0001: Passkey
0x0002: Default Code
0x0004: Just Allow
SMCOMMISSIONING_PROFILE_SETPASSKEYCHAR_UUID
- Description: BLE characteristic used to define the Passkey entered by a user during the TI154Stack SM Passkey based commissioning process.
- UUID: 0xf000baad-0451-4000-b000-000000000000
- Len: 4
- GATT Properties: GATT_PROP_WRITE
- GATT Val Permissions: GATT_PERMIT_AUTHEN_WRITE
- Valid Values: Any
Block Mode Test
Block Mode is demonstrated in DMM example applications via the Block Mode Test feature. This feature allows a user via the serial interface to enable/disable a periodic timer that toggles DMM Block Mode on and off at user defined periods.
This feature is enabled by declaring the BLOCK_MODE_TEST
pre-compile variable in the DMM project .opts
file.
User Interface
Using the serial user interface, the user can configure the following Block Mode Test parameters at runtime:
- Block Mode Test On
- Block Mode Test Off
- Block Mode On Period (ms)
- Block Mode Off Period (ms)
The instructions below cover the Block Mode Test configuration for the BLE remote_display application, but also apply to the secondary stack application.
Using the Left or Right arrow keys on your keyboard, navigate to the
TI Remote Display
menu and press the Enter key.Using the Left or Right arrow keys on your keyboard, navigate to the
BLOCK MODE TEST
menu and press the Enter key.To turn on the Block Mode Test, use the Left or Right arrow keys on your keyboard, navigate to the
BM TEST ON
menu and press the Enter key. You will see theBLOCK MODE TEST STATUS
line change toEnabled
.To turn off the Block Mode Test, use the Left or Right arrow keys on your keyboard, navigate to the
BM TEST OFF
menu and press the Enter key. You will see theBLOCK MODE TEST STATUS
line change toDisabled
.To change the Block Mode On Period, use the Left or Right arrow keys on your keyboard, navigate to the
ON VAL (ms)
menu and press the Enter key. You will then be able to enter a 4 digit decimal value representing the period of time for which Block Mode will be enabled for BLE in milliseconds. Press the Enter key to submit you changes.To change the Block Mode Off Period, use the Left or Right arrow keys on your keyboard, navigate to the
OFF VAL (ms)
menu and press the Enter key. You will then be able to enter a 4 digit decimal value representing the period of time for which Block Mode will be disabled for BLE in milliseconds. Press the Enter key to submit you changes.
Block Mode Test Activity
The diagram below represents the stack activity when you enabled and disable the Block Mode Test.
On the Block Mode Clock event, the DMM Block Mode Status will be toggled and the Block Mode Test Period will be updated. If the current DMM Block Mode Status is "True", the DMM Block Mode status will be set "Off" (DMM Block Mode Status will be set to "False") and the Block Mode Test Clock will be updated to a timeout value of RD_BLOCK_MODE_OFF_PERIOD. If the current DMM Block Mode Status is "False", the DMM Block Mode status will be set "On" (DMM Block Mode Status will be set to "True") and the Block Mode Test Clock will be updated to a timeout value of RD_BLOCK_MODE_ON_PERIOD.
Disabling Common User Interface
The common user interface (CUI) is a UART based interface that allows users to control and receive updates regarding the application. For various reasons, including reducing the memory footprint, the user is able to disable the common user interface (CUI). To disable the CUI, the following variable must be defined in the dmm_154sensor_remote_display_app.opts
:
-DCUI_DISABLE
Please Note: particular features that are dependednt on the CUI wil be unavailable when this feature is enabled.
DMM Sensor Reboot and Reset
By default the DMM 15.4 Sensor RD is configured to store network parameters in Non-Volatile memory and will be allow the sensor to rejoin the network on power cycle or reset. To disable this feature you need to change:
-DNV_RESTORE
to
-DxNV_RESTORE
in the
Tools/dmm_154sensor_remote_display_cc13x2r1lp_app_FlashROM_Release.opt
file.
Once this feature is disabled the sensor will not store its connected collector information in NV. The connected sensor will not rejoin the network when it is reset or power cycled.
By default, the DMM Sensor will not rejoin the 15.4 network on its own on reset. It must be done manually using the steps above with either the GPIO buttons, the CUI, or BLE.
To clear the NV, perform a device reset while holding the RIGHT button.
Note: Once booted the RIGHT button is used to turn Disassociate from the network. Be careful not to hold the Right button down for to long.
DMM Limitations
The initial implementation of 15.4 + BLE DMM has only been tested with this policy.
The following limitations exist in the DMM implementation:
- Connection intervals lower than 60ms will result in high sub1G packet loss when BLE is connected.
- When connecting to a central device Sub-1G packet loss may be experienced until the update parameters are sent 1s after connection. This will be dependent on the initial connection interval of the BLE central devices.
5.10.xx Release Notes
FEATURE_FREQ_HOP_MODE has been added as a pre-defined symbol to the DMM 15.4 Collector & Sensor Sub-1 GHz examples for the CC1352 devices. This symbol is added to keep the capability of the Frequency Hopping mode, which is still required to be turned on through SysConfig. It is recommended that developers do not remove or modify this symbol.